PCB Fabrication: Prototype & Mass Production

FR-4 PCB

FR-4 PCB

Made with A-grade materials, supporting 1–32-layer PCBs with controlled impedance. Prices start at $2 for 5 pcs, with build times as fast as 24 hours.

Flex PCB

Flex PCB

Offers excellent flexibility and high circuit density, supporting PI, FR-4, and 3M tape stiffeners. Prices start at $2 for 5 pcs, with build times as fast as 4 days.

Aluminum PCB

Aluminum PCB

Features high thermal conductivity and excellent electrical insulation, making it ideal for LED applications. Prices start at $4 for 5 pcs, with build times as fast as 3 days.

Copper PCB

Copper PCB

Offers excellent thermal conductivity and heat dissipation for high-power supplies and LED applications.

Rogers PCB

Rogers PCB

Low dissipation factor and excellent dimensional stability. Perfect for high-frequency applications.

PTFE Teflon PCB

PTFE Teflon PCB

Low dissipation factor and excellent performance in high-temperature and high-frequency applications.

Your Trusted Global PCB Partner

3,000+

Daily Orders Processed

8M+

PCBs Produced Annually

100+

Professional Assembly Lines

180+

Countries and Regions Served

We power the electronics industry with scalable manufacturing and reliable quality across prototype, batch-build, and mass production—backed by 20+ years of precision engineering.

PCB manufacturing facility

PCB Assembly Manufacturing Process

Phase 1: Pre-production

  • Step 1 Data Preparation
  • Step 2 Data Finalization
  • Step 3 Components Sourcing
  • Step 4 PCB Fabrication

Phase 2: Assembly

  • Step 5 Solder Paste Printing
  • Step 6 SPI Inspection
  • Step 7 PCB Assembly Setup
  • Step 8 Reflow Soldering

Phase 3: Inspection & Logistics

  • Step 9 SMT Assembly QC (AOI)
  • Step 10 Wave Soldering / QC
  • Step 11 Packaging
  • Step 12 Shipping

Customer Testimonials

PCBA pricing is incredibly competitive without sacrificing quality. It's refreshing to find a supplier that delivers such great value.

Amazing PCB fabrication! Rapid delivery was critical in our ability to launch new products on time. Highly recommended.

After switching to LCSC PCBA, we noticed a significant improvement in reliability. The quality is evident in every board.

Technical support during design was exceptional. Proactive feedback helped us catch errors early — first-attempt perfection.

Scaling from prototype to full production was seamless. Consistency across thousands of units is remarkable.

We ordered from multiple suppliers simultaneously. LCSC arrived first, had the best finish, and cost the least.

The solder mask and silkscreen alignment on our multi-layer boards were flawless. Exceptional precision for high-density layouts at a fraction of local fabrication costs.

Integration between the LCSC component catalog and the PCB assembly pipeline is incredibly streamlined. Saved us weeks of sourcing hassle, and the turnaround time was phenomenal.

PCBA pricing is incredibly competitive without sacrificing quality. It's refreshing to find a supplier that delivers such great value.

Amazing PCB fabrication! Rapid delivery was critical in our ability to launch new products on time. Highly recommended.

After switching to LCSC PCBA, we noticed a significant improvement in reliability. The quality is evident in every board.

Technical support during design was exceptional. Proactive feedback helped us catch errors early — first-attempt perfection.

Scaling from prototype to full production was seamless. Consistency across thousands of units is remarkable.

We ordered from multiple suppliers simultaneously. LCSC arrived first, had the best finish, and cost the least.

The solder mask and silkscreen alignment on our multi-layer boards were flawless. Exceptional precision for high-density layouts at a fraction of local fabrication costs.

Integration between the LCSC component catalog and the PCB assembly pipeline is incredibly streamlined. Saved us weeks of sourcing hassle, and the turnaround time was phenomenal.

Built for Every Industry

LCSC PCB & PCBA solutions engineered for the world's most demanding environments

Industrial Control

Industrial Control

Industrial Control

Reliable assemblies designed for harsh environments and long product lifecycles.

  • High Reliability
  • Long lifecycle
  • Harsh environments
  • IPC Class 2
Most Popular
Medical Devices

Medical Devices

Medical Devices

Controlled manufacturing processes compliant with global healthcare standards.

  • High Precision
  • Strict traceability
Most Popular
Consumer Electronics

Consumer Electronics

Consumer Electronics

Fast turnaround for prototypes and iterative product development with optimized cost efficiency.

  • Rapid Prototyping
  • Agile Development
  • Cost Efficiency
Most Popular

FAQ

  • 1. Could you tell me the maximum dimensions for PCB assembly?

    The maximum dimensions vary depending on the order type:
    Economic PCBA:
    - Single PCB size: 10 x 10 mm to 470 x 500 mm
    - PCB panel size: 10 x 10 mm to 250 x 250 mm
    Standard PCBA:
    - Single PCB size: 70 x 70 mm to 460 x 500 mm
    - PCB panel size: 70 x 70 mm to 250 x 250 mm

  • 2. For a custom printed circuit board, what file formats are accepted for the drill file?
  • 3. What documents are required for pcba orders?
  • 4. I have a PCB design that includes both SMD and through-hole (THT) components. Can you assemble it?
  • 5. Do you assemble PCBs with surface-mount components on both sides?

New Member Offer

Save Up to $158 on PCB & PCBA

Free registration required