EAGLE — an acronym for Easily Applicable Graphical Layout Editor — was an electronic design automation (EDA) application originally developed by the German company CadSoft Computer GmbH and later acquired by Autodesk Inc.
SCH and .BRD design files aren’t lost: Autodesk Fusion’s Electronics workspace opens them directly, and KiCad’s built-in EAGLE importer is the most common free migration path. Previously generated Gerber and Excellon/NC drill files remain fully manufacturable on any fabrication line, regardless of which CAD tool produced them.
What Was EAGLE PCB CAD?
At its core, EAGLE was a scriptable EDA application combining schematic capture, printed circuit board layout, an auto-router, and computer-aided manufacturing (CAM) output. Schematic files used the .SCH extension, board layouts used .BRD, and component definitions lived in .LBR device libraries, with parts placeable across multiple sheets and connected through logical ports.
EAGLE was built to solve a specific problem: making professional-grade PCB design accessible to individuals and small teams without the cost or complexity of enterprise EDA suites. It linked a schematic editor to a PCB layout editor so that circuit connections drawn on paper-like diagrams translated directly into copper traces on a board, with automatic synchronization between schematic and layout keeping both representations consistent as a design evolved.
Functionally, a designer placed components from device libraries onto a schematic sheet, wired them together, then switched to the board editor to arrange footprints and route traces — manually or with the built-in autorouter. A full set of electronic rule checks validated the design against specification before it moved to manufacturing, and the software produced standard Gerber and drill-file outputs compatible with mainstream fabricators.
Its lasting appeal came from a gentle learning curve, a large library of community-contributed parts, and a free license tier for hobbyists and students, which turned it into the de facto teaching tool of a generation of electronics hackers. That advantage faded after Autodesk’s acquisition, when EAGLE moved from a perpetual-license model to a subscription model — and its standalone existence has now ended entirely, folded into Autodesk Fusion’s Electronics workspace.
Key Features and Advantages
| Feature | Description | Benefit |
| Schematic capture | Multi-sheet schematic editor with port-based hierarchical connections | Organizes complex designs into reusable blocks |
| Schematic-layout sync | Bidirectional synchronization between .SCH and .BRD files | Prevents drift between circuit intent and physical layout |
| Design rule checking | Built-in electrical (ERC) and design (DRC) rule checks | Catches errors before fabrication, reducing respins |
| Autorouter | Automated trace-routing engine | Speeds up layout of simple to moderate density boards |
| CAM/Gerber output | Built-in templates for standard Gerber and drill data | Straightforward handoff to PCB manufacturers |
| MCAD-ECAD bridge | Component placement synced with Fusion, no file conversion | Reduces enclosure-fit errors between teams |
Technical Specifications and Timeline
| Parameter | Value / Detail |
| File formats | .SCH (schematic), .BRD (board), .LBR (library) |
| Fabrication output | Gerber (RS-274X), Excellon/NC drill files |
| Platforms (historical) | Windows, macOS, Linux (64-bit only from v8.0.0) |
| Licensing model | Subscription-only since v8.0.0 (2017); bundled with Fusion 360 since Jan 2020 |
| Last standalone version | EAGLE 9.6.2, released 27 May 2020 |
| End of life | June 7, 2026 — no longer sold or supported, and the standalone application can no longer be run |
| Continuation path | Design technology continues inside Autodesk Fusion’s Electronics workspace |
Migration Options for Existing EAGLE Users
- Migrate to Autodesk Fusion — Fusion opens EAGLE .sch and .brd files directly, preserving schematic and layout data inside Autodesk’s unified mechanical-and-electronics platform.
- Migrate to KiCad — KiCad is free, open-source, and includes an importer that reads EAGLE files natively, making it the most common landing point for users leaving the Autodesk ecosystem.
- Keep fabrication outputs as-is — Gerber and Excellon/NC drill files are industry-standard formats accepted by any PCB manufacturer regardless of the originating CAD tool, so completed designs remain manufacturable even now that the software itself is gone.
- Archive-only use — some teams retain old EAGLE installations purely to reference legacy .brd/.sch files before a full migration.
Where EAGLE Was Used
- Education — many universities and small R&D teams taught and used EAGLE for years because of its long history, stable feature set, and abundant tutorials.
- Maker and hobbyist electronics — the free tier made EAGLE the default choice for hackerspace projects, Arduino shields, and small IoT gadgets for over a decade.
- Small hardware teams / startups — EAGLE targeted users building consumer electronics, IoT devices, and educational prototypes rather than high-end signal-integrity work.
- Mechanical-electrical co-design — linking board layout to Fusion’s mechanical modeling let component and outline changes propagate to the 3D enclosure.
- Legacy design maintenance — a large volume of existing boards and reference designs remain in EAGLE format, keeping some installations alive purely for maintenance.
Manufacturing and Fabrication Support
EAGLE itself never manufactured boards, but it was built to hand designs cleanly to fabricators: it provided standard CAM outputs — Gerber and drill files — along with integrated PCB quoting options, simplifying work with mainstream PCB fabricators. For product teams working with OEM/ODM suppliers, exporting EAGLE files alongside CAD data supported accurate enclosure-fit checks before tooling. None of this changes for boards already designed — a finished EAGLE project’s fabrication files remain valid and manufacturable on any standard production line, independent of whether EAGLE itself is still running.
EAGLE vs. KiCad vs. Fusion Electronics
| Attribute | EAGLE (legacy) | KiCad | Fusion Electronics |
| Cost | Subscription (discontinued) | Free, open-source | Included with Fusion subscription |
| Support status | End of life since June 7, 2026 | Actively developed | Actively developed |
| Learning curve | Low-moderate | Low-moderate | Moderate |
| MCAD integration | Via Fusion only | Limited/third-party | Native, unified |
| Library size | Large legacy libraries | 100k+ symbols/footprints | Thousands of managed parts |
| Best fit | Legacy project maintenance only | Hobbyists, educators, migrators | Teams wanting one ECAD+MCAD vendor |
Frequently Asked Questions
Is EAGLE PCB CAD still available to buy or download?
No. Autodesk’s end-of-life date for EAGLE was June 7, 2026, after which it is no longer sold or supported, and the standalone application can no longer be run.
Can I still open my old .sch and .brd files now that EAGLE is discontinued?
Yes, through migration — Autodesk Fusion opens EAGLE .sch and .brd files directly, and KiCad can import them via its EAGLE importer.
Will my previously fabricated Gerber files still work with PCB manufacturers?
Yes — Gerber and Excellon/NC drill files are industry standards accepted by any PCB manufacturer regardless of which CAD tool produced them.
What’s the recommended free alternative to EAGLE?
KiCad is the most commonly recommended alternative — free, open-source, actively developed, and includes an EAGLE file importer.
Why did Autodesk retire EAGLE instead of continuing to update it?
Autodesk has been consolidating its electronics-design tooling into Fusion’s unified Electronics workspace, merging mechanical and electrical design in one platform rather than maintaining EAGLE as a separate product line.
Find What You Need on LCSC
Whichever CAD tool you migrate to — Fusion Electronics, KiCad, or another platform — LCSC supports the fabrication side of the workflow with standard Gerber and Excellon/NC file uploads for instant PCB quoting, alongside the components your migrated schematic calls for. Search LCSC’s catalog by part number, package, or specification to match footprints carried over from legacy EAGLE libraries, with clear datasheets and stock levels for verification before you place an order. Browse LCSC’s PCB fabrication and component sourcing tools to move a migrated design from files to finished boards.