Electrochemical sensor design and capacitor selection rely on two formulas that show up constantly in analog front-end and power circuit work: the Nernst equation, which governs how voltage responds to ion concentration, and capacitor unit conversion, which governs how engineers move between picofarads, nanofarads, microfarads, and farads.
Takeaway
- The Nernst equation, E = E° − (RT/nF) × ln(Q), predicts how an electrochemical cell’s voltage shifts with ion concentration and temperature — central to BMS design, pH probes, and corrosion monitoring.
- At 25°C, RT/F simplifies to about 0.02569 V, a constant engineers use for fast hand calculations.
- Capacitor units scale by powers of 1,000: 1 F = 1,000,000 µF, 1 µF = 1,000 nF, 1 nF = 1,000 pF.
- A 0.1 µF capacitor equals 100,000 pF and is marked “104” on ceramic packages.
- Both formulas converge in sensor front-end design, where a Nernstian signal is filtered through nF-to-µF capacitors before reaching an ADC.
The Nernst Equation
The Nernst equation describes how the voltage, or electrode potential, of an electrochemical cell changes as a function of ion concentration and temperature, moving beyond the idealized “standard condition” assumptions used in basic electrochemistry. In its standard form:
E = E° − (RT/nF) × ln(Q)
| Symbol | Meaning |
| E | Observed electrode potential (V) |
| E° | Standard electrode potential (V) |
| R | Universal gas constant (8.314 J/mol·K) |
| T | Temperature (Kelvin) |
| n | Number of electrons transferred in the reaction |
| F | Faraday’s constant (96,485 C/mol) |
| Q | Reaction quotient (products over reactants) |
At room temperature (25°C), the term RT/F simplifies to a fixed value of approximately 0.02569 V, which engineers often convert to base-10 logarithms for faster hand calculations.
Where Does the Nernst Equation Show Up in Electronic Design?
For electronic component designers, the Nernst equation isn’t just chemistry-class theory — it directly explains the behavior of components that convert chemical or ionic activity into electrical signals:
- Batteries and fuel cells: the equation predicts how open-circuit voltage shifts as a cell discharges and ion concentrations change, which is central to battery management system (BMS) design and state-of-charge estimation.
- Electrochemical sensors: pH probes, oxygen sensors, and ion-selective electrodes rely on Nernstian response curves to convert a chemical concentration into a measurable voltage for downstream analog front-end circuitry.
- Corrosion monitoring circuits: potentiostats and corrosion-monitoring instrumentation apply the Nernst equation’s principles to deliver accurate, real-time data, informing protective circuitry in industrial and marine electronics.
- PCB and control system design: the Nernst equation helps define the control unit and measurement algorithm before schematic and layout work begins on electrochemical monitoring systems.
Because the equation is temperature-dependent, designers building temperature-compensated sensor front-ends need to account for the RT/nF term shifting with ambient or process temperature — a detail that matters as much in component selection as in firmware calibration.
Capacitor Unit Conversions
Once a circuit’s electrical behavior is defined, engineers translate design requirements into physical components. Capacitors are specified across an enormous dynamic range — from single-digit picofarads in RF tuning circuits to thousands of microfarads in power supply filtering. Moving cleanly between units prevents costly BOM errors, datasheet misreads, and prototype failures.
The base relationships :
| Conversion | Multiplier |
| 1 F → µF | × 1,000,000 |
| 1 µF → nF | × 1,000 |
| 1 nF → pF | × 1,000 |
| 1 pF → nF | ÷ 1,000 |
| 1 nF → µF | ÷ 1,000 |
| 1 µF → F | ÷ 1,000,000 |
In short: 1 farad equals 1,000,000 µF, 1 µF equals 1,000 nF, and 1 nF equals 1,000 pF.
How Do You Convert Between Capacitor Units?
A capacitor conversion calculator automates this scaling so engineers don’t have to track decimal places by hand. The user enters a value, selects the source unit, selects the target unit, and the tool returns the converted result instantly. Internally, most calculators first convert the input value to picofarads — the smallest common unit — before converting to the desired output unit.
Worked example: converting 0.1 µF to nanofarads is 0.1 × 1,000 = 100 nF. That same 0.1 µF value equals 100,000 pF, and appears on many capacitor packages under the printed code “104,” per EIA capacitor marking convention — where the first two digits represent the significant value and the third digit is the multiplier of zeros, expressed in picofarads.
Unit choice also correlates with capacitor type and application:
| Unit Range | Typical Capacitor Type | Common Application |
| 1–100 pF | Ceramic (NP0/C0G) | RF tuning, timing circuits |
| 100 pF–1 nF | Ceramic, film | Filtering, coupling |
| 1 nF–1 µF | Film, ceramic (X7R) | Decoupling, snubber circuits |
| 1 µF–10,000+ µF | Electrolytic, tantalum | Power supply filtering, bulk storage |
Conversion accuracy matters beyond simple unit relabeling. Real capacitors carry tolerance, and capacitance can shift with temperature, frequency, DC bias, and aging depending on the dielectric technology used.
Where the Two Concepts Meet
While the Nernst equation and capacitor unit conversions sit in different domains — one electrochemical, one purely dimensional — they nevertheless converge directly in electrochemical sensor front-end design. Specifically, a Nernstian sensor produces a small, temperature-sensitive voltage; engineers typically buffer and filter this signal using capacitors specified in the nF-to-µF range to reject noise before it reaches an ADC. Consequently, getting the Nernst-predicted signal range right and selecting the correct filter capacitor value are both prerequisites for an accurate sensor circuit.
FAQ
What is the Nernst equation used for in electronics?
It’s used to predict how the voltage output of electrochemical cells, batteries, and ion-sensitive sensors changes with concentration and temperature, which informs analog front-end and BMS design.
How do I convert microfarads to picofarads?
Multiply the microfarad value by 1,000,000, or convert in two steps: µF → nF (×1,000), then nF → pF (×1,000).
Why do capacitor datasheets use different units (pF, nF, µF)?
Indeed, different capacitor technologies and applications span an immense range of values. For example, engineers typically specify RF ceramics under 100 pF, whereas they use electrolytics reaching thousands of µF for power filtering. Consequently, manufacturers conventionally express each component family in the unit that keeps numbers manageable.
Does temperature affect the Nernst equation’s result?
Yes. Temperature appears directly in the RT/nF term, so a sensor’s Nernstian output voltage shifts with ambient or process temperature, which is why many designs include temperature compensation.
Can a capacitor conversion calculator account for tolerance?
No. A conversion calculator handles the exact mathematical relationship between units only.
Find What You Need on LCSC
LCSC stocks millions of components from More Asian Brands at Better Value, including NP0/C0G, X7R, electrolytic, and tantalum capacitors across the full pF-to-µF range covered in this guide, plus potentiostats, ADCs, and analog front-end ICs for electrochemical sensor and BMS designs. Full datasheets, real-time stock levels, and parametric filtering — by capacitance, tolerance, voltage rating, and package size — make it easy to confirm a converted capacitor value against the manufacturer’s actual test conditions before you commit it to a BOM.