Key Takeaways: Power supply architecture selection starts by comparing input and output voltage ranges. If Vin always exceeds Vout, use a buck converter; if Vin is always lower, use a boost; if the ranges overlap, use a buck-boost or SEPIC. Add an LDO only when noise or PSRR matters more than efficiency.
Every power supply design starts with the same question: how do you get from the voltage you have to the voltage your circuit needs? The answer isn’t just “buck or boost.” Modern designs pull from a toolbox of switching and linear topologies, each with trade-offs in efficiency, noise, size, and cost. Pick the wrong one, and you’ll fight thermal issues, EMI failures, or blown BOM budgets. This voltage conversion guide covers the core principles engineers use to match a topology to a spec sheet.
What Determines Which Power Supply Topology You Need?
Three variables drive almost every decision: the voltage relationship (is Vout always below Vin, always above, or does the range straddle it — as with a battery sagging from 4.2 V to 3.0 V while the load needs a steady 3.3 V?); the efficiency and thermal budget (how much power can the design dissipate as heat?); and noise sensitivity (does an RF front end, ADC reference, or PLL need a clean rail, or can it tolerate switching noise?). Once these are pinned down, the topology choice narrows quickly.
Buck (Step-Down) Converters: The Default for Lowering Voltage
A buck converter switches current through an inductor and capacitor network to produce a stable output lower than the input, with no transformer and no isolation between input and output. Because the switch, inductor, and capacitor operate at the output current level rather than a higher circulating current, buck converters are inherently efficient — lower cost and higher efficiency than a buck-boost with the same component count. This is why buck is the default whenever the input rail (a 12 V bus, a 48 V battery pack, USB-PD) is reliably higher than the target rail.
When to reach for buck: point-of-load regulation from a higher-voltage bus (12 V → 3.3 V, 48 V → 5 V), digital core and MCU/SoC supplies that tolerate moderate ripple, or any design where Vin never dips below Vout.
Synchronous rectification (a low-RDS(on) MOSFET replacing the freewheeling diode) recovers efficiency, and multiphase interleaving reduces input ripple at higher current. LCSC stocks synchronous buck controllers and integrated FET buck regulators across many switching frequencies and current ratings, plus the shielded inductors and low-ESR capacitors these designs depend on.
Boost (Step-Up) Converters: Raising a Lower Rail
A boost converter stores energy in an inductor while the switch is on, then releases that energy — combined with the input — into the output capacitor when the switch turns off, producing an output higher than the input. This topology is also used in most Power Factor Control (PFC) sections of AC-DC power supplies.
Boost is unavoidable when the source voltage is inherently lower than the load — a single-cell Li-ion battery (2.5–4.2 V) powering a 5 V USB output, or a solar cell feeding a higher-voltage bus. Boost converters carry slightly higher conduction losses than buck converters because the inductor and switch current equals the input current rather than the output current. In practice, this shows up as a small efficiency gap: well-designed boost converters still commonly land in the 90–95% range, just a few points behind an equivalent buck.
Buck-Boost and SEPIC: When Vin Crosses Vout
The hardest case is when the input range straddles the desired output — common with batteries that start above regulation and discharge below it. If your input voltage range overlaps your output voltage, you are forced to use buck-boost — no shortcuts.
Two families handle this: a 4-switch buck-boost integrates buck and boost stages, switching seamlessly as Vin crosses Vout — efficient and compact, but uses more silicon than a single-mode converter. A SEPIC produces the same non-inverting result using two inductors and a series coupling capacitor, with an advantage over the buck-boost of inherent protection against output shorts.
LDO vs. Switching Regulator: When Efficiency Isn’t the Priority
Not every rail should be a switcher. LDOs remain the right choice whenever noise matters more than efficiency: linear regulators give excellent low-frequency noise performance because the pass device operates in the linear region with no high-frequency switching. For RF front ends, PLLs, and precision ADC references, that quiet output can mean the difference between meeting a noise floor and missing it.
The standard hybrid architecture uses a switching converter for the bulk of the voltage drop, followed by an LDO for final regulation and noise cleanup — the LDO’s power supply ripple rejection (PSRR) becomes paramount, filtering the switcher’s residual ripple without bulky LC filter stages. That noise benefit comes at a real efficiency cost: it’s not unusual for a design to accept roughly 60% LDO efficiency versus 90%+ for an equivalent buck, because the rail’s noise requirements leave no other option.
Buck vs. LDO vs. Buck-Boost: Quick Comparison
| Topology | Voltage Relationship | Typical Efficiency | Output Noise | Relative Complexity | Best For |
| Buck (step-down) | Vout < Vin | 90–95%+ | Moderate (switching ripple) | Low–Medium | POL digital rails, MCU/SoC supplies |
| Boost (step-up) | Vout > Vin | 90–95% | Moderate | Low–Medium | Single-cell battery to 5V/12V rails |
| Buck-boost / SEPIC | Vin straddles Vout | 85–93% | Moderate | Medium–High | Battery-powered systems, wide Vin |
| LDO (linear) | Vout < Vin (small drop) | 40–75% (drop-dependent) | Very low | Low | RF, ADC references, PLLs, sensor bias |
| Flyback (isolated) | Any, with galvanic isolation | 80–90% | Moderate | High | Offline AC-DC, safety-isolated rails |
Isolated Topologies: Flyback and Beyond
When galvanic isolation is required — offline AC-DC adapters, safety-rated industrial supplies, or any design where input and output grounds must never connect — a transformer-based topology is mandatory. Flyback is essentially a buck-boost isolated by using a transformer as the storage inductor, keeping parts count low. It’s the simplest, most common isolated topology for low-power applications, though best suited to lower output currents.
For non-isolated designs covering the same wide input range, SEPIC is a strong alternative: in automotive-grade comparisons, SEPIC generally achieves four per cent higher efficiency overall than flyback, reaching a peak of 92.7 per cent — the trade-off being a larger coupled inductor. For most engineers working within LCSC’s catalog, flyback remains the pragmatic default whenever true isolation is required.
Voltage Conversion Guide: A 5-Step Framework for Selecting Your Power Supply Architecture
- Map the voltage relationship. Vout outside the Vin range means a straightforward buck or boost; Vout inside the range means buck-boost or SEPIC.
- Set the efficiency and thermal budget. Calculate worst-case dissipation at your target efficiency and confirm it fits your thermal design.
- Check noise and PSRR requirements. RF, audio, or precision ADC loads call for an LDO post-regulator regardless of switching topology.
- Confirm isolation requirements. A mains-AC connection or safety standard requiring galvanic separation points to flyback.
- Validate with a power supply calculator. Confirm the topology holds up under real-world tolerances, not just the nominal case.
Power Supplies Calculator: Verify Before You Commit
Manufacturer design tools (TI’s WEBENCH, Analog Devices’ LTpowerCAD, and similar utilities) let you enter Vin range, Vout, and load current to generate a BOM, efficiency curve, and thermal estimate before committing to silicon — a fast way to catch a topology that fails at minimum Vin or maximum load.
Frequently Asked Questions
Q: Is a buck converter always more efficient than a boost converter?
Generally yes. Buck converters edge out boost converters because the switch and inductor carry only the output current rather than the higher input current a boost stage requires — though both commonly exceed 90% efficiency in well-designed circuits.
Q: When should I use an LDO instead of a switching regulator?
When output noise and PSRR matter more than efficiency, RF supplies, PLLs, ADC references, and other noise-sensitive rails. A common pattern pairs a switching regulator for bulk conversion with an LDO downstream for final cleanup.
Q: What’s the difference between buck-boost and SEPIC topologies?
Both handle Vin ranges that straddle the output. A 4-switch buck-boost integrates buck and boost stages in one IC. A SEPIC uses two inductors and a coupling capacitor for the same function, with a non-inverting output and inherent short-circuit protection.
Q: Do I need an isolated topology like a flyback for every AC-DC design?
Only when galvanic isolation is required by the application or a safety standard, most commonly offline mains-connected supplies. Non-isolated systems can use buck, boost, buck-boost, or SEPIC instead.
Sourcing Your Power Supply Design
Component selection determines whether a design hits its efficiency, noise, and thermal targets in practice. LCSC stocks buck and boost controllers, buck-boost and SEPIC controller ICs, low-noise LDOs, and flyback controllers alongside the shielded inductors, low-ESR capacitors, and power MOSFETs each topology needs — with competitive pricing, broad inventory, and direct integration into JLCPCB for board assembly.
Browse LCSC’s full range of DC-DC converter ICs, LDO regulators, and power inductors to source your next power supply design.