Flux vs. Solder Paste Guide for PCB Assembly

Flux is a chemical cleaning agent that removes oxidation and helps solder flow — it contains no metal and cannot form a joint on its own. Solder paste is flux plus microscopic solder alloy powder (typically 85–90% metal by weight), and it both deposits the metal and prepares the surface, making it the primary joining material in SMT reflow. 

Flux vs. Solder Paste: The Core Difference

Flux and solder paste are related but functionally distinct materials, and the difference comes down to one question: does the material supply the metal that forms the joint, or does it only prepare the surface for that metal?In other words, flux is a process enabler, while solder paste is a complete joining material.

Solder paste — also called pasta flux — is a gray, homogeneous mixture built for automated assembly. It consists of microscopic solder alloy particles suspended in a flux medium. It serves as the primary joining material in surface mount technology (SMT) reflow soldering, providing the metallic filler that forms the electrical and mechanical bond. At the same time, it supplies the chemical cleaning action needed to form that bond. The alloy is typically a leaded formulation such as Sn63Pb37 or a lead-free alloy such as SAC305 (Sn96.5Ag3Cu0.5), and the metal-to-flux ratio is usually 85–90% metal by weight, which directly affects printing performance and joint formation.

Flux type also matters for downstream cleaning requirements. No-clean flux minimizes post-soldering cleaning and is common in high-volume consumer electronics, while rosin or water-soluble flux is preferred where thorough post-soldering cleaning is required.

Attribute Flux (Flux Solder) Solder Paste (Pasta Flux)
Contains metal No Yes (typically 85–90% by weight)
Primary process Manual/hand soldering, wave soldering SMT stencil printing + reflow
Typical form Liquid, gel, or paste (no metal) Gray metal-flux paste
Shelf life Long, stable at room temperature Short — 3 to 6 months, refrigerated
Common standard IPC J-STD-004 IPC J-STD-005
Typical alloys used with it Sn63Pb37 wire, SAC305 wire Sn63Pb37, SAC305 pre-mixed in paste

How Much Does Flux and Solder Paste Cost Per Board?

Because flux and solder paste are priced and consumed so differently, a single “material cost” line item on a quote can be misleading. Estimating spend accurately means pricing each material against how it is actually used on the line, not against a flat per-board number.

Flux Cost Inputs

Plain flux is priced by volume (liquid/gel jars or bottles) and consumed in very small quantities per joint, so its cost per board is usually negligible compared to paste, labor, or components. The main cost drivers are:

  • Flux type and grade (no-clean vs. water-soluble vs. rosin-activated)
  • Container size and purchase volume (per-liter pricing drops sharply at bulk quantities)
  • Cleaning cost, if the flux residue requires post-soldering wash (adds equipment, solvent, and labor cost that no-clean flux avoids)

Solder Paste Cost Inputs

Solder paste pricing is driven by weight, alloy, and particle size (Type 3 vs. the finer Type 4/5/6 powders needed for fine-pitch parts). High-quality lead-free solder paste typically costs between $50 and $150 per kilogram, depending on alloy composition and particle size, and bulk lead-free paste can run well over a thousand dollars per kilogram at the high end, while small retail packs of leaded paste range from tens to hundreds of dollars. On top of the sticker price, refrigerated storage, disposal of expired jars, and hazardous-material shipping fees can inflate the effective cost of solder paste by an estimated 20–30%.

A practical way to estimate per-board material cost is:

Solder paste cost per board = (paste weight per board in grams ÷ 1000) × price per kilogram

Paste volume per board varies by design — a smartphone-class PCB with roughly 2,000 fine-pitch components may need only 0.5–1.0 grams of paste with an optimized printer, versus 1.0–1.5 grams with an older, less precise printer.

Worked example — mid-volume SMT board, lead-free SAC305 paste at $100/kg, 0.8 g of paste per board:

Input Value
Paste price $100 / kg
Paste used per board 0.8 g
Paste cost per board $0.08
Storage/handling overhead (25%) +$0.02
Effective paste cost per board ≈ $0.10
Flux (wave/touch-up, per board) ≈ $0.01–0.03
Combined flux + paste cost per board ≈ $0.11–0.13

Multiply the per-board figure by production volume to get a batch total, then add it back into the broader assembly quote alongside components, stencil, labor, and testing. Material cost — covering PCB substrate, solder paste, and flux — is only one line in the overall unit cost formula, where total assembly cost divided by the number of boards produced gives the final per-unit price. For most designs, flux and paste together represent a small fraction of total assembly cost, but at high volumes even a $0.02-per-board difference in paste efficiency compounds into thousands of dollars a month, which is why paste type, printer precision, and storage discipline are worth optimizing even though the unit price looks small.

Choosing the Right Material for the Job

  • Hand soldering, rework, and touch-up: use flux paired with solder wire — solder paste is not designed to be applied this way and can leave excessive residue or bridging if substituted.
  • Wave soldering (through-hole): flux is applied separately to the board before it passes through the molten solder wave.
  • SMT reflow assembly: solder paste is required, since it deposits both the metal and the flux precisely at each pad location via stencil printing.
  • High-reliability builds (medical, aerospace, military): water-soluble or rosin flux with thorough post-solder cleaning is typically specified over no-clean formulations.
  • High-volume consumer electronics: no-clean flux (in wire form or within paste) is standard, since it removes the cleaning step from the line.

Frequently Asked Questions

Is flux the same as solder paste?

No. Solder paste combines solder alloy and flux, enabling simultaneous metal deposition and surface preparation for surface-mount and reflow processes, while flux alone acts only as a chemical cleaning agent that removes impurities and aids solder flow, particularly during manual or wave soldering.

Can solder paste be used instead of flux for wave or through-hole soldering?

No — solder paste should not replace flux in wave soldering or through-hole soldering, since substituting it can leave excessive solder deposits, create bridging, and cause poor joint formation. Flux applied separately is the correct material for those processes.

Why does solder paste need refrigeration while flux typically does not?

Solder paste is a suspension of fine metal particles in a flux medium, and that suspension is unstable at room temperature over time — the particles can separate and the paste can dry out, shortening its usable shelf life to a few months. Plain flux contains no metal particles to separate, so it stores far longer under normal conditions.

What is the biggest hidden cost in solder paste versus flux?

Beyond the purchase price, refrigerated storage, disposal of expired material, and hazardous-material shipping fees are the main hidden costs, and together they can inflate the effective cost of solder paste by an estimated 20–30% above the quoted per-kilogram price. Flux does not carry these overheads to the same degree, since it is more chemically stable and easier to store and transport.

Does the choice of flux or paste affect PCB assembly compliance?

Yes. Flux and solder paste chemistries are covered by IPC standards (J-STD-004 for flux, J-STD-005 for paste), and choosing a formulation that is not qualified for the intended cleaning process or reliability class can affect certification and long-term joint reliability, particularly for RoHS-compliant, lead-free builds.

Find What You Need on LCSC

Whether you’re stocking up on flux for hand soldering and wave lines or sourcing solder paste for high-volume SMT reflow, LCSC carries a wide range of flux formulations (no-clean, water-soluble, rosin-activated) and solder paste alloys (Sn63Pb37, SAC305, and other lead-free options) in various pack sizes for prototyping through production runs. Before ordering, confirm alloy type, flux classification, and particle size against your component pitch and reliability requirements — these details drive both cost and yield more than any other line item on the quote. Browse LCSC’s soldering materials category to compare specifications, pricing, and stock availability side by side, and reach out to LCSC’s support team if you need help matching a material to your process.

More Discount Information
Connect With Us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30 am - 12 am, 1:30 pm - 10 pm
Monday - Friday, UTC/GMT +8
View Our Social Channels
Encrypted
Payment
© 2025 LCSC.COM All Rights Reserved.
粤ICP备17041818号 ISO/IEC