HUAXIN Analyzes Hall Effect Sensor Application

Hello everyone. This week, LCSC electronics supplier HUAXIN talks about the hall effect sensor. What is a hall effect sensor? And what role does it play in mobile phones?

What Is a Hall Effect Sensor?

A hall effect sensor (or simply a hall sensor) is a sensor that uses the hall effect to detect the presence and strength of a magnetic field. Actually, it is a type of magnetoelectric effect. An expert named Hall discovered this phenomenon in 1879 while studying the conducting mechanism of metals.

People who buy a cell phone like to study the parameters of the new cell phone, even if they have read it before buying it.

Most of the parameters above mobile phones are understandable, but some are half-understood. For example, the geek was a little confused when he saw the word “Hall Effect Sensor”.  What the hell is that? What does it do?

Well, as a non-science student and not an academic master, please allow me to simply understand the Hall effect as the interaction between “magnetic field” and “electricity”.

What Does it Do In mobile phones?

As Qian Zhongshu once said, “Eggs are delightful, but knowledge of the hen that lays them isn’t essential.” Not everyone has to comprehend its principle.

Its function  is a hall switch, which can make our mobile phone cases intelligent. The specific effect is to turn on the bright screen and close the black screen. There is nothing new because this function was often on flip mobile phones. Of course, it is also available on tablet computers.

In short, if a mobile phone has a hall effect sensor and a magnet built into the leather case, it can perform the above functions, and most smartphones currently have hall sensors.

Why does a mobile phone have this sensor, but the official does not publicize it? There are many reasons. First of all, when promoting, you only need to tell users that there is a “smart sleep” function. There is no need to introduce it specifically and professionally. If the introduction is not good, it will confuse users. And it is not as important as the CPU, camera, etc. So it is not necessary to promote this.

Also, Mobile phone brands are worried that the media/netizens will comment about radiation and health hazards, which will cause trouble for them.

Its prime function (also called a magnetic field sensor) is to detect the geomagnetic field and realize the compass function. The hall switch is just a supplementary function.

ABOUT HUAXIN

Established in 2003, Wuxi Huaxin Sheng Technology Co., Ltd. is a large-scale comprehensive enterprise. It specializes in R & D, production, testing, and sales of hall components. The company mainly produces advanced hall-effect integrated sensor products.​
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
SSL encrypted
payment
© 2024 LCSC.COM All Rights Reserved. 粤ICP备17041818号