Key Takeaways
- PCB assembly involves two primary component mounting technologies: SMT (surface-mount) and through-hole (THT), each with distinct process flows.
- Reflow soldering is the standard process for SMT components; wave soldering is the traditional process for through-hole components and selective SMT on the bottom side.
- The choice between SMT, through-hole, or mixed assembly affects board cost, cycle time, mechanical robustness, and component availability.
- Design for Manufacturing and Assembly (DFMA) principles applied during PCB layout directly reduce assembly defects, rework costs, and time-to-market.
- PCB surface finish (HASL, ENIG, OSP, ENEPIG) determines solderability, shelf life, and compatibility with fine-pitch components.
- Moisture Sensitivity Level (MSL) governs how long ICs can remain outside their moisture barrier bag before baking is required. MSL 1 is unlimited; MSL 3 requires use within 168 hours of opening.
1. The PCB Assembly Process: An End-to-End Overview
A fully assembled PCB — called a PCBA (Printed Circuit Board Assembly) — starts as a bare board and goes through a series of controlled manufacturing steps before it becomes a functional electronic module. Here is the complete process sequence for a standard SMT assembly run:
Step 1: Incoming Inspection and Kitting
Before assembly begins, the bare PCBs and all components are inspected. The PCB is checked for warpage, surface finish quality, and dimensional accuracy. Components are verified against the Bill of Materials (BOM) — part numbers, package codes, polarity, and quantity. This kitting stage identifies substitutions, shortages, or counterfeit components before they reach the line.
Step 2: Solder Paste Application
A stainless steel or nickel-alloy stencil — laser-cut to match the PCB’s pad geometry — is aligned over the board. A squeegee draws solder paste (a mixture of tin-silver-copper alloy particles suspended in flux) across the stencil, depositing a precise volume of paste onto each SMD pad. Aperture size in the stencil is typically 1:1 with the pad, or slightly reduced for fine-pitch components to prevent bridging.
Critical parameter: solder paste volume consistency determines joint quality. Too little paste causes insufficient joints and cold solder; too much causes bridging between adjacent pads. Automated Solder Paste Inspection (SPI) systems verify paste volume and alignment after every stencil print.
Step 3: SMT Component Placement
The paste-printed board moves to a pick-and-place machine, which uses vacuum nozzles to pick components from tape-and-reel, tray, or tube feeders and place them precisely onto the pasted pads. Modern pick-and-place machines achieve placement accuracies of ±25 μm at speeds of 30,000 to 100,000 components per hour.
Step 4: Reflow Soldering
The populated board passes through a reflow oven — a conveyor furnace with multiple temperature zones. The thermal profile brings the board through four stages: preheat (activates flux, drives off volatiles), soak (equalises temperature across the board), reflow (melts the solder paste, forming solder joints), and cooling (solidifies the joints with the correct microstructure).
Standard lead-free solder (SAC305: 96.5% Sn, 3% Ag, 0.5% Cu) has a melting point of approximately 217°C. A typical lead-free reflow profile peaks at 245–260°C with the time above liquidus (TAL) controlled to 30–90 seconds.
| Reflow Zone | Temperature Range | Duration | Purpose |
| Preheat | 25°C → 150°C | 60–120 s | Activates flux; evaporates solvents; prevents thermal shock |
| Soak | 150°C → 180°C | 60–120 s | Equalises temperature across the board; flux activates and cleans pad surfaces |
| Reflow | 217°C → 245–260°C peak | 30–90 s above liquidus | Solder melts, wets pads and component leads, forms metallurgical joint |
| Cooling | 260°C → < 100°C | Controlled ramp | Solidifies joints with correct grain structure; too fast causes brittle joints |
Step 5: Automated Optical Inspection (AOI)
After reflow, every board passes under an AOI system — a camera array that compares the assembled board against a reference image. AOI detects missing components, wrong polarity, lifted leads, solder bridges, insufficient solder, and tombstoning (a defect where a small passive stands on end due to unequal reflow on both pads).
Step 6: Through-Hole Insertion (if applicable)
For mixed-technology boards, through-hole parts are inserted after SMT reflow. Axial and radial leaded components, connectors, and large electrolytics are inserted by hand or automated insertion machines, then soldered by wave or selective soldering.
Step 7: Wave or Selective Soldering
Through-hole components are soldered by passing the underside of the board over a wave of molten solder. The board is first fluxed (spray or foam flux), preheated, then passed over the solder wave. Selective soldering uses a small localised solder nozzle to solder specific through-hole areas on mixed boards without exposing SMT components to the wave.
Step 8: Electrical Testing
Functional test (FCT) powers up the assembled board and exercises its functionality using test fixtures or boundary scan (JTAG). In-circuit test (ICT) uses a bed-of-nails fixture to verify component values, solder joint continuity, and shorts at the component level. Flying probe testing is a flexible, fixtureless alternative for low-volume or prototype assemblies.
2. SMT vs. Through-Hole: Choosing the Right Assembly Method
| Factor | SMT (Surface-Mount) | Through-Hole (THT) |
| Component size | Much smaller; 0201, 0402, QFN, BGA | Larger leads and bodies |
| Assembly speed | High — fully automated pick-and-place | Slower — manual or semi-automated insertion |
| Mechanical strength | Moderate — solder joints on surface only | High — leads clinched through board |
| Vibration resistance | Lower without underfill | Excellent — ideal for automotive, industrial |
| Best for | High-volume consumer, IoT, mobile, computing | Connectors, power components, harsh environments |
Use through-hole when: high-current power connectors and terminal blocks require mechanical pull-out strength; components subject to repeated mating cycles; large electrolytics and inductors where the mass would stress SMT pads; or environments with high vibration, shock, or thermal cycling that would fatigue SMT solder joints.
3. PCB Surface Finishes: Solderability, Shelf Life, and Application
| Surface Finish | Process | Shelf Life | Fine-Pitch | Best Application |
| HASL | Board dipped in molten solder; air-levelled | 12 months | No — uneven | General purpose; low-cost boards |
| ENIG | Electroless Ni then Immersion Au | 12 months | Yes — flat | Fine-pitch QFN, BGA, wire bonding |
| OSP | Organic coating on bare copper | 6 months | Yes | High-volume SMT; cost-sensitive |
| ENEPIG | Ni, Palladium, then Au | 12 months | Yes — premium | Wire bonding pads; gold stud bumping |
| Immersion Silver | Silver deposited on copper | 6–12 months | Yes | RF boards; press-fit connectors |
ENIG vs. HASL: ENIG is the default choice for any board with QFN, BGA, or other fine-pitch components, because its flat, consistent surface enables reliable solder paste deposition and joint formation. HASL’s uneven surface causes paste volume variation on small pads. However, ENIG costs 20–40% more than HASL and requires careful handling to prevent ‘black pad’ — a corrosion failure mode at the nickel-gold interface caused by hypercorrosion during gold deposition.
4. Moisture Sensitivity Level (MSL)
ICs and other plastic-packaged components absorb atmospheric moisture over time. During reflow, this moisture vaporises explosively and can crack the package. MSL ratings (IPC/JEDEC J-STD-020) define how long a component can remain outside its moisture barrier bag before baking is required. MSL 1 components are unlimited; MSL 3 must be used within 168 hours of opening.
5. Design for Manufacturing and Assembly (DFMA) — Rules That Save Money
- Fiducial marks: Place at least 3 fiducial marks (bare copper circles, typically 1 mm diameter) on the PCB for pick-and-place machine vision alignment. Global fiducials go at board corners; local fiducials go near fine-pitch ICs.
- Component clearance: Maintain a minimum 0.2 mm clearance between adjacent SMD component bodies. Components placed too close interfere with nozzle access and create solder bridging risk.
- Uniform pad design: Use IPC-7351 standard land patterns. Non-standard pad sizes cause paste volume errors and unreliable joints.
- Consistent component orientation: Orient all polarised components (electrolytic capacitors, diodes, ICs) consistently. This dramatically reduces placement errors and inspection time.
- Thermal relief vias: Essential on large copper pads. Without them, the copper plane acts as a heat sink and prevents the pad from reaching reflow temperature.
- Panel design: For production volumes, arrange multiple PCBs in a panel (array) with V-score or tab-routed break lines, fiducials, and tooling holes in the panel frame. This enables efficient automated assembly.
6. Component Sourcing for PCB Assembly
The BOM Hierarchy: Primary, Second Source, and Approved Equivalents
- Primary part: Your first-choice component, fully characterised and qualified to your design.
- Second source: An alternative manufacturer’s equivalent part with identical pin-out and electrical parameters. Always identify a second source before production — primary parts go on allocation.
- Approved equivalent: A functionally equivalent part that may require a minor schematic or footprint change. Requires engineering sign-off before substitution.
What to Check Before Ordering Components
- Package code match: Verify the exact package (e.g., SOT-23-5 vs. SOT-23-3 are different footprints).
- Temperature range: Industrial (−40°C to +85°C) vs. commercial (0°C to +70°C) ratings matter for reliability.
- MSL rating: Check moisture sensitivity for ICs — MSL 3 or higher requires baking before assembly.
- RoHS compliance: Verify lead-free compliance for markets that require it (EU, China, and most global markets).
Quick Selection Guide: PCB Assembly Process in 60 Seconds
- High-volume SMT design (IoT, consumer electronics, computing) → Full SMT; pick-and-place + reflow oven; ENIG for fine-pitch, HASL for general use
- High-current connectors or components subject to repeated mating cycles → Through-hole for mechanical strength; wave or selective soldering
- Mixed SMT + through-hole (most industrial boards) → SMT top-side reflow first, then through-hole insertion + wave or selective soldering on bottom
- Fine-pitch QFN, BGA, or components with pads < 0.5 mm pitch? → ENIG surface finish mandatory; stencil aperture reduce by 10–15% to prevent bridging
- Low-volume prototype or NPI → Flying probe test (no fixture NRE); OSP or HASL finish; manual through-hole assembly acceptable
- IPC Class 3 required (aerospace, medical, military) → 100% AOI + X-ray inspection for BGAs; IPC/WHMA-A-620 Class 3 workmanship standard; hi-pot testing at 2× rated voltage
- BOM includes MSL 3+ ICs → Bake components per IPC/JEDEC J-STD-033 before assembly; use within 168 hours of opening moisture barrier bag
Frequently Asked Questions
What is the difference between PCB assembly and PCB manufacturing?
PCB manufacturing (fabrication) produces the bare board — drilling, laminating, plating, and applying solder mask. PCB assembly (PCBA) is the subsequent process of populating the bare board with components. Many contract manufacturers offer both services under one roof, simplifying supply chain management.
Can I mix SMT and through-hole components on the same board?
Yes, and most production boards do. The typical process is: SMT components on the top side are placed and reflowed first, then through-hole components are inserted and soldered by wave or selective soldering. Bottom-side SMT components that must survive wave soldering are bonded with adhesive before wave soldering to prevent them washing off the wave.
What causes tombstoning and how do I prevent it?
Tombstoning occurs when a small passive component (0402, 0201) stands vertically on one pad during reflow. It is caused by unequal solder paste volumes or unequal thermal mass on the two pads, causing one end to melt and wet before the other. Prevention: use symmetric pad designs per IPC-7351, ensure uniform paste deposition with SPI, and keep small passives away from large thermal mass components that create temperature gradients across the pad pair.
Why does my board need a specific IPC class?
IPC-A-610 classifies PCBAs into three classes based on the consequences of failure.
Class 1 applies to general electronics like toys and consumer goods with relaxed workmanship standards.However, Class 2 is designated for dedicated service electronics, such as industrial instrumentation, requiring higher reliability. Finally, Class 3 represents high-performance electronics for aerospace, medical, and military sectors, which must adhere to the strictest standards.
Conclusion: Understanding Assembly Makes You a Better Designer
PCB assembly is not a black box that happens after you send your Gerber files. It is a precision manufacturing process with dozens of variables, each of which you can influence through thoughtful design decisions. Knowing how solder paste is deposited, how reflow profiles affect joint quality, why surface finish matters for fine-pitch components, and how DFMA principles reduce defects gives you the vocabulary and insight to design boards that are not just electrically correct, but production-ready.
Find What You Need on LCSC
LCSC Electronics provides the component depth and datasheet transparency you need to build a bulletproof BOM for your next PCB assembly run — with MSL ratings, RoHS status, AEC-Q100 qualification filters, and real-time stock availability.