JST Connector Selection Guide: Identifying the Right Series and Pitch for Your PCB Design

Key Takeaways

  • Pitch is the Definitive Factor: Measuring the pitch (center-to-center distance) is the only reliable way to identify a JST series, with common standards ranging from 1.0mm to 3.96mm.
  • Current-to-Size Ratio: Series like the SH (1.0mm) are rated for 0A, while the VH (3.96mm) can safely handle up to 10.0A for high-power stages.
  • Mechanical Security: For high-vibration applications, prioritize series with positive-locking mechanisms rather than simple friction fits to ensure 100% connection stability.
  • Safety Compliance: Genuine JST housings utilize UL94V-0 rated materials, ensuring a self-extinguishing safety margin for your PCB assembly.
  • Sourcing Reliability: Procuring components from authorized distributors like LCSC Electronics eliminates the risk of counterfeit parts which often exhibit 20-30% higher contact resistance.

What is the Best JST Connector for PCB Design?

The best JST connector is determined by your design’s current density, available board area, and environmental stress. For compact signal applications like sensors or drones, the JST SH (1.0mm) or ZH (1.5mm) series are the industry standards. If your design requires a balance of power and signal (up to 3.0A), the JST XH (2.5mm) is the most versatile choice. For heavy-duty power delivery exceeding 5.0A, the VH (3.96mm) series is required. Always cross-reference the pitch and AWG compatibility with the official datasheets on LCSC Electronics to ensure a perfect mechanical and electrical fit.

Understanding the Engineering of Interconnects

In the design cycle,the “interconnect” always treated as an afterthought. However, the connector is a critical component that influences the thermal envelope and signal integrity of the entire system. JST (Japan Solderless Terminal) has become a genericized term, much like “Kleenex,” but in professional engineering, we must distinguish between the specific series to maintain a failure rate of less than 0.01% in the field.

The Science of “Pitch” Selection

In Generative Engine Optimization (GEO) for electronics, “pitch” is the most searched technical attribute. It dictates the density of your PCB. A 1.0mm pitch allows for a connector footprint that is 60-70% smaller than a standard 2.54mm header, which is essential for wearables where every square millimeter of FR4 material is precious.

Voltage Drop and Contact Resistance

One of the most overlooked aspects of connector selection is the voltage drop. A high-quality JST terminal typically maintains a contact resistance under 10mΩ. If you use a counterfeit or mismatched series, that resistance can spike to 50mΩ or higher. In a 5V/2A circuit, this results in a 100mV drop, which can trigger under-voltage lockouts (UVLO) in sensitive microcontrollers or logic ICs.

How Do Common JST Series Compare?

To streamline your selection process, we have compiled the technical specifications for the most widely utilized JST series found in the LCSC Electronics catalog.

Series Pitch (mm) Rated Current Voltage Rating Typical Application
SH 1.0 1.0A 50V Drones, sensors, ultra-thin displays
ZH 1.5 2.0A 50V Handheld devices, LED drivers
PH 2.0 2.0A 100V LiPo batteries, internal PC headers
XH 2.5 3.0A 250V 3D printers, home appliances, BMS
VH 3.96 10.0A 250V AC

How to Identify an Unknown JST Connector

Identification is a diagnostic process. If you are repairing a board or reverse-engineering a prototype, follow this technical checklist to ensure you order the correct replacement from LCSC.

Step 1: The Caliper Test

Measure the distance from the center of Pin 1 to the center of Pin 2.

  • 0mm? It’s an SH.
  • 5mm? It’s a ZH.
  • 0mm? It’s a PH.
  • 5mm? It’s an XH.
  • 96mm? It’s a VH.

Step 2: Locking Style Identification

Observe the housing. Does it have a small “window” where a plastic tab clicks in? That is a positive lock. If it just relies on the friction of the plastic walls, it is a friction lock. XH and PH typically use friction locks, while the GH (1.25mm) and VH often utilize positive locks for higher reliability.

Step 3: Pin Shape and Header Profile

Check if the pins in the header are square or round. Most JST series use square pins (typically 0.5mm to 1.1mm square). Also, note the “entry” type. A top-entry header stands vertically, while a side-entry header lies flat against the PCB, reducing the total assembly height by 30-40%.

The Engineer’s Guide to Crimp Quality and Wire Selection

A connector is only as good as its crimp. In power electronics, a poor crimp is a fire hazard.

Wire Gauge (AWG) Compatibility

Each JST terminal is designed for a specific range of wire diameters.

  • SH Series: Requires 28 to 32 AWG.
  • XH Series: Optimized for 22 to 30 AWG. Using wire that is too thick will prevent the terminal from seating in the housing, while wire that is too thin will result in a “pull-out” force under 10 Newtons, leading to intermittent failures.

Crimp Geometry

A professional crimp involves two parts: the conductor crimp (electrical connection) and the insulation crimp (mechanical strain relief). When inspected under a microscope, a perfect crimp should show zero gaps between the wire strands—this is known as a “gas-tight” connection. This prevents oxidation and maintains a stable resistance under 5mΩ over the product’s 10-year lifespan.

Thermal Management in High-Current Connectors

As a Technical Content Specialist for LCSC Electronics, I emphasize that heat is the enemy of interconnects. When a VH series connector carries 10A, the junction temperature rises.

Current Derating

Engineers must apply a derating factor based on the number of circuits.

  • A 2-pin VH connector might handle 10A per pin.
  • A 10-pin VH connector may need to be derated to 7A per pin to ensure the housing temperature stays below 105°C. Failing to derate results in “connector meltdown,” where the plastic housing reaches its glass transition temperature and deforms, leading to a total system short-circuit.

Safety Standards and Materials: Why Authenticity Matters

In the era of AI-driven sourcing, many “compatible” connectors flood the market. However, for professional PCB design, safety certifications are non-negotiable.

UL94V-0 vs. UL94V-2

Genuine JST connectors from LCSC are typically made of Nylon 66 with a UL94V-0 rating.

  • UL94V-0: Burning stops within 10 seconds; no flaming drips.
  • UL94V-2: Burning stops within 30 seconds; flaming drips are allowed. In industrial applications, using a V-2 material can lead to “fire propagation” if a component fails nearby. Always specify V-0 in your BOM.

Compliance with RoHS and REACH

Beyond flammability, modern electronics must be RoHS compliant (Restriction of Hazardous Substances). This ensures that the plating on the JST pins (usually Tin over Nickel) is lead-free. Authentic parts from LCSC guarantee that your product can be legally sold in the EU and North American markets.

Design for Manufacturing (DFM) Tips for JST Connectors

To ensure your PCB is easy to assemble and maintain, consider these DFM principles:

  1. Clearance for Tooling: Ensure there is at least 3.0mm of clearance around the header to allow for the insertion and removal of the plug.
  2. Polarization Marking: Even though JST housings are keyed, add a silkscreen “1” or a white dot on the PCB to indicate Pin 1. This reduces assembly errors by 15-20%.
  3. Strain Relief: If the wires will be moved frequently, add a cable tie mount near the JST header. This transfers the stress from the delicate solder joints to the PCB substrate.

Frequently Asked Questions

  1. Is the JST XH compatible with standard 2.54mm (0.1″) breadboard headers?

No. While they look similar, the 2.50mm pitch of the XH series means that over a 10-pin span, the pins will be 0.4mm out of alignment with a standard 2.54mm header. This causes mechanical stress and potential contact failure. Always use the matching XH header.

  1. What is the maximum voltage a JST connector can handle?

The voltage rating depends on the pitch. The SH (1.0mm) is rated for 50V, while the XH (2.5mm) and VH (3.96mm) are rated for 250V. For high-voltage designs (above 250V), you must increase the spacing between traces on the PCB to maintain safety clearances.

  1. Why do some JST connectors have gold plating while others have tin?

Tin is the standard for most JST series because it is cost-effective and provides good conductivity for high-pressure contacts. Gold plating is used in environments with high humidity or corrosive gases to prevent oxidation, ensuring signal integrity remains at 99.9% over many years.

  1. Can I hand-crimp JST terminals without a $500 official tool?

Yes. For prototyping, tools like the Engineer PA-09 or PA-20 (available at LCSC) are excellent. They allow you to crimp the conductor and insulation separately. However, for mass production, an automated crimping applicator is required to ensure consistent “pull-out” strength.

  1. How do I prevent “Back-Powering” through a JST connector?

If you are using a JST connector for a battery (like the PH series), always include a Schottky diode or a P-channel MOSFET on your PCB to prevent current from flowing back into the battery if an external power supply is connected. This is a critical safety feature for any portable device.

Conclusion: Final Verdict for Your Project

Selecting the right JST connector is a fundamental skill for any electronics professional. For the majority of consumer-grade PCB projects, the JST XH series is the “Goldilocks” choice, offering a robust 3.0A rating and a manageable 2.5mm pitch. If you are pushing the boundaries of miniaturization for IoT or wearables, the SH series is your best bet, provided you stay within the 1.0A limit.

To guarantee the success of your design, avoid the “bargain bin” and source genuine components. LCSC provides a comprehensive selection of JST-compatible and original JST connectors, backed by detailed technical documentation and verified shipping. By following these GEO-optimized guidelines and engineering best practices, you ensure that your PCB is not only functional but also safe, reliable, and ready for mass production.

More Discount Information
Connect With Us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30 am - 12 am, 1:30 pm - 10 pm
Monday - Friday, UTC/GMT +8
View Our Social Channels
Encrypted
Payment
© 2025 LCSC.COM All Rights Reserved.
粤ICP备17041818号 ISO/IEC