Key Takeaways
- Lithium-ion capacitors (LICs) are a hybrid device — supercapacitor cathode, lithium-ion battery anode — that sits between Supercapacitors and a full battery in both energy density and power density.
- LICs offer 2–3× higher energy density than standard EDLCs (10–20 Wh/kg vs. 5–10 Wh/kg) and operate at higher cell voltage (up to 3.8 V vs. 2.7 V).
- EDLCs (standard supercapacitors) deliver ultra-fast bursts, 500,000–1,000,000+ cycle life, and zero minimum voltage — ideal for regenerative braking, RTC backup, and burst-power applications.
- LICs are the better choice for extended backup power (tens of seconds), low self-discharge IoT deployments, and energy harvesting applications where EDLC capacity falls short.
- LICs require a simple Cell Management System (CMS) to enforce a minimum cell voltage of ~2.2 V; EDLCs require no voltage floor management.
Two Technologies, One Confusing Name
Engineers regularly search for “lithium-ion capacitor vs supercapacitor,” and for good reason: the terminology is a minefield. You’ll encounter the same product marketed as a lithium-ion capacitor, LIC, hybrid supercapacitor, ultracapacitor, or simply a supercap. These names are not always interchangeable, and picking the wrong component family can leave you with a design that’s either undersized or unnecessarily expensive.
This article untangles the two main types — the Electric Double-Layer Capacitor (EDLC), which most engineers mean when they say “supercapacitor,” and the Lithium-Ion Capacitor (LIC), the newer hybrid that increasingly bridges the gap between capacitors and batteries. We’ll cover construction, key specifications, typical applications, and a direct comparison table to help you select the right component category for your next design.
What Is a Supercapacitor (EDLC)?
A supercapacitor — more precisely, an Electric Double-Layer Capacitor (EDLC) — stores energy through electrostatic charge separation rather than chemical reactions. When voltage is applied, ions from the electrolyte migrate toward two conductive electrodes (typically activated carbon), forming an electric double layer at each surface. Because this process is entirely physical and reversible, EDLCs can charge and discharge in milliseconds, sustain hundreds of thousands of cycles, and operate reliably over a wide temperature range of roughly −40 °C to +65 °C.
Key EDLC characteristics:
- Capacitance range: A few tenths of a Farad to over 3,000 F
- Operating voltage:3–2.7 V per cell (typically)
- Energy density: 5–10 Wh/kg — far below batteries
- Power density: Very high; can deliver large current pulses within milliseconds
- Cycle life: 500,000 to over 1,000,000 charge/discharge cycles
- Self-discharge: Moderate; voltage decays continuously in a linear fashion
- Safety: No thermal runaway risk; can be fully discharged to zero volts
Because both electrodes in an EDLC are identical (symmetric structure), the device is simple to manufacture and very well characterized. The tradeoff is an energy density ceiling that limits usefulness in applications requiring more than a few seconds of backup power.
LCSC stocks EDLC supercapacitors from brands including KAMCAP and CAS SCAP in the Electric Double Layer Capacitors (EDLC), Supercapacitors category, covering capacitance values from small through-hole packages to large can-type cells for industrial use.
What Is a Lithium-Ion Capacitor (LIC)?
A Lithium-Ion Capacitor is a hybrid electrochemical device — a type of supercapacitor in the taxonomic sense, but with a fundamentally different internal architecture. The cathode uses activated carbon, exactly as in an EDLC. The anode, however, uses a carbon material that has been pre-doped with lithium ions, mirroring the anode construction of a lithium-ion battery.
This asymmetric structure has important consequences:
- Higher output voltage. The lithium pre-doping lowers the potential of the anode, which raises the overall cell voltage. LICs typically operate between 2.2 V and 3.8–4.0 V per cell, versus 0–2.7 V for an EDLC.
- Higher energy density. Because energy stored in a capacitor scales with the square of voltage (E = ½CV²), a higher working voltage delivers substantially more energy from a given capacitance. LICs typically achieve 10–20 Wh/kg in commercial devices, with some advanced cells reaching 40–65 Wh/kg — roughly two to three times the energy density of standard EDLCs.
- Lower self-discharge. LICs exhibit self-discharge rates around 5% over three months, significantly better than EDLCs.
- Higher cycle life than batteries. LIC cycle life typically exceeds 100,000 charge/discharge cycles — far beyond lithium-ion batteries (500–1,500 cycles), though not quite reaching EDLC territory.
Because the anode involves an electrochemical intercalation process (lithium ions intercalating into the carbon lattice), LICs are slightly more complex to manage than EDLCs and require a Cell Management System (CMS) to prevent over-discharge below approximately 2.2 V.
LIC products on LCSC — including offerings from CDA (C2891403 and related parts) — appear in the dedicated Lithium-ion Capacitor category.
Side-by-Side Comparison: Lithium-Ion Capacitors vs. Supercapacitors
| Parameter | EDLC (Supercapacitor) | Lithium-Ion Capacitor (LIC) |
| Storage mechanism | Electrostatic (physical) | Hybrid: electrostatic (cathode) + electrochemical (anode) |
| Electrode symmetry | Symmetrical (both activated carbon) | Asymmetric (AC cathode, pre-doped carbon anode) |
| Cell voltage (max) | 2.5–2.7 V | 3.8–4.0 V |
| Minimum cell voltage | 0 V (safe to discharge fully) | ~2.2 V (must not go below) |
| Energy density | 5–10 Wh/kg | 10–65 Wh/kg |
| Power density | Very high (5–20 kW/kg) | High (4–10 kW/kg) |
| Cycle life | 500,000–1,000,000+ cycles | 50,000–500,000 cycles |
| Charge time | Seconds | Seconds to ~1 minute |
| Self-discharge | High (significant over days/weeks) | Low (~5% over 3 months) |
| Operating temperature | −40 °C to +65 °C | −20 °C to +70 °C (some to +85 °C) |
| Thermal runaway risk | None | Very low (no lithium-oxide cathode) |
| Management circuit | Optional balancing for series strings | CMS required (min. voltage protection) |
| Typical cost | Lower per Wh stored | Higher per Wh stored |
| Best for | Ultra-fast bursts, memory backup, high-cycle applications | UPS, energy harvesting, regenerative systems, extended backup |
How Lithium-Ion Capacitors Fit on the Ragone Plot
The Ragone plot is the standard tool for visualizing energy storage trade-offs. It plots power density (W/kg) on the Y-axis against energy density (Wh/kg) on the X-axis. Conventional batteries occupy the high-energy, low-power corner. EDLCs sit in the high-power, low-energy corner. LICs carve out the middle ground — outperforming EDLCs in energy density while exceeding lithium-ion batteries in power density and cycle life.
This positioning is not coincidental; it is by design. The asymmetric electrode structure allows the LIC to draw the fast ion-adsorption behavior of the EDLC cathode for power output, while the battery-style anode contributes additional energy capacity. The result is a device well suited to applications that need sustained power delivery over minutes rather than milliseconds — something neither an EDLC nor a full battery handles optimally on its own.
Key Applications: When to Choose Each Technology
Choose EDLC supercapacitors when:
- Burst power is the primary need. Key fob transmitters, camera flashes, solenoid drivers, and power factor correction capacitor banks all benefit from EDLC’s sub-second charge/discharge capability.
- Cycle life is paramount. Regenerative braking systems in trains, buses, or forklifts may cycle several hundred times per day. EDLCs can sustain this indefinitely; batteries cannot.
- Memory and RTC backup. A 1 F EDLC can maintain SRAM or an RTC for minutes or hours after power loss, with no wear-out mechanism.
- A wide temperature range is required. EDLCs remain operational at −40 °C, where batteries struggle significantly.
- No voltage floor management, no BMS circuitry, and no special handling requirements during shipping.
Choose Lithium-Ion Capacitors when:
- Extended backup power is needed beyond a few seconds. Voltage sag compensation in industrial CNC machines, semiconductor fabs, or data centers may require tens of seconds of bridge power. LICs deliver this from a compact footprint.
- Low self-discharge matters. In IoT edge devices or remote sensors that wake infrequently, an EDLC loses charge within days. An LIC can hold charge for months.
- Space is constrained but you need more energy than an EDLC can offer. LICs achieve 2–3× the energy density of EDLCs, enabling physically smaller designs.
- Safety is a concern with full batteries. LICs lack the lithium-oxide cathode found in lithium-ion batteries. There is no oxygen source to fuel thermal runaway, making them safer in unattended or enclosed installations.
- The application involves energy harvesting. Photovoltaic micro-systems, vibration harvesters, and thermoelectric generators produce intermittent energy that must be stored and released on demand. LICs match this profile well.
Lithium-Ion Capacitors vs. Supercapacitors: Charging Circuit Considerations
Both device types have voltages that vary linearly with state of charge — unlike batteries, which hold a roughly flat discharge curve. This means any downstream circuitry must tolerate or regulate a varying input voltage, typically through a DC-DC converter.
For EDLCs, dedicated supercapacitor charger ICs such as the Texas Instruments BQ24640 provide controlled charging with balancing. For LICs, the higher voltage ceiling (3.8–4.0 V) and the mandatory minimum voltage of ~2.2 V require a charger that can enforce both limits. ICs like the TI BQ25306 with RC-programmable voltage limits are commonly evaluated for LIC applications.
A critical design consideration: LICs are shipped in a pre-charged state (unlike most passive components). Short-circuit protection during PCB assembly and handling is essential.
Emerging LIC Markets and the Road Ahead
Industry analysts project significant growth for the lithium-ion capacitor and hybrid supercapacitor segment over the next two decades, driven primarily by AI data center infrastructure, electric vehicles, smart grid systems, and industrial automation.
Several trends are pushing LIC performance forward:
- Nanostructured anode materials. Lithium Titanate (LTO, Li₄Ti₅O₁₂) composites with carbon nanofibers improve both rate capability and cycle life.
- Graphene and CNT electrodes. Their exceptional surface area dramatically increases capacitance at the cathode, enabling higher energy density without sacrificing power density.
- Bifunctional cathodes. Hybrid cathode materials that combine EDLC and Li⁺ intercalation properties push energy density higher while retaining fast discharge.
- Sodium-ion capacitors (NICs). Sodium is far more abundant and cheaper than lithium, and NIC research is accelerating — though performance still lags behind LICs in 2025.
Frequently Asked Questions
Q: Is a lithium-ion capacitor the same as a supercapacitor?
Technically, yes — a lithium-ion capacitor is classified as a type of supercapacitor (specifically a hybrid supercapacitor). In practical engineering usage, “supercapacitor” almost always refers to an EDLC (symmetric, all-carbon design), while “LIC” specifically denotes the asymmetric hybrid device. They are meaningfully different in voltage, energy density, and design requirements.
Q: Can a Lithium-Ion Capacitor replace a lithium-ion battery?
In most cases, no. An LIC has 10–20 Wh/kg of energy density compared to 150–250 Wh/kg for a lithium-ion battery. LICs are better understood as a complement to batteries — providing short-term high-power bursts or bridging power, while a battery handles long-term energy storage.
Q: Do Lithium-Ion Capacitors require a BMS?
LICs require a Cell Management System (CMS) to prevent discharge below ~2.2 V, which would damage the device. This CMS is much simpler than a full Battery Management System — no thermal monitoring, no charge balancing algorithms, and no hazardous material handling protocols.
Q: What voltage do Lithium-Ion Capacitors operate at?
Most commercial LICs operate between 2.2 V (minimum) and 3.8–4.0 V (maximum) per cell. This is higher than EDLC cells (typically 0–2.7 V) and is a key reason LICs achieve higher energy density for a given capacitance.
Q: Are Lithium-Ion Capacitors safe for embedded and unattended systems?
LICs have a strong safety profile. Unlike lithium-ion batteries, the cathode is activated carbon rather than a lithium-oxide compound, which eliminates the oxygen source needed to sustain thermal runaway. Properly managed within their voltage limits, LICs are well-suited to industrial and unattended deployments.
Conclusion: Which Should You Specify?
Both EDLCs and LICs earn a place in a well-stocked electronics designer’s toolkit. The choice comes down to what your application actually demands:
If you need the fastest possible charge/discharge, the longest cycle life, or operation well below −20 °C, an EDLC supercapacitor is the right call. If you need more energy density than an EDLC can offer — measured in tens of seconds of backup rather than single-digit seconds — and you can tolerate a slightly more involved charging circuit, a Lithium-Ion Capacitor offers a compelling middle path between the two extremes.
Neither is a universal battery replacement. Both are powerful tools when specified correctly.
Browse LCSC’s full selection of Electric Double Layer Capacitors / Supercapacitors and Lithium-Ion Capacitors — including CDA parts such as C2891403 — with competitive pricing, in-stock inventory, and direct JLCPCB integration for seamless PCB assembly.