IC Basics Explained: How Do Integrated Circuits Work?

An integrated circuit (IC) is a complete electronic circuit. It integrates transistors, resistors, capacitors, and wiring onto a single piece of semiconductor material, usually silicon. Today, a modern IC packs millions or billions of transistors onto a chip just a few millimeters wide. Consequently, it can switch signals billions of times per second to perform logic or shape analog waveforms.

However, the real story behind this definition is much deeper. It explains how a flat piece of sand becomes a powerful processor. This journey spans crystal growth, photolithography, and transistor physics. Furthermore, it involves critical packaging decisions that affect every subsequent PCB design. Here is how it all fits together.

Key Takeaways — How Integrated Circuits(IC) Work

  • An IC builds millions to billions of components onto one piece of silicon. Therefore, it avoids the need to wire separate parts together.
  • The fabrication process grows a pure silicon crystal and slices it into wafers. After that, workers build up to 30+ patterned layers using photolithography, etching, and doping.
  • Most digital ICs work by switching CMOS transistors on and off in combinations called logic gates. In contrast, analog ICs shape continuous voltage and current.
  • Engineers classify ICs by signal type, such as digital, analog, or mixed-signal. Then, they package them into forms like DIP, SOIC, QFN, or BGA based on pin count, size, and thermal needs.
  • In 2026, leading-edge progress is shifting toward chiplet packaging. This happens because gains per new node are slowing down while wafer costs rise.

What Is an Integrated Circuit(IC), Exactly?

Every IC starts as a design schematic. This schematic describes how to arrange transistors, interconnects, and passive elements to perform a function. For example, the design might amplify a signal, store a bit, or execute an instruction. Next, engineers translate that design into a physical layout. A manufacturing facility then builds it onto a semiconductor wafer using a sequence of chemical and optical processes called fabrication.

The defining trait of an IC is integration. Every component shares the same substrate. Layers built on that substrate stack up 30 or more times in a finished chip. Each layer is incredibly thin, measuring just a few millionths of a millimeter. Furthermore, designers determine whether a region becomes a transistor, resistor, or wire entirely by where they place n-type and p-type semiconductor regions across each layer.

Consequently, engineers describe IC complexity using scale tiers. These categories include SSI, MSI, LSI, VLSI, and ULSI. They distinguish chips by transistor count and integration density rather than their specific function. For instance, a 1970s logic chip had only a few dozen transistors. In contrast, a modern applications processor contains tens of billions of transistors. Both are technically integrated circuits, but they sit at opposite ends of the scale.

How Are Integrated Circuits(ICs) Made? The Fabrication Process

IC fabrication happens in a semiconductor fab. This facility is incredibly sensitive to contamination. In fact, experts measure air cleanliness in particles per cubic foot. The manufacturing sequence generally follows several distinct stages.

  1. Crystal Growth and Wafer Slicing

First, manufacturers grow a single, ultra-pure silicon crystal. They typically use the Czochralski method for this step. In this process, operators melt electronic-grade silicon at around 1,500°C. This silicon is highly refined, containing less than one impurity per 100 billion atoms. The machine slowly pulls the molten silicon into a cylindrical ingot. Finally, a diamond saw slices the ingot into thin discs called wafers. The largest wafers today run 300mm in diameter, though the industry is evaluating a future move to 450mm.

  1. Layering and Photolithography

Next, the deposition stage begins. Workers deposit a layer of material across the wafer surface. This material is destined to become wiring, a transistor gate, or an insulator. Common deposition techniques include chemical vapor deposition (CVD) and physical vapor deposition (PVD).

After deposition, photolithography patterns the wafer. A machine projects the circuit pattern from a photomask onto a photoresist-coated wafer using light. This step defines exactly where the next processing action should occur. At advanced nodes, this step uses extreme ultraviolet (EUV) light with wavelengths around 13.5nm. As a result, it can resolve features measured in nanometers.

  1. Etching, Doping, and Planarization

Subsequently, etching removes unwanted material from the wafer. Chemicals handle wet etching, while plasma drives dry etching. This process carves out the exact pattern defined by the photoresist.

Then, ion implantation embeds dopants into the wafer. These dopants create regions of increased or decreased conductivity. Specifically, they form the p-type and n-type silicon regions that build every transistor.

To prepare for the next layer, chemical-mechanical planarization (CMP) polishes the wafer flat. This ensures the next layer can deposit accurately. Workers repeat these deposition, lithography, etching, and doping steps dozens of times to build the chip layer by layer.

  1. Testing and Final Packaging

Once the wafer is complete, automated equipment electrically tests every die. Testing machines mark bad dies so operators can separate them later. The ratio of good dies to total dies is called the wafer’s yield. Next, machines cut the good dies apart during a process called singulation. Finally, workers seal each good die into a protective package that connects it to the outside world.

At advanced process nodes, this entire sequence requires significant time. For example, fabrication at modern 14/10/7nm-class nodes can take up to 15 weeks. Typically, the process lasts 11 to 13 weeks. Therefore, component sourcing and inventory planning matter just as much as the design itself. A quick design change to a part already in stock can save months of waiting.

How Does an IC Actually Work?

At the transistor level, an IC’s job is simple. It controls the flow of electrical current while using almost no current itself. The dominant technology for this is the MOSFET. Engineers arrange these switches in CMOS configurations. These configurations pair p-channel and n-channel transistors to switch states with very low power draw between transitions.

Each transistor acts as a microscopic switch. If you combine enough switches, you create logic gates like AND, OR, NOT, and NAND. These gates further combine into adders, registers, and entire processor cores. Consequently, a modern CPU or GPU die is an incredibly large network of these switches. They clock in lockstep to execute instructions at gigahertz speeds.

However, not every IC works this way. Analog ICs do not switch between discrete states. Instead, they manipulate continuous voltages and currents to amplify, filter, or condition a signal. Furthermore, mixed-signal ICs combine both jobs on the same die. This integration is exactly what makes a smartphone’s touchscreen controller or audio codec possible.

Types of Integrated Circuits(IC)

Engineers classify ICs along a few overlapping dimensions. These include signal domain, function, and integration scale. Typically, the signal domain serves as the most common starting point. Integrated circuits are generally digital or analog, though mixed-signal ICs combine both circuit types on a single die.

IC Category What It Does Typical Examples Common Applications
Digital

 

Processes discrete binary signals (0s and 1s) Microprocessors, microcontrollers, FPGAs, logic gates, memory (DRAM, SRAM, flash) Computers, embedded controllers, digital logic
Analog

 

Processes continuous signals through amplification, filtering, demodulation, and mixing Op-amps, voltage references, analog filters, power management ICs Sensor interfaces, power regulation, audio
Mixed-signal

 

Combines analog and digital circuitry on one die, sometimes with embedded software ADCs, DACs, CMOS image sensors, touch controllers Smartphone SoCs, cameras, touchscreens, radios
RF/Communication

 

Processes high-frequency signals for wireless links Low-noise amplifiers (LNAs), power amplifiers (PAs), mixers Cellular modems, Wi-Fi/Bluetooth radios
Programmable logic

 

Configurable logic blocks and interconnects that can be reprogrammed after manufacturing FPGAs, CPLDs Prototyping, hardware acceleration, custom protocols
ASIC

 

Custom-designed chips optimized for one specific application Crypto-mining chips, AI accelerators High-volume, performance-critical designs

Note: Within digital ICs, memory deserves special mention. DRAM, SRAM, and non-volatile flash memory are the dominant memory types. Standalone memory ICs remain common. However, designers increasingly embed memory functions directly into larger System-on-Chip (SoC) designs rather than shipping them as separate parts.

IC Packages: From Bare Die to PCB-Ready Component

The silicon die is only half the story. The package around it determines how the chip mounts to a board. It also affects how well it dissipates heat and behaves at high frequencies. Generally, IC packages fall into three broad families: through-hole packages, leaded surface-mount packages, and array packages.

Package Mounting Pin Pitch Best For Trade-off
DIP

 

Through-hole 0.1″ (2.54mm) Prototyping, breadboards, hobbyist builds Large footprint, weak high-speed performance
SOIC

 

Surface-mount 1.27mm (50 mil) General-purpose analog/digital ICs Limited pin count vs. QFN/BGA
TSSOP

 

Surface-mount Reduced pitch, ~1.0–1.2mm body Memory ICs, gate drivers, space-constrained boards Harder to hand-solder than SOIC
QFN

 

Surface-mount, no leads 0.4–1.0mm Compact, thermally demanding, RF-sensitive designs Requires reflow; hard to hand-solder
BGA

 

Array, solder balls Varies (0.4–1mm typical) High pin-count processors, FPGAs, and DDR memory Requires X-ray inspection; difficult rework
WLCSP

 

Array, wafer-level Sub-mm Space-critical mobile and wearable designs Smallest size but lowest pin-count ceiling

Furthermore, package choice drives thermal and electrical performance. Through-hole DIP packages run 50–100°C/W in junction-to-ambient thermal resistance. Standard SOIC reaches 80–120°C/W. In contrast, a properly designed QFN drops to 15–40°C/W. BGA packages achieve 10–30°C/W, while flip-chip BGA variants drop under 10°C/W using thermal balls. This difference matters significantly for any design pushing current through a small package.

Therefore, follow this common rule of thumb for PCB design:

  • DIP is easiest for hand soldering.
  • SOIC is the most forgiving general-purpose SMT choice.
  • QFN balances size and thermal performance best for compact designs.
  • BGA is the right call when pin count and high-speed performance matter most.

Why Moore’s Law Looks Different in 2026

For decades, IC progress meant shrinking the transistor to fit more of them on a die. That trend is still alive, but its character has changed. For instance, TSMC confirmed that its N2 (2nm) process entered volume production in the fourth quarter of 2025. This milestone marks the industry’s shift from FinFET transistor architecture to Nanosheet Gate-All-Around (GAA) technology. In this design, the gate surrounds the channel on all four sides. Consequently, it provides tighter electrostatic control and reduces leakage.

However, the economics of that progress are shifting too. Industry roadmaps through the rest of the decade increasingly use angstrom-based naming instead of nanometers. Furthermore, analysts note that the density gain between consecutive generations has narrowed significantly. It no longer matches the doubling that Moore’s Law once implied. As a direct response, leading-edge chipmakers are increasingly assembling multiple dies into a single advanced package. This practice is known as chiplet design or heterogeneous integration.

For component buyers and PCB designers, the practical takeaway focuses on availability and cost. Reports indicate that TSMC’s 2nm process costs at least 50% more than the 3nm node. This high cost filters down through allocation, lead times, and pricing. Therefore, mature nodes (28nm and above) remain the practical, cost-effective choice for most boards. That is exactly where manufacturers continue to produce the bulk of catalog ICs, including microcontrollers and op-amps.

Choosing the Right IC for Your Design

Component selection comes down to a short list of practical questions:

  1. What signal domain does the function need? Pure logic points to digital. Sensor conditioning points to analog. Meanwhile, anything involving conversion points to mixed-signal.
  2. What is the production volume? Low-volume prototyping favors hand-solderable packages like DIP or SOIC. Conversely, high-volume designs favor QFN or BGA because they save space.
  3. What is the thermal budget? A power IC running near its current limit benefits from a QFN or BGA package. These packages provide an exposed thermal pad.
  4. Is the part likely to face allocation risk? Components built on leading-edge nodes carry more supply risk. Therefore, parts built on mature nodes with multiple qualified manufacturers offer safer alternatives.

Fortunately, sourcing platforms like LCSC help narrow your part list. They stock a broad catalog of ICs with full datasheet access and stock visibility. Furthermore, they integrate directly with JLCPCB to help designs move smoothly from BOM to assembled board.

FAQ: Integrated Circuit(IC) Basics

Q: What is the difference between a chip and an integrated circuit?

They are generally the same thing. “Chip” is the colloquial term, while “integrated circuit” is the formal one. Both refer to a complete electronic circuit fabricated together on a single piece of semiconductor material. The term “chip” applies equally to a simple logic device and a modern processor. In everyday engineering conversation, professionals use the two terms interchangeably without any technical distinction.

Q: What material are most ICs made from?

Silicon dominates the industry due to its natural abundance and stable oxide layer. This layer makes insulating and patterning the surface much easier. Furthermore, decades of well-understood doping behavior support this choice. Specialized applications sometimes use gallium arsenide for better electron mobility. However, silicon’s combination of low cost and supply chain maturity ensures it dominates mainstream IC production.

Q: Why are modern ICs measured in nanometers or angstroms?

The figure refers to a process node. Historically, this tracked the physical size of a transistor’s smallest feature, like the gate length. Today, node names have less direct relation to actual transistor dimensions. Instead, manufacturers treat them as marketing labels that summarize a bundle of performance improvements. Nevertheless, smaller node numbers still correlate with higher transistor density and improved efficiency.

Q: Can an IC be repaired if it fails?

No, you cannot repair an IC. Unlike discrete circuits, an IC is a single sealed unit fabricated as one inseparable piece of silicon. If any internal transistor fails due to electrical overstress, you cannot access it. Therefore, you must replace the entire chip. Because of this, manufacturers invest heavily in wafer probing to catch defective dies early.

Q: What is the difference between an ASIC and an FPGA?

An ASIC is custom-designed to perform one specific function. Its logic is permanently set in silicon during manufacturing. Conversely, an FPGA contains an array of configurable logic blocks. Engineers can reprogram these blocks repeatedly after manufacturing using hardware description languages. This flexibility makes FPGAs excellent for prototyping. However, ASICs win on raw performance and lower per-unit cost at high volumes.

Conclusion

An integrated circuit takes the physics of a microscopic switch and replicates it billions of times across a few square millimeters of silicon. The core fabrication concepts have not changed fundamentally since the 1960s, even as precision has reached atomic scales. Whether you are specifying an op-amp or evaluating a BGA-packaged SoC, understanding the fabrication process helps you predict thermal behavior, sourcing risk, and assembly costs.

Therefore, you should explore comprehensive component catalogs to compare specs and check stock before finalizing your next BOM.

More Discount Information
Connect With Us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30 am - 12 am, 1:30 pm - 10 pm
Monday - Friday, UTC/GMT +8
View Our Social Channels
Encrypted
Payment
© 2025 LCSC.COM All Rights Reserved.
粤ICP备17041818号 ISO/IEC