High-Voltage MOS Tube Application in Hair Dryers

Hello everyone, LCSC Electronic supplier MDD shared the MOS tube application solution for hair dryers. In the article, MDD analyzed the requirements for the circuit design of high-speed hair dryers and recommended MOS tubes that suit this solution.

High-speed Hair Dryers Circuit Design Requirements

The high rotational speed of the high-speed hair dryer is mainly from the DC three-phase brushless motor, which has the advantages of simple structure, high reliability, good speed regulation performance, long life, no reversing spark, high output torque, small size, and lightweight to combine with the hair dryer.

The traditional hair dryer serves to dry the hair at high temperatures. Excessive temperature will damage the hair quality. However, the high-speed hair dryer has temperature control chips. So the maximum temperature will not exceed 57 degrees. In addition, some high-speed hair dryers also offer hair care functions, such as essential oils and negative ions, to provide better hair protection.

Secondly, the weight of the high-speed hair dryer is light. Compared with the traditional hair dryer, the structure of the high-speed hair dryer is streamlined. Therefore, the size of the whole machine is smaller, and the weight is lighter, which is easier to carry.

High-Voltage MOS Tube Application in Hair Dryers

Typical Application Topology and Application Cases

full bridge DC motor drive circuit

The full-bridge DC motor drive circuit is to accurately control the three sets of MOS through the program setting of the control center. To make the three-phase brushless motor work properly, we control the motor conduction of different phases with a specific turnover sequence. At the same time, through high-frequency switches, it increases speed and meets the air volume requirements of high-speed hair dryers.

The application of high-voltage MOS tubes in high-speed hair dryers is mainly to control the speed of the motor. MOSFET (Metal Oxide Semiconductor Field Effect Transistor) has a high switching frequency, a simple control method, a response speed, small incentive resistance, high reliability, etc. It is ideal for application in high-speed hair dryers.

Recommended MOS Tube Products

MOS Tube Products

MOS Tube Products

MOS Tube Model Selection

MOS Tube Model Selection

 

About Supplier MDD

MDD is a national high-tech enterprise specializing in R&D, packaging, testing, and selling semiconductor power devices for 15 years. It always adheres to product technology as the driving force and customer demand as the core. It offers a complete series of highly reliable and high-performance product service matrices covering MOSFET, diode, transistor, rectifier bridge, SiC, and other fields. The products serve in new energy vehicles, industrial control, consumer electronics, communication, home appliances, medical, lighting, security, instruments, and meters for over 40 countries and regions.

The company adheres to the development concept of keeping up with the times. Based on the current advanced power device design and packaging testing capabilities, It continuously pays attention to the development trends of cutting-edge technologies and application fields. It comprehensively promotes product upgrading and iteration, improves the industrialization of power devices and the ability to provide closed-loop services, and provides customers with sustainable, comprehensive, and differentiated one-stop product solutions.

Founded in 2012 in Shenzhen, bordering Hong Kong, LCSC Electronics is committed to helping engineers and enterprises who purchase qualified electronic parts for samples and small production purposes. After years of unremitting efforts, LCSC has become a global distributor with an extensive selection of electronic components. LCSC is the authorized distributor of MDD. Select MDD’s MOS tube and other products at LCSC Electronics.

More Discount Information
Connect With Us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30 am - 12 am, 1:30 pm - 10 pm
Monday - Friday, UTC/GMT +8
View Our Social Channels
Encrypted
Payment
© 2025 LCSC.COM All Rights Reserved.
粤ICP备17041818号 ISO/IEC