Key Takeaways
- Housing is a precision-engineered component: not a commodity plastic shell. It maintains dielectric breakdown voltage of 500–1500 V AC, keeps terminals seated under high pull-out forces, and can achieve IP67/IP68 sealing against moisture ingress.
- Material selection determines temperature class: Nylon 66 handles −40°C to +105°C for commercial/industrial; PBT extends to +120°C with lower moisture absorption (< 0.1%) for automotive; LCP withstands −55°C to +240°C and is mandatory for SMT reflow processes above 260°C.
- Keyed and polarised geometry prevents mis-mating: proper keying reduces assembly errors by 95–99%. Reducing pitch increases creepage risk; always specify a housing with integrated barriers for high-voltage designs.
- Retention force determines vibration survival: friction lock suits low-vibration low-cost designs; positive lock (5–20 N actuation force) suits automotive and robotics; TPA (Terminal Position Assurance) provides a fail-safe check that cannot close unless all terminals are fully seated.
- UL 94V-0 is the correct flammability specification for all safety-critical and consumer-facing devices: burning stops within 10 seconds, no flaming drips. V-2 allows flaming drips and is not acceptable for consumer-facing or safety-critical applications.
The Critical Role of Connector Housing in Power Systems
Many design failures in power electronics are traced not to the silicon but to an underspecified connector housing that could not withstand the environmental stressors of the application. While the pins and sockets (terminals) carry the electrical current, the connector housing is the silent guardian of signal integrity. In high-power applications, a failure in the housing often leads to catastrophic shorts or thermal runaway.
The housing must be viewed as a precision-engineered component that manages:
- Electrical Isolation: maintaining a dielectric breakdown voltage often exceeding 500 V to 1500 V AC.
- Mechanical Protection: preventing physical damage to fragile crimp terminals and ensuring they remain seated under high pull-out forces.
- Environmental Sealing: achieving IP ratings such as IP67 or IP68 to block dust and moisture ingress, which can reduce insulation resistance by 80–90% over time.
Technical Specifications: Material Science Deep Dive
Common Polymers
- Polyamide (Nylon 66): The industry standard for wire-to-board housings. It offers excellent toughness and a high melting point. However, it is hygroscopic, absorbing 1.5–2.5% moisture by weight, which can affect dimensional stability in high-precision applications.
- PBT (Polybutylene Terephthalate): Preferred for automotive and industrial use. It has low moisture absorption (under 0.1%) and maintains its shape under chemical exposure.
- LCP (Liquid Crystal Polymer): Essential for SMT processes. LCP can withstand reflow soldering temperatures of 260°C to 280°C without warping or off-gassing.
Material Performance Data
| Material | Dielectric Strength (kV/mm) | Continuous Use Temp (°C) | Flammability Rating |
| Nylon 66 | 18–22 | −40 to +105 | UL94V-2/V-0 |
| PBT | 15–20 | −40 to +120 | UL94V-0 |
| LCP | 30–35 | −55 to +240 | UL94V-0 |
Mechanical Design and Alignment Features
Polarisation and Keying
Polarisation ensures the connector can only be inserted in one orientation. Keying goes a step further, using unique rib or notch patterns to prevent a cable from being plugged into the wrong header on a crowded PCB. In complex systems, using keyed housings can reduce assembly errors by 95–99%.
Pitch and Density
Pitch is the distance from the centre of one conductor to the centre of the next.
- Standard Pitch (2.54 mm / 0.1”): Common in breadboarding and legacy industrial gear.
- Micro Pitch (1.25 mm to 0.5 mm): Used in modern consumer electronics where space is at a 30–40% premium.
Reducing pitch increases the risk of creepage (current tracking over the surface). For high-voltage designs, always select a housing with a wider pitch or integrated barriers to maintain an air gap and prevent arcing.
Primary Retention Mechanisms
A connector is only as good as its ability to stay connected under stress. The retention force required depends on the vibration profile of the application.
- Friction Lock: Relies on the fit between the header and the housing. Best for low-vibration, low-cost environments.
- Positive Lock: Uses a physical latch or ‘ramp’ that clicks into place. This requires a specific actuation force (typically 5–20 N) to release, making it ideal for automotive or robotics where uninterrupted contact continuity must be maintained despite mechanical shock.
- TPA (Terminal Position Assurance): An auxiliary clip that ensures the metal terminal is fully seated. If the terminal isn’t in place, the TPA won’t close, providing a fail-safe check during assembly.
Actionable Selection Guide: A Step-by-Step Workflow
Step 1: Calculate Current and Voltage Requirements
To begin with,if your circuit carries 10A, ensure the housing material can dissipate the heat generated by the contact resistance (usually kept under 10–20 mΩ). If the temperature rise exceeds 30°C, select a higher-grade thermoplastic.
Step 2: Confirm Environmental Constraints
Secondly,if the device operates in an engine bay, select a housing with an operating range of −40°C to +125°C. For outdoor sensors, an IP67 housing will survive immersion in 1 metre of water for 30 minutes, maintaining internal humidity near 0%.
Step 3: Match Assembly Process to Housing Material
Furthermore,for high-volume manufacturing, confirm housings are compatible with automated crimping machines. For SMT assembly, LCP housing is mandatory to avoid blistering during the reflow oven cycle, where temperatures peak at 245°C–260°C.
Common Failure Modes and How to Avoid Them
- Terminal Back-out: Occurs when a terminal is pushed out during mating. TPA-compatible housings eliminate this risk by 98%.
- Stress Cracking: Caused by non-compatible cleaning solvents. Therefore,you should confirm chemical compatibility charts for PBT and Polycarbonate.
- Contact Fretting: Small-scale vibrations (under 100 microns) wear down plating.To prevent this,select a housing with a high normal force to dampen movement.
Future Trends: Miniaturisation and Hybridisation
As a result of moving toward Industry 4.0, connector housings are evolving. Demand is growing for Hybrid Housings — single shells that carry both power (up to 20A) and high-speed data signals (up to 10 Gbps).
In addition,new polymers incorporate EMI/RFI shielding directly into the plastic matrix, providing 40–60 dB of attenuation without the weight of traditional metal shells. This allows for more compact power modules.
Quick Selection Guide: Connector Housing in 60 Seconds
- For commercial / industrial, < +105°C → Nylon 66 housing; standard pitch (2.54 mm or 1.25 mm)
- Automotive underhood or industrial, < +120°C, low moisture absorption → PBT housing; IATF 16949 qualified
- Specifically for SMT reflow assembly (peak 260°C) → LCP housing mandatory — However,Nylon 66 and PBT cannot survive reflow without blistering
- In the case of high-power circuit (> 10A) → Confirm contact resistance < 20 mΩ; temperature rise < 30°C; select thermoplastic rated above max junction temperature
- Regarding outdoor or wet environment → IP67 or IP68 sealed housing variant; integral wire seal per contact cavity
- For safety-critical or consumer-facing device → UL 94V-0 flammability rating mandatory (V-2 allows flaming drips and is not acceptable)
- High-vibration environment (automotive / robotics) → Positive lock (5–20 N actuation force) + TPA secondary retention
Frequently Asked Questions
What is the difference between a connector shell and a housing?
A housing is the internal plastic insulating body that holds the terminals. A shell usually refers to an outer metal or reinforced plastic casing (like in D-Sub or circular connectors) used for EMI shielding and extra mechanical mounting strength. Confirm the shell and housing materials are galvanically compatible when sourcing.
How do I choose between UL 94V-0 and 94V-2 ratings?
Always select UL 94V-0 for safety-critical or consumer-facing devices. A V-0 rating means burning stops within 10 seconds on a vertical specimen and does not allow flaming drips. A V-2 rating is less stringent and allows for flaming drips, which can lead to a fire spreading across the PCB.
Does housing colour affect technical performance?
Beyond aesthetics, colour is a functional key. Many engineers use different colours (e.g., Red for Power, Black for Ground) to confirm correct assembly at a glance. In some cases, specific dyes can slightly alter the dielectric constant or UV resistance, so check the datasheet if using connectors in direct sunlight.
How does ‘Glow Wire’ testing differ from UL 94V-0?
While UL 94V-0 measures flammability, Glow Wire testing (IEC 60695-2-11) simulates a faulty connection overheating. The housing must meet the Glow Wire Ignition Temperature (GWIT) requirements for the European home appliance market.
What is the impact of ‘Contact Retention Force’ on housing design?
The housing must be rigid enough to hold the terminal against the insertion force. The terminal-to-housing retention force specification for a standard power connector should typically be above 30 N. If the housing is too soft, terminals will ‘float,’ leading to intermittent connections and loss of contact continuity.
Conclusion
Understanding connector housing is about balancing material science with mechanical reality. By choosing high-quality components from a trusted distributor like LCSC Electronics, you ensure your design meets the rigorous standards of modern power electronics. Evaluate your thermal loads, confirm your locking mechanisms, and select materials that match your assembly process to guarantee a failure-free lifecycle.
Find What You Need on LCSC
Browse thousands of connector housings from Molex, JST, TE Connectivity, and more on LCSC Electronics, all with detailed datasheets and ready-to-ship inventory. Filter by material, pitch, pin count, and IP rating.