Why Soldering Temperature Matters: Prevent Cracks, Cold Joints, and Poor Connections in PCB Assembly

Imagine you’re designing a brand-new electronic product, creating an innovative solution from scratch. PCB assembly is the process that turns your ideas and designs into a practical product. However, PCBA manufacturing isn’t just about placing components onto a board; controlling the soldering temperature directly affects the quality of each solder joint. The strength of the solder joint and the reliability of the electrical connection will ultimately determine the product’s performance and durability. 

Understanding and optimizing soldering temperature is a crucial step in enhancing product quality, which manufacturers and buyers must consider during production.

What is the Role of Soldering Temperature in PCBA Manufacturing?

Soldering temperature is a key factor in ensuring that solder joints provide stable and reliable electrical connections. The melting point of solder typically ranges between 180°C and 210°C. Within this temperature range, the solder can efficiently cover the pads and component leads, forming a stable electrical connection through diffusion and bonding, ensuring circuit reliability.

What Happens When Soldering Temperature is Too High or Too Low?

Effects of Excessive Temperature:

  • Cracked Solder Joints: Overheating can cause micro-cracks in the solder joints, reducing mechanical strength.
  • Oxidation: High temperatures accelerate solder oxidation, leading to unstable wettability and resulting in weak joints.
  • Component Damage: Sensitive components may fail due to high temperature, such as plastic housings deforming or chips overheating.
Overheated solder joint with burn marks, causing cracks, oxidation, and potential component damage
Overheated solder joint with burn marks, causing cracks, oxidation, and potential component damage (Image source: online)

Effects of Insufficient Soldering Temperature:

  • Poor Wetting: Solder may not fully melt, preventing proper coverage of pads and leads.
  • Cold Joints: Weak connection in soldering joints, leading to broken joints under mechanical vibration or temperature fluctuations.
Cold solder joint with poor wetting, leading to weak electrical and mechanical connections
Cold solder joint with poor wetting, leading to weak electrical and mechanical connections (Image source: online)

Common Soldering Processes and Their Temperature Requirements

Different soldering techniques require varying temperatures based on PCB material, solder type, and component types. Below are typical temperature ranges for common soldering processes.

Manual Soldering:

  • Typically uses a soldering iron with a temperature range of 300°C–400°C, suitable for small batches and repair work. However, manual soldering depends heavily on the skill level of operator, and improper techniques can lead to solder joint issues.
Manual soldering with soldering iron and solder wire, suitable for small batch production and repairs
Manual soldering with soldering iron and solder wire, suitable for small batch production and repairs (Image source: online)

Wave Soldering:

  • This highly efficient automated process is commonly used for through-hole components. The temperature is generally set between 240°C–260°C, ideal for mass production and reducing human error.
Wave soldering temperature zone adjustment interface for efficient automated soldering of through-hole components
Wave soldering temperature zone adjustment interface for efficient automated soldering of through-hole components (Image source: online)

Reflow Soldering:

  • Reflow soldering is widely used for surface-mount components (SMT). The temperature profile typically includes a preheat, soldering, and cooling stage, with peak temperatures controlled between 230°C–245°C.
Surface mount components on PCB, designed for automated placement and soldering
Surface mount components on PCB, designed for automated placement and soldering (Image source: online)

Advanced Temperature Control Techniques in PCBA Manufacturing

Effective temperature control is crucial in optimizing soldering processes and enhancing solder joint reliability. At LCSC, we strive to provide reliable thermocouple measurement solutions through innovative technologies.

Infrared Temperature Detection:

Infrared sensors enable real-time monitoring of temperature distribution across the soldering zone, ensuring uniform heating. By reducing temperature overshoot, infrared technology helps prevent solder joint quality issues caused by excessively high or low temperatures. However, non-contact methods may face accuracy limitations in complex PCB structures.

Thermocouple Measurement:

In comparison to infrared technology, thermocouple measurement offers higher precision, particularly for complex structures and densely populated PCBs. The thermocouple is directly embedded in the soldering zone, capturing small temperature variations to ensure optimal soldering conditions for each joint.

Optimizing Temperature Profiles:

An ideal temperature profile includes the following stages:

  1. Preheat Zone: Gradually increasing temperature to 120°C–150°C can prevent thermal shock in the soldering area.
  2. Soldering Zone: Rapidly heating to peak temperature (e.g., 230°C–245°C) to complete solder joint wetting.
  3. Cooling Zone: Quickly cooling to room temperature to ensure solder joint solidification.
Temperature monitoring technology for controlling reflow temperature profile
Temperature monitoring technology for controlling reflow temperature profile (Image source: online)

Common Issues and Solutions for Soldering Temperature Control

Common Issues:

  • High Temperature Problems: Solder joint cracking, component damage.
  • Low Temperature Problems: Poor wetting, cold joint formation.

Solutions:

  1. Experiment with Process Parameters: Optimize temperature, time, and solder type through testing.
  2. Use Advanced Equipment: Employ precision temperature control devices for enhanced accuracy.
  3. Regular Maintenance: Maintain soldering equipment to prevent sensor malfunction.
Image showing solder joint cracking and poor wetting issues
Image showing solder joint cracking and poor wetting issues (Image source: online)

Optimizing Soldering Temperature for Reliable PCBs

Temperature control is essential at every stage of PCBA manufacturing. Through careful process selection, advanced technology, and strict quality monitoring, manufacturers can significantly enhance solder joint quality and PCB performance, ensuring product reliability and stability.

At LCSC, we understand customer expectations for quality and reliability, continuously optimizing our production processes to meet the needs of industries ranging from consumer electronics to industrial control. By investing in innovative solutions, we work alongside customers to drive technological progress in the electronics manufacturing industry.

Some images are sourced online. Please contact us for removal if any copyright concerns arise.


Custom Cables: Save 50%+ Avg Cost By JST, Molex, TE Alternatives | Processing Fee Down to $1 Per Piece | No Minimum Order Quantity (MOQ) Required

PCB & PCBA: New Customer Get Coupons Up to $125 | 1 – 32 Layers From $2 /5pcs | PCB Assembly From $8 /5pcs

Front Panels: High-quality Front Panel Acrylic/PET | Front Panel Order Up to 30% Off | Membrane Switch Available Soon

More Discount Information
Connect With Us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30 am - 12 am, 1:30 pm - 10 pm
Monday - Friday, UTC/GMT +8
View Our Social Channels
Encrypted
Payment
© 2025 LCSC.COM All Rights Reserved.
粤ICP备17041818号 ISO/IEC