Why Soldering Defects Are Costing You: Solutions to Minimize Rework in PCB Assembly

The quality of a PCBA is largely determined by a crucial yet often underestimated step, soldering. Just like the foundation of a building, soldering securely connects electronic components to the circuit board, ensures stability. However, soldering isn’t always flawless. Soldering defects can severely impact the functionality and reliability of the PCBA. These defects may not only reduce product performance but can also lead to failures, or shorten the lifespan of product.

PCBA assembly with mixed SMT and through-hole components
PCBA assembly with mixed SMT and through-hole components (Image source: online)

Common Types of Soldering Defects and Their Causes

There are various types of soldering defects, each with specific causes and impacts. Understanding these common defects is crucial for effective quality control:

  • Voids: Tiny bubbles trapped in the solder joint. These are voids, which form when gas isn’t fully expelled during the soldering process. Voids reduce the strength and conductivity of the solder joint.
Soldering defects example: voids in solder joints caused by trapped gas bubbles, reducing strength and conductivity
Voids in solder joints caused by trapped gas bubbles, reducing strength and conductivity (Image source: online)
  • Cold Soldering: If the soldering temperature is not hot enough or the solder does not fully melt, cold soldering occurs. This results in poor connections, much like glue not fully adhering to surfaces, causing intermittent issues like flickering lights.
Cold solder joint causing poor contact and potential cracking of solder, leading to intermittent circuit connection
Soldering defects: Cold solder joint causing poor contact and potential cracking of solder (Image source: online)
  • Bridging: When too much solder is applied or soldering is not precise, it causes short circuits between adjacent solder joints. This disrupts the functionality of the circuit and could damage components.
Solder bridging between adjacent pads causing short circuits in QFP component, leading to malfunction
Solder bridging between adjacent pads causing short circuits in QFP component, leading to malfunction (Image source: online)
  • Dry Joints (Incomplete Soldering): Sometimes, solder joints may appear normal, but internally they lack a solid connection. Dry joints lead to poor contact and intermittent failures, making them difficult to troubleshoot.
Dry joint on L-shaped pin with solder on the lead but no solder on the pad, causing intermittent circuit failure
Soldering defects: Dry joint on L-shaped pin with solder on the lead but no solder on the pad (Image source: online)

Key Factors Affecting Soldering Quality

Several factors influence soldering quality; controlling them is essential for optimal results:

  • Soldering Temperature Profile: Reflow soldering is like baking in an oven; it requires a specific temperature profile to ensure the solder melts, stays molten for a period, and then cools slowly. Improper temperature curves lead to poor solder joints.
  • Solder Material: Different solder materials have distinct properties. Using the correct type of solder ensures better quality. For environmental reasons, we recommend using lead-free solder to maintain quality while protecting the environment.
  • PCB Surface Cleanliness: If the PCB surface is contaminated with dust or oil, it can affect solder adhesion, leading to defects.
Cleaning PCB surface with a brush to remove dust and oil for better solder adhesion
Cleaning PCB surface with a brush to remove dust and oil for better solder adhesion (Image source: online)
  • Soldering Equipment: Manual and automated soldering equipment each have their advantages and disadvantages. While manual soldering is flexible, yet less Automated equipment, on the other hand, offers higher accuracy and efficiency. Choosing the right soldering method is paramount for improving soldering quality.

Solutions to Soldering Defects

To address soldering defects, we focus on prevention and detection, with an emphasis on preventative measures:

  • Prevention: Optimize soldering parameters (like temperature and time) and ensure components and PCB surfaces are clean to minimize the likelihood of defects.
  • Real-Time Detection: X-ray inspection equipment can quickly identify soldering defects. This technology allows for a thorough examination of solder joints, ensuring each joint meets quality standards.
X-ray inspection of solder joints to detect internal defects and ensure quality
X-ray inspection of solder joints to detect internal soldering defects and ensure quality (Image source: online)
  • Automation: Automated Optical Inspection (AOI) systems enable efficient and accurate detection of soldering defects, ensuring product consistency and quality.
  • Process Optimization: By analyzing data from the production process, continuous improvements made to the soldering process have positive effects, such as reducing defect rates and improving overall efficiency.

Case Study: Voids Causing Circuit Disconnection

During a production run, some samples exhibited malfuntion. Upon inspection, the solder joints had numerous voids, which caused poor contact and resulted in circuit disconnection. The reason was traced back to an incorrect soldering temperature profile that failed to expel all the gas during the process. Readjusting the temperature profile and refining the soldering process

isual inspection of PCB to detect voids in solder joints causing circuit failure
visual inspection of PCB to detect voids in solder joints causing circuit failure (Image source: online)

Some images are sourced online. Please contact us for removal if any copyright concerns arise.


Custom Cables: Save 50%+ Avg Cost By JST, Molex, TE Alternatives | Processing Fee Down to $1 Per Piece | No Minimum Order Quantity (MOQ) Required

PCB & PCBA: New Customer Get Coupons Up to $125 | 1 – 32 Layers From $2 /5pcs | PCB Assembly From $8 /5pcs

Front Panels: High-quality Front Panel Acrylic/PET | Front Panel Order Up to 30% Off | Membrane Switch Available Soon

More Discount Information
Connect With Us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30 am - 12 am, 1:30 pm - 10 pm
Monday - Friday, UTC/GMT +8
View Our Social Channels
Encrypted
Payment
© 2025 LCSC.COM All Rights Reserved.
粤ICP备17041818号 ISO/IEC