Key Takeaways
- FL (Hirose) and IPEX MHF connectors are both 50-ohm micro-coaxial board-level RF connectors used to connect PCB-mounted radios to external antennas.
- FL and MHF1 are mechanically compatible and interchangeable; MHF4 and MHF5 are smaller, higher-frequency variants that are not footprint-compatible with U.FL.
- Impedance matching at 50 ohms is critical — a single poorly matched connector can cause VSWR to spike, producing signal reflections that degrade range, throughput, and regulatory compliance.
- Shielding effectiveness depends as much on your PCB ground-plane design as on the connector itself; both families rely on the outer shell contacting a well-designed ground ring.
- Selection rule of thumb: space-constrained IoT/Wearable → MHF4; general-purpose WiFi/BLE/GPS → U.FL or MHF1; 5G/mmWave → MHF5 or consider SMA/MMCX.
What IS U.FL and IPEX MHF Connector?
U.FL is an ultra-miniature 50-ohm coaxial connector series developed by Hirose Electric, the Japanese connector giant. Introduced in the early 2000s, the U.FL quickly became the industry-standard interface for board-to-antenna RF connections in consumer electronics. The receptacle (part number U.FL-R-SMT-1) solders directly to the PCB as a surface-mount component, while a mating plug — typically terminated to a thin coaxial pigtail cable — snaps onto it. U.FL connectors are rated for operation from DC to 6 GHz, with a minimum durability of 30 mating cycles.
IPEX MHF (Micro High Frequency) is a family of micro-coaxial connectors manufactured by IPEX Connectors (now part of the Amphenol group). The MHF1 variant was designed as a direct compatible alternative to Hirose’s U.FL — same footprint, same mating interface, same electrical envelope. But IPEX didn’t stop there. The MHF series has since expanded into a full portfolio of progressively smaller variants targeting higher frequencies and tighter space constraints.
The key distinction to understand from the start: “IPEX” (or “IPX,” in colloquial usage) is often used generically to describe this whole category of micro-coaxial RF connectors — but technically, U.FL is Hirose’s original design, and MHF is IPEX’s compatible product line. The two coexist in the market, and for the MHF1 variant specifically, they are physically interchangeable.
The IPEX MHF Family: One Series, Five Variants
If you’ve ever browsed an LCSC RF connector category page looking for “the little antenna connector” and felt overwhelmed by the options, here’s why: the MHF family spans five major generations, each with distinct mechanical and electrical characteristics.
| Variant | PCB Footprint | Mated Height | Frequency Range | U.FL Compatible? | Typical Use Case |
| MHF1 | 3.0 × 3.1 mm | ~2.5 mm | DC–6 GHz | ✅ Yes | WiFi, BLE, GPS, general IoT |
| MHF2 | 2.0 × 2.0 mm | ~1.4 mm | DC–6 GHz | ❌ No | Thin laptops, tablets |
| MHF3 | 1.7 × 1.7 mm | ~1.3 mm | DC–6 GHz | ❌ No | Smartphones, wearables |
| MHF4 | 1.7 × 1.7 mm | ~1.2 mm | DC–10 GHz | ❌ No | 5G sub-6, compact IoT, drones |
| MHF5 | 1.4 × 1.4 mm | ~1.0 mm | DC–15 GHz | ❌ No | mmWave, Wi-Fi 6E/7, ultrabooks |
MHF1 is the only variant that mates with standard U.FL plugs. If your design currently uses an off-the-shelf U.FL antenna or cable assembly, switching to MHF1 is mechanically seamless. All subsequent MHF variants (MHF2 through MHF5) use progressively smaller interfaces that are mechanically incompatible with U.FL plugs — you cannot snap a U.FL cable onto an MHF4 receptacle, and attempting to do so risks damaging both components.
MHF4 has emerged as the most popular variant for new IoT and wireless designs, striking a balance between ultra-compact size and wide frequency coverage up to 10 GHz. It’s the connector you’ll find on many modern Wi-Fi 6, Bluetooth 5.x, and 5G sub-6 GHz modules from manufacturers like Quectel, u-blox, and Nordic Semiconductor.
Impedance Matching: Why 50 Ohms Is Non-Negotiable
Both U.FL and MHF connectors are designed for 50-ohm characteristic impedance — the universal standard for RF and microwave systems, settled on as a compromise between minimum loss (which occurs around 77 ohms for air-dielectric coax) and maximum power handling (which peaks around 30 ohms). Every element in your RF chain — the transceiver output, the PCB trace, the connector, the coaxial cable, and the antenna — must present 50 ohms to maintain a matched condition.
When impedance is matched, maximum power transfers from source to load with zero reflection. When it isn’t, part of the signal bounces back toward the source. That reflection is quantified by two related metrics:
- VSWR (Voltage Standing Wave Ratio): The ratio of maximum to minimum voltage along the transmission line due to reflected waves. A perfectly matched line has VSWR = 1.0:1. In practice, a VSWR ≤ 1.5:1 is considered acceptable for most consumer wireless applications.
- Return Loss: The power reflected expressed in dB. A VSWR of 1.5:1 corresponds to approximately 14 dB return loss — meaning about 4% of transmitted power is reflected.
A single poorly matched connector can cascade into system-level failures. Consider a WiFi router transmitting at +20 dBm (100 mW). If the antenna connector introduces a VSWR of 2.0:1 rather than the expected 1.3:1, roughly 11% of the power reflects back instead of radiating. That’s not just lost range — it’s also heat dissipated in the transmitter output stage and potential spurious emissions that could push the product out of regulatory compliance.
Both Hirose and IPEX specify VSWR performance for their connectors:
- FL: VSWR ≤ 1.3 (DC–3 GHz), ≤ 1.5 (3–6 GHz)
- MHF1: VSWR ≤ 1.3 (DC–3 GHz), ≤ 1.4 (3–6 GHz)
- MHF4: VSWR ≤ 1.4 (DC–6 GHz), ≤ 1.6 (6–10 GHz)
Shielding Effectiveness: It’s Not Just the Connector
“Which connector has better shielding — U.FL or MHF?” This is one of the most common questions engineers ask, and the honest answer is: the connector itself contributes relatively little to overall shielding effectiveness compared to your PCB design.
Both U.FL and MHF connectors use the same fundamental coaxial construction: a center pin carrying the signal, surrounded by an outer shell connected to ground. This geometry is inherently self-shielding — the ground shell acts as a Faraday cage around the signal conductor. When properly installed, both families provide excellent EMI isolation.
What actually determines real-world shielding performance is:
- Ground plane continuity beneath the connector. The receptacle’s ground pins must connect to a solid, unbroken ground plane on the PCB’s top layer. Any gap, split, or void under the connector creates an impedance discontinuity that radiates.
- Ground via stitching around the connector footprint. A ring of closely spaced ground vias (≤ 1 mm pitch for frequencies above 3 GHz) around the connector footprint creates a “via fence” that suppresses lateral RF leakage and constrains the field within the PCB stackup.
- The transition from microstrip/stripline to connector. The RF trace must transition cleanly to the connector’s center pin pad. Any stub, neck-down, or sharp bend creates a parasitic inductance that degrades both impedance match and shielding.
- Mating integrity. The plug must be fully seated on the receptacle. A partially seated connector leaves a gap in the ground shell, creating a slot antenna that radiates at frequencies where the gap dimension approaches a quarter-wavelength.
For both connector families, shielding is a system-level property, not a component specification. A $0.05 MHF1 receptacle on a well-designed PCB with proper grounding will outperform a $2 SMA connector on a poorly laid-out board every time.
Head-to-Head: U.FL vs. MHF Technical Comparison
Here is a side-by-side comparison of the key electrical and mechanical parameters for the most commonly used variants:
| Parameter | Hirose U.FL | IPEX MHF1 | IPEX MHF4 | IPEX MHF5 |
| Impedance | 50 Ω | 50 Ω | 50 Ω | 50 Ω |
| Frequency Range | DC–6 GHz | DC–6 GHz | DC–10 GHz | DC–15 GHz |
| VSWR (typ, 3 GHz) | ≤ 1.3 | ≤ 1.3 | ≤ 1.3 | ≤ 1.3 |
| Insertion Loss @ 2.4 GHz | ~0.15 dB | ~0.15 dB | ~0.2 dB | ~0.2 dB |
| Insertion Loss @ 6 GHz | ~0.5 dB | ~0.5 dB | ~0.4 dB | ~0.35 dB |
| Mated Height | 2.5 mm | 2.5 mm | 1.2 mm | 1.0 mm |
| Mating Cycles (min) | 30 | 30 | 30 | 20 |
| Receptacle Footprint | 3.0 × 3.1 mm | 3.0 × 3.1 mm | 1.7 × 1.7 mm | 1.4 × 1.4 mm |
| Plug Retention Force | ~2 N | ~2 N | ~1 N | ~0.8 N |
| Mass Production Status | Mature | Mature | Active | Active |
Insertion Loss: Where the dB Adds Up
Insertion loss is the power lost as the signal passes through the connector. At 2.4 GHz (WiFi/BLE), both U.FL and MHF1 connectors introduce roughly 0.15 dB of loss each. That’s negligible for most designs — it represents about 3.4% power loss per connector.
However, in systems operating at higher frequencies or those with multiple connector transitions (PCB → pigtail → bulkhead → antenna), the losses accumulate. At 6 GHz, each U.FL or MHF1 pair contributes roughly 0.5 dB of loss. In a system with three connector transitions, that’s 1.5 dB — a 30% power loss before considering cable attenuation.
For 5 GHz WiFi and above, consider MHF4 or MHF5, which are optimized for lower insertion loss at higher frequencies. At 6 GHz, the MHF4 typically achieves 0.4 dB — a 20% improvement over U.FL — and the gap widens further as frequency increases.
PCB Layout and Footprint Compatibility
The single most consequential design decision around these connectors comes down to one question: do you need U.FL footprint compatibility, or can you commit to a newer, smaller standard?
The U.FL / MHF1 Footprint Ecosystem
U.FL and MHF1 share an identical recommended PCB land pattern: a rectangular footprint approximately 3.0 × 3.1 mm, with a central signal pad and two outer ground pads. This footprint has been stabilized for over two decades, and it is supported by virtually every RF module on the market — ESP32, nRF52/nRF53, Raspberry Pi CM4, u-blox GPS modules, and thousands of others.
The advantage of staying with U.FL/MHF1 is compatibility. Antenna cable assemblies with U.FL/MHF1 plugs are commodity items available from dozens of manufacturers. Your design is compatible with both Hirose U.FL and IPEX MHF1 (and countless third-party alternatives), giving procurement maximum flexibility.
MHF4 and Smaller: No Going Back
Once you move to MHF4 (1.7 × 1.7 mm footprint) or MHF5 (1.4 × 1.4 mm), you lose backward compatibility with U.FL. The smaller land pattern requires tighter PCB manufacturing tolerances, and the reduced retention force (1 N vs. 2 N for U.FL) means you need to be more careful about mechanical strain on the cable assembly.
The trade-off is worth it when space is at a premium. The MHF4’s footprint is less than one-third the area of U.FL, freeing precious board real estate in wearables, sensor nodes, and compact IoT modules.
Best Practices for Both Families
Regardless of which connector you choose:
- Keep the RF trace as short as possible between the transceiver and the connector pad
- Use a continuous, unbroken ground plane on layer 2 directly beneath the connector
- Stitch ground vias (≥ 4, ideally 6–8) around the connector footprint with ≤ 1 mm spacing
- Avoid placing the connector near board edges where ground return paths are compromised
- Consider adding a strain-relief feature or adhesive anchor point for the cable assembly
Applications: Where Each Connector Excels
U.FL / MHF1 — The Workhorse
If your design operates at or below 6 GHz and doesn’t push extreme space constraints, U.FL or MHF1 is almost certainly the right answer. You’ll find these connectors on:
- WiFi and Bluetooth modules (ESP32, nRF52, CYW43439)
- GPS/GNSS modules and active antenna connections
- LoRa and Zigbee gateways (868/915 MHz, 2.4 GHz)
- SDR (Software Defined Radio) dongles and evaluation boards
- LTE Cat-M1 / NB-IoT modules in industrial IoT
The broad ecosystem of compatible cables and antennas means faster prototyping and fewer sourcing headaches.
MHF4 — The Compact Performer
MHF4 has become the connector of choice for designs that push beyond 6 GHz or demand the smallest possible footprint:
- Wi-Fi 6/6E modules operating in the 5–7 GHz range
- 5G sub-6 GHz modules (n77/n78/n79 bands)
- Compact GNSS + L-band correction service receivers
- Drone FPV and telemetry systems
- Wearable medical and fitness devices with BLE
MHF5 — The Highest Frequency Frontier
MHF5 is still gaining traction, targeting applications above 10 GHz:
- Wi-Fi 7 (802.11be) with operation up to 7.125 GHz
- mmWave antenna modules (with appropriate system-level design)
- Ultra-wideband (UWB) precise ranging and radar systems
U.FL and MHF vs. Other RF Connector
For context, here is how U.FL and MHF fit into the broader landscape of RF connector options:
| Connector | Impedance | Frequency Range | Size (PCB) | Mating Cycles | Best For |
| U.FL / MHF1 | 50 Ω | DC–6 GHz | 3.0 × 3.1 mm | 30 | Internal board-to-antenna |
| MHF4 | 50 Ω | DC–10 GHz | 1.7 × 1.7 mm | 30 | Compact internal RF |
| MMCX | 50 Ω | DC–6 GHz | ~5 mm dia. | 500 | External test ports, modular RF |
| MCX | 50/75 Ω | DC–6 GHz | ~6 mm dia. | 500 | GPS, instrumentation |
| SMA | 50 Ω | DC–18 GHz | ~8 mm hex | 500+ | Lab equipment, external antennas |
| RP-SMA | 50 Ω | DC–18 GHz | ~8 mm hex | 500+ | Consumer WiFi APs/routers |
SMA and RP-SMA are the large, threaded connectors you see on the back of WiFi routers and on lab-grade RF test equipment. They’re durable (500+ cycles) and handle up to 18 GHz, but they’re far too large for board-level integration in compact products.
MMCX (Micro-Miniature Coaxial) occupies the middle ground — larger than U.FL/MHF but rated for 500 mating cycles thanks to its snap-on mechanism with a more robust retention design. It’s common on evaluation boards and products where the antenna connection doubles as a test port.
For internal board-to-antenna connections in mass-produced products, U.FL and MHF remain the dominant choice due to their size, cost, and ecosystem maturity.
How to Choose: A Practical Selection Framework
Walk through these five questions when selecting between U.FL and MHF variants for a new design:
1. What’s your maximum operating frequency?
- ≤ 3 GHz (GPS, 2.4 GHz WiFi, BLE, LoRa, Zigbee) → U.FL or MHF1. No benefit from higher-spec variants.
- 3–6 GHz (5 GHz WiFi, some LTE bands) → U.FL/MHF1 still adequate; MHF4 provides headroom.
- 6–10 GHz (Wi-Fi 6E, 5G n77/n78/n79) → MHF4 minimum.
- > 10 GHz (Wi-Fi 7, mmWave) → MHF5, or reconsider whether a board-level micro-coaxial connector is even the right choice — you may need a precision SMA or integrated antenna solution.
2. How much PCB space do you have?
- Plenty → U.FL/MHF1 for maximum compatibility and sourcing flexibility.
- Tight → MHF4 saves ~70% PCB area vs. U.FL.
- Extremely constrained → MHF5, but verify cable assembly availability first.
3. What’s your production volume and supply chain strategy?
- Low to medium volume / prototyping → U.FL/MHF1. The larger ecosystem of off-the-shelf compatible parts saves time.
- High volume (100k+ units) → Consider MHF4 if your CM can reliably handle the smaller footprint. Single-source risk is real — qualify at least two suppliers for the receptacle.
- Dual sourcing required by procurement → U.FL/MHF1. With the shared footprint, you can buy from Hirose, IPEX, or compatible third-party manufacturers without board changes.
4. Will the antenna be connected/disconnected frequently?
- > 20 cycles over product lifetime → U.FL/MHF1 with standard retention force. For anything approaching 30–50 cycles, consider MMCX instead — U.FL and MHF are not designed for frequent reconnection, and connector wear degrades both VSWR and mechanical retention.
- Connect once during assembly, never again → Any variant works. This is the intended use case for both families.
5. Do you need to connect to off-the-shelf antennas?
- Yes, using standard pigtail assemblies → U.FL/MHF1. The U.FL-connectorized pigtail market is enormous at LCSC and elsewhere — IPEX-to-SMA, U.FL-to-RP-SMA, MHF1-to-open-ended, you name it.
- Yes, custom antenna vendor → Check with the vendor which connector they support. Most antenna manufacturers offer U.FL/MHF1 as standard; MHF4 is increasingly available but not yet universal.
FAQ: IPEX vs. U.FL Connector
Q: Are IPEX MHF1 and U.FL connector interchangeable?
Yes, MHF1 and U.FL are mechanically and electrically interchangeable. The MHF1 receptacle shares the same PCB footprint (3.0 × 3.1 mm) and mates with standard U.FL plugs without issue. However, MHF2, MHF3, MHF4, and MHF5 are not compatible with U.FL — their smaller physical dimensions make mating impossible. Always verify which MHF variant you’re working with; “IPEX” alone doesn’t tell you.
Q: What happens if impedance matching is off?
When your connector or transmission line isn’t matched to 50 ohms, signal reflections occur at the impedance discontinuity. These reflections manifest as: (1) reduced radiated power — your range shrinks; (2) increased VSWR — the transmitter sees a mismatched load, which can cause overheating or automatic power back-off in modern radio ICs; (3) degraded signal integrity in both TX and RX paths. A VSWR of 2.0:1 (roughly 10% reflected power) is enough to noticeably degrade WiFi throughput in marginal signal conditions.
Q: Does MHF4 perform better than U.FL at WiFi frequencies?
At 2.4 GHz, the difference is negligible — both deliver approximately 0.15 dB insertion loss and VSWR ≤ 1.3. At 5 GHz WiFi, MHF4 holds a small advantage (0.3 dB vs. 0.4 dB insertion loss), which translates to marginally better range in noise-limited environments. The primary reason to choose MHF4 over U.FL for a WiFi design is size, not RF performance. If you have the board space for a U.FL/MHF1 footprint and your design stays below 6 GHz, the performance difference won’t be the deciding factor.
Q: Can I use U.FL or MHF connector for external antenna ports on an enclosure?
Not directly — U.FL and MHF connectors are designed for internal board-to-antenna connections and are not rated for repeated mating cycles or external environmental exposure. The standard design pattern is: PCB receptacle (U.FL/MHF) → short pigtail cable → bulkhead-mounted SMA or RP-SMA connector on the enclosure → external antenna. This approach keeps the delicate micro-coaxial interface safely inside the product while providing a robust, user-facing connector.
Q: Where can I source U.FL and MHF connector reliably?
LCSC stocks both Hirose U.FL and IPEX MHF series connectors, along with a wide selection of compatible cable assemblies, antennas, and RF modules. For the U.FL/MHF1 footprint, parts are available from Hirose, IPEX, and multiple qualified third-party manufacturers — search for “RF Connectors / Coaxial Connectors” or “RF Cable Assemblies” on LCSC’s category pages. For newer variants like MHF4, ensure you verify the specific manufacturer part number against your design, as footprint compatibility across brands is not guaranteed for non-MHF1 variants.
Conclusion: It’s About the System, Not the Connector
IPEX MHF and U.FL connectors are both mature, well-engineered solutions for board-level RF interconnects. The choice between them is rarely about electrical performance alone — a well-laid-out U.FL connection will outperform a poorly implemented MHF4 every time — and more often about the practical engineering trade-offs of size, ecosystem compatibility, and supply chain flexibility.
For most designs operating below 6 GHz with reasonable PCB space, U.FL or MHF1 remains the pragmatic default. The massive ecosystem of compatible modules, cables, and antennas means you’ll spend less time sourcing and more time designing. MHF4 earns its place when every square millimeter counts or when you’re pushing past 6 GHz. MHF5 is the forward-looking choice for Wi-Fi 7 and emerging mmWave applications — but check your cable assembly supply chain before committing.
Whatever you choose, remember: the connector is just one link in the RF chain. The ground plane beneath it, the trace leading to it, and the cable assembly leaving it all matter just as much. Get the system right, and your antenna will radiate exactly what your transceiver intended.