BHFUSE: 1812/3A/24V High Voltage Resettable Fuse

LCSC Supplier BHFUSE Industrial launched a new high-voltage resettable fuse—BSMD1812-300-24V (1812/3A/24V) at lCSC Electronics. Customers often inquire about this typical high-voltage model on the market. Compared with internationally renowned brands, BHFUSE resettable fuse BSMD1812-300-24V has significant advantages in price. And it can better meet the requirements of some subdivisions.

Brief Introduction to Resettable Fuse

A resettable fuse, also known as a Polymer Positive Temperature Coefficient (PPTC) device. It is a crucial passive electronic component in electronic circuits that provides overcurrent protection. It finds applications in various fields like computers, mobile phones, multimedia, automotive, industrial controls, telephony and broadband, game machines and portable electronics. 

BHFUSE Resettable Fuse Characteristics

BHFUSE resettable fuse—BSMD1812-300-24V (1812/3A/24V) has following characteristics:

  • Low standby power consumption: 

According to P=Ihold*Ihold*R, from the figure below, Ihold=3A, Rmin=0.012Ω, Rmax=0.06Ω for (BSMD1812-300-24V), then Pmin=3*3* 0.012=0.108W, Pmax=3*3*0.06=0.54W. That is to say that the power consumption in the standby state is 0.108W~0.54W, Which is much lower than the traditional direct plug-in model with the same parameters;

BHFUSE Resettable Fuse Characteristics

BHFUSE Resettable Fuse Characteristics

 

  • Smaller package size: 

1812 package size, seamless replacing the traditional 2920 package or direct plug series;

BHFUSE Resettable Fuse Characteristics

  • A large amount of ready stock, high quality, and low price, leading the industry.
About Supplier BHFUSE

Established in 2013, Shenzhen BHFUSE Industrial Co., Ltd. strives for the R&D and manufacturing of polymer positive temperature coefficient thermistors (PPTC resettable fuses) for circuit protection devices. Its R&D team are all veterans in the PPTC industry and have many years of experience in PPTC R&D and application. BHFUSE can provide a variety of stringent customized PPTCs to meet high-precision and high-standard circuit protection needs.

BHFUSE adheres to the development philosophy of pursuing innovation and quality. Their shipment volume has reached an annual output of 200 million units, covering the SMD patch series and DIP plug-in series PPTC resettable fuse. The company has earned recognition from many well-known companies.

Founded in 2012 in Shenzhen, which borders Hong Kong, LCSC Electronics aims to assist engineers and enterprises in purchasing qualified electronic parts for samples and production purposes. After years of continuous effort, LCSC has become a global distributor with an extensive selection of electronic components and more than 4 million registered customers worldwide. LCSC is the authorized distributor of BFFUSE. Choose BFFUSE’s  PPTC resettable fuse products at LCSC.

More Discount Information
Connect With Us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30 am - 12 am, 1:30 pm - 10 pm
Monday - Friday, UTC/GMT +8
View Our Social Channels
Encrypted
Payment
© 2025 LCSC.COM All Rights Reserved.
粤ICP备17041818号 ISO/IEC