CHAHUA

Marki azjatyckie
Chahua Modern Housewares Co., Ltd., established in 1997, is specializing in design, development, production, and sales of household items. Chahua is the first honorable enterprise accredited as a “well-known Trademark in China” in the plastic housewares industry and is also among China’s top 10 enterprises in the industry. In 2017, Chahua was listed on Shanghai Stock Exchange (Ticker Symbol. 603615). Chahua has 2 large-scale production bases,armed with highest level of fully automatic production line in the industry at present, and the most advanced high-precision equipment, such as CNC mold processing equipment, numerically-controlled machine tools, and injection machines, making it the largest production base of plastic housewares in China. We have obtained over 100 R&D design patents, received China’s Innovative Design Red Star Award for two consecutive years, and also obtained the ISO9001, ISO14001, ISO45001, BSCI and audited by Newell Rubbermaid, Target, Metro, Lotus, and QVC. CHAHUA always strives for supplying innovative and high-quality houseware to consumers worldwide, helping people live a better life!
Zarejestruj się, aby uzyskać więcej korzyści