How can we help?
Categories
PCB & PCBA
- 1. What files do I need to prepare to get a quotation for PCB & PCBA?
- 2. How can I get a quotation for PCB & PCBA?
- 3. How long it takes to get a quotation for PCB and PCBA?
- 4. What is the build time for PCB and PCBA?
- 5. What is the MOQ for PCB and PCBA?
- 6. What are the main products of your PCB & PCBA services?
- 7. How to get coupons for PCB and PCBA?
New customers can receive a total of $105 coupon after registration and login.
- 8. How to use the coupon for my order of PCB and PCBA?
- 9. How can I get support for PCB and PCBA?
- 10. How can you ensure the confidentiality of our PCB & PCBA files and information?
- 11. How to do the Solder-Resistance Bridges for printed circuit board?
- 12. What will you do with the English descriptions and other attachments in the zip file for the printed circuit board?
- 13. What if PCB file and Gerber file in the zip file at the same time?
- 14. How to do the Plated Edges or Slots for the printed circuit board?
- 15. Who is responsible for the issue with Software Incompatibility of the printed circuit board?
- 16. How do you deal with the markings on Base Materials?
- 17. What if my design has V-Cuts, Cutouts, Millings, and Slots for the printed circuit board?
- 18. Gerber View
- 19. What is the smallest text you can print on the boards during PCB assembly?
- 20. Can I place an order for 3-layer PCB fabrication?
- 21. How to place a repeat order correctly?
- 22. What are the design standards for the board outlines?
- 23. Can you produce printed circuit boards larger than 200mm x 250mm?
- 24. What should be considered regarding the thickness of the board outline, slots, cutouts, and milling?
- 25. What is your suggestions for boards within or less than 50mm x 50mm?
- 26. Could you tell me the maximum dimensions for assembling a PCB board? We have different sizes for various order types.
- 27. In a flex PCB design, which stiffener types do you support?
- 28. How long can a PCB board be effectively utilized?
- 29. What is the value of the FR-4 dielectric constant or relative permittivity for FR-4 used in the 1 oz, 2-layer PCB board?
- 30. Can you provide the temperature/fire class (for conformity with EN62368-1), the toxic substances (RoHS 3 statement), and the SVHC statement for my FR-4 board orders?
- 31. Can I know the layer stack values for aluminum base?
- 32. Can through-hole connectors be utilized in an aluminum PCB to link to the copper layer, or do they risk short-circuiting with the aluminum substrate?
- 33. What is the maximum temperature that could be used in the reflow oven for soldering flex PCBs?
- 34. Can you proceed without surface finishing on the PCB?
- 35. In a custom printed circuit board, what is the required file format for the drill file extension?
- 36. Our Project Involves Producing a 4-Layer Rigid PCB with a Thickness of 2mm and 2 Oz Copper Thickness on Both the Inner and Outer Layers. Is It Possible to Keep a Track Width and Clearance of 6 Mil?
- 37. Is It Required for Me to Mirror My PCB Design Before I Upload the Gerber Files, or Do You Take Care of This Automatically? It's a One-Sided PCB.
- 38. Given That We Can Only Employ Plated Through Holes (PTH) and Not Blind Vias on Four-Layer Circuit Boards, How Do We Achieve Interconnection Between the Mid Layers?
- 39. In a 2-Layer Flexible PCB, Is the Stiffener Located Between the Two Layers?
- 40. How Many Times Are Your Flexible PCBs Rated for Flexing? I Need to Choose a Flexible PCB for an Application Involving a Constantly Moving Carriage, and It’s Important to Ensure the Ratings Are Sufficient.
- 41. What documents are required for PCBA orders?
- 42. Do you support both SMD and THT components for PCB assembly?
- 43. Do you assemble boards with surface mount components on both sides?
- 44. Do you support downloading the corrected Pick and Place file for PCBA from your system?
- 45. What packages are supported by the economical PCB assembly service?
- 46. What does your quotation include for PCB assembly?
- 47. Do you support assembling THT components? What is the cost?
- 48. Do you accept components supplied by customers?
- 49. What are your requirements for the panelized board?
- 50. Do I need to add fiducial marks myself?
- 51. Do you offer assembly on boards fabricated by another company?
- 52. Do you support BGA component assembly?