{"id":4107,"date":"2026-06-09T03:14:20","date_gmt":"2026-06-09T03:14:20","guid":{"rendered":"https:\/\/blogs.lcsc.com\/blog\/?p=4107"},"modified":"2026-06-17T10:26:48","modified_gmt":"2026-06-17T10:26:48","slug":"led-1210-and-smd-1210","status":"publish","type":"post","link":"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/","title":{"rendered":"LED 1210 and SMD 1210 Components Guide"},"content":{"rendered":"<div>\n<p><a href=\"https:\/\/www.lcsc.com\/search?q=LED%25201210%2520and%2520SMD%25201210&amp;s_z=n_q_LED%25201210%2520and%2520SMD%25201210\">LED 1210 and SMD 1210 components<\/a> use a standardized package measuring 3.2 mm \u00d7 2.5 mm. The EIA imperial code represents the body size in hundredths of an inch: 0.12&#8243; \u00d7 0.10&#8243;, while the metric designation is 3225. IEC 60115-8, JEDEC, and IPC-7351 standards define the footprint specifications. In addition, the 1210 package supports various SMD components, including resistors, MLCC capacitors, ferrite beads, and LED diodes, making it one of the most versatile package formats in <a href=\"http:\/\/blogs.lcsc.com\/blog\/guide-circuit-board\">SMT applications<\/a>. Engineers widely use LED 1210 and SMD 1210 devices in automotive electronics, industrial controls, and front panel indicator circuits.<\/p>\n<\/div>\n<h2><strong>Key Takeaways<\/strong><\/h2>\n<ul>\n<li>The SMD 1210 package measures 3.2 mm \u00d7 2.5 mm and is also called 3225 in metric datasheets.<\/li>\n<li>Thick-film resistors in 1210 dissipate up to 0.5 W \u2014 double the 1206 rating.<\/li>\n<li>X7R MLCCs reach 100 V to 630 V, making 1210 essential in high-voltage snubber circuits.<\/li>\n<li>LED variants include flat chip-type and PLCC-2 \/ 3528, both suited to front panel indicator use.<\/li>\n<li>AEC-Q200 and AEC-Q102 grades support automotive and industrial qualification requirements.<\/li>\n<li>LCSC stocks 1210 components from Murata, TDK, Yageo, Cree, and Everlight, with cut-tape sampling from 1 piece.<\/li>\n<\/ul>\n<h2>What Is the SMD 1210 Component?<\/h2>\n<p>The SMD 1210 is a two-terminal chip component with a rectangular ceramic or polymer body. Metallised end-cap terminations allow it to reflow directly onto PCB pads. Standardised dimensions are 3.2 mm (L) \u00d7 2.5 mm (W), with height ranging from 0.55 mm to 1.0 mm. PCB land patterns follow IPC-7351B, with pad dimensions of approximately 1.8 mm \u00d7 3.0 mm. Additionally, a courtyard clearance of 0.25 mm keeps adjacent components safely separated.<\/p>\n<h3>Passive Variants: Resistors and Capacitors<\/h3>\n<p>The 1210 package accommodates thick-film and thin-film resistors, plus X7R and C0G MLCCs. Thick-film resistors deliver 0.5 W power dissipation at T\u2082 = 70 \u00b0C. Moreover, X7R MLCCs achieve voltage ratings up to 200 V in this footprint. The larger solder fillet area improves resistance to flex cracking and thermal cycling stress. Consequently, the 1210 consistently meets AEC-Q200 automotive qualification and IPC-A-610 Class 3 workmanship.<\/p>\n<h3>LED Variants for Front Panel Indicator Use<\/h3>\n<p>When the 1210 package houses an LED, it takes one of two distinct forms. First, the flat chip-type LED delivers 20 mcd to 300 mcd at a forward voltage of 1.8 V to 3.5 V. Second, the PLCC-2 \/ 3528 package provides a reflector cavity for higher on-axis brightness. The PLCC-2 measures 3.5 mm \u00d7 2.8 mm and suits front panel indicator and signage applications. Engineers should always verify body dimensions, lead count, and pin polarity before committing to a footprint.<\/p>\n<h2>Key Features and Advantages of the 1210 Package<\/h2>\n<h3>Higher Power Rating Than the 1206<\/h3>\n<p>The 1210 dissipates up to 0.5 W in thick-film resistor variants. That is double the typical 0.25 W limit of the smaller 1206. The larger ceramic substrate provides more thermal mass and heat-transfer surface area. In motor-drive circuits, resistors regularly operate at 60\u201380 % of rated power. Therefore, the 1210\u2019s headroom prevents derating violations and extends component life.<\/p>\n<h3>Elevated Voltage Capability for MLCC Capacitors<\/h3>\n<p>The wider 1210 body allows more dielectric layers or thicker material stacks. As a result, X7R and C0G dielectrics reach voltage ratings of 100 V to 630 V. This capability makes the package indispensable in AC-DC converter snubber circuits. Gate-drive bootstrap capacitors and high-voltage sensor conditioning networks also benefit. In contrast, the 1206 cannot match these voltage ratings at equivalent capacitance values.<\/p>\n<h3>Superior Mechanical Reliability<\/h3>\n<p>The 3.2 mm \u00d7 2.5 mm footprint produces a larger solder joint volume than smaller chip packages. Consequently, stress per unit area is lower during temperature cycling from \u221255 \u00b0C to +125 \u00b0C. That cycling range follows IEC 60068-2-14 board-level test standards. In automotive applications, the 1210 passes 1,000-cycle thermal shock profiles. Furthermore, it survives 1.5 mm peak-to-peak vibration profiles required by AEC-Q200.<\/p>\n<h3>Compatible with Standard Pick-and-Place Equipment<\/h3>\n<p>At 3.2 mm \u00d7 2.5 mm, the 1210 sits within all mainstream pick-and-place placement tolerances. Standard nozzle diameters of 1.5\u20133.0 mm handle the component without adjustment. The balanced pad geometry and symmetric thermal mass reduce tombstoning risk. That stability is critical in lead-free SAC305 reflow profiles peaking at 245\u2013260 \u00b0C. In short, the 1210 integrates smoothly into high-volume SMT assembly lines.<\/p>\n<h3>Wide Availability Across Component Types<\/h3>\n<p>The 1210 footprint is shared by resistors, MLCCs, ferrite beads, varistors, and LED diodes. Therefore, a single PCB land pattern can accommodate multiple passive functions. Designers can swap component types at the design-change stage without re-laying out the board. In addition, this cross-type compatibility reduces BOM complexity. It also simplifies second-source qualification during supply-chain disruptions.<\/p>\n<h2>Technical Specifications of LED 1210 and SMD 1210 Components<\/h2>\n<table style=\"height: 405px;\" width=\"446\">\n<tbody>\n<tr>\n<td width=\"133\"><strong>Parameter<\/strong><\/td>\n<td width=\"80\"><strong>Symbol<\/strong><\/td>\n<td width=\"120\"><strong>Typical Range<\/strong><\/td>\n<td width=\"60\"><strong>Unit<\/strong><\/td>\n<td width=\"231\"><strong>Notes<\/strong><\/td>\n<\/tr>\n<tr>\n<td width=\"133\">Body Length<\/td>\n<td width=\"80\">L<\/td>\n<td width=\"120\">3.2 (\u00b10.2)<\/td>\n<td width=\"60\">mm<\/td>\n<td width=\"231\">EIA 1210 \/ Metric 3225<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">Body Width<\/td>\n<td width=\"80\">W<\/td>\n<td width=\"120\">2.5 (\u00b10.2)<\/td>\n<td width=\"60\">mm<\/td>\n<td width=\"231\">IPC-7351B land pattern<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">Component Height<\/td>\n<td width=\"80\">H<\/td>\n<td width=\"120\">0.55 \u2013 1.00<\/td>\n<td width=\"60\">mm<\/td>\n<td width=\"231\">Varies by dielectric \/ die<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">Resistor Power Rating<\/td>\n<td width=\"80\">P<\/td>\n<td width=\"120\">0.50<\/td>\n<td width=\"60\">W<\/td>\n<td width=\"231\">Thick-film, Ta = 70 \u00b0C<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">MLCC Voltage Rating<\/td>\n<td width=\"80\">VR<\/td>\n<td width=\"120\">10 \u2013 630<\/td>\n<td width=\"60\">V<\/td>\n<td width=\"231\">Depends on dielectric class<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">LED Forward Voltage<\/td>\n<td width=\"80\">Vf<\/td>\n<td width=\"120\">1.8 \u2013 3.5<\/td>\n<td width=\"60\">V<\/td>\n<td width=\"231\">Wavel<\/p>\n<p>ength-dependent<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">LED Forward Current<\/td>\n<td width=\"80\">If<\/td>\n<td width=\"120\">20 \u2013 30<\/td>\n<td width=\"60\">mA<\/td>\n<td width=\"231\">DC; derate above Ta = 25 \u00b0C<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">Operating Temperature<\/td>\n<td width=\"80\">Ta<\/td>\n<td width=\"120\">\u221255 to +125<\/td>\n<td width=\"60\">\u00b0C<\/td>\n<td width=\"231\">AEC-Q200 capable grades<\/td>\n<\/tr>\n<\/tbody>\n<\/table>\n<p>The 1210 package covers a broad electrical performance range. Resistors span 0.01 \u03a9 to 10 M\u03a9, with thin-film tolerances as tight as \u00b10.1 %. MLCC capacitors range from 1 pF to 100 \u00b5F depending on the dielectric. Moreover, LED variants cover wavelengths from 470 nm (blue) to 660 nm (red). High-brightness emitters reach 300 mcd luminous intensity at 20 mA.<\/p>\n<h2>Customisation and Configuration Options<\/h2>\n<h3>Resistor Technologies: Thick-Film vs. Thin-Film<\/h3>\n<p>Thick-film resistors use ruthenium-oxide paste fired onto an alumina substrate. They offer tolerances of \u00b11 % or \u00b15 % and a TCR of \u00b1100\u2013200 ppm\/\u00b0C. Thin-film resistors, by contrast, deposit a nickel-chromium alloy layer under vacuum. That process achieves tolerances of \u00b10.1 % to \u00b10.5 % and TCR values of \u00b110\u201325 ppm\/\u00b0C. As a result, thin-film variants suit precision measurement bridges and analog reference dividers.<\/p>\n<h3>LED Colour, Lens, and Front Panel Indicator Configuration<\/h3>\n<p>LED variants in the 1210 footprint include red (AlGaInP), green (InGaN), blue, yellow, and white. Furthermore, bi-colour and RGB options use multi-die or PLCC-4 packages. Diffused lenses spread light across a 120\u00b0 viewing angle for wide-area front panel indicator coverage. Clear lenses, on the other hand, concentrate flux for narrower beam signage applications. Both lens types ship in tape-and-reel or tray packaging to suit high-volume SMT lines.<\/p>\n<h3>LED 1210 and SMD 1210 Procurement Formats<\/h3>\n<p>The 1210 package ships in 8 mm tape and reel per EIA-481-D at 2,500 to 10,000 pieces per reel. Tray packaging is available for PLCC-type LEDs and sampler kits. Additionally, bulk packaging supports lower-volume prototyping requirements. LCSC stocks all three formats, with cut-tape and full-reel options available for immediate despatch.<\/p>\n<h2>LED 1210 and SMD 1210 Common Application Scenarios<\/h2>\n<h3>Automotive Front Panel Indicator Backlighting<\/h3>\n<p>Dashboard PCBs operating from a 12 V automotive rail rely on 1210 LEDs for uniform backlighting. The PLCC-2 \/ 3528 front panel indicator LED maintains consistent colour temperature from \u221240 \u00b0C to +105 \u00b0C. Moreover, its reflector cavity improves on-axis brightness, reducing die count per PCB segment. Total power stays below 500 mW per segment as a result. The component also satisfies AEC-Q102 LED qualification for automotive-grade reliability.<\/p>\n<h3>Industrial Power Supply Snubber and Decoupling Networks<\/h3>\n<p>Switch-mode power supplies in DIN-rail controllers and servo drives use 1210 MLCC capacitors. Specifically, X7R types rated at 100 V to 250 V act as primary bus decoupling components. X7R ceramics lose 30\u201340 % of rated capacitance at full DC voltage. However, the 1210\u2019s larger body allows a higher nominal value, preserving effective capacitance. Consequently, the design window remains met even after DC bias derating.<\/p>\n<h3>Precision Analogue Signal Conditioning<\/h3>\n<p>Instrumentation amplifiers and Wheatstone bridge circuits require matched resistor networks. Specifically, TCR below 25 ppm\/\u00b0C is essential in industrial weighing and pressure sensing. 1210 thin-film resistors provide \u00b10.1 % tolerance and \u00b110 ppm\/\u00b0C TCR. As a result, gain error stays below 10 ppm across the operating temperature range. That precision level is critical for 16-bit ADC measurement systems.<\/p>\n<h3>Front Panel Indicator for Consumer Electronics Status Display<\/h3>\n<p>In household appliances and gaming peripherals, 1210 chip LEDs serve as power and fault indicators. The 1210 front panel indicator is compatible with lead-free SAC305 and low-temperature SnBi alloys. Furthermore, its 50,000+ hour rated lifespan reduces field return rates. It also simplifies compliance with RoHS Directive 2011\/65\/EU. Therefore, designers can meet sustainability requirements without sacrificing indicator performance.<\/p>\n<h2>Manufacturing and Procurement<\/h2>\n<p>The 1210 component family is manufactured under AEC-Q200 (passives), AEC-Q102 (LEDs), and JEDEC JESD22 standards. Key qualification tests include MSL assessment per IPC\/JEDEC J-STD-020 and thermal shock per IEC 60068-2-14. Board-level drop testing follows JEDEC JESD22-B111. Additionally, RoHS and REACH compliance certificates are required for EU market entry. Halogen-free variants are mandated by major OEM supply agreements in automotive and telecom sectors.<\/p>\n<p>LCSC sources 1210 components from verified manufacturers including <a href=\"http:\/\/lcsc.com\/brand-detail\/79.html?s_z=n_q_Murata&amp;globalKeyword=Murata\">Murata<\/a>, TDK, Yageo, Walsin, Cree, and Everlight. Full traceability to date codes and factory lot numbers is maintained throughout. Standard lead times for high-runner 1210 resistor and MLCC values are 1\u20133 business days from stock. However, specialised thin-film or automotive-grade parts may carry 4\u20138 week lead times. MOQ starts at a single cut-tape piece for sampling, with full-reel pricing at 2,500+ pieces.<\/p>\n<p>When procuring 1210 components, engineers should specify the dielectric class for MLCCs explicitly. Similarly, the TCR grade for resistors and dominant wavelength tolerance for LEDs must be stated. Price and availability vary significantly across grades. Moreover, cross-referencing with IPC land-pattern libraries before a first-article order reduces PCB re-spin risk. That step accelerates time-to-production and lowers qualification cost.<\/p>\n<h2>Type and Variant Comparison<\/h2>\n<table style=\"height: 415px;\" width=\"485\">\n<tbody>\n<tr>\n<td width=\"133\"><strong>Type<\/strong><\/td>\n<td width=\"147\"><strong>Key Spec<\/strong><\/td>\n<td width=\"173\"><strong>Best For<\/strong><\/td>\n<td width=\"171\"><strong>Trade-off<\/strong><\/td>\n<\/tr>\n<tr>\n<td width=\"133\">1210 Thick-Film Resistor<\/td>\n<td width=\"147\">0.5 W, \u00b11 %, 100\u2013200 ppm\/\u00b0C TCR<\/td>\n<td width=\"173\">Power-stage bias, current sensing<\/td>\n<td width=\"171\">Lower precision vs. thin-film<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">1210 Thin-Film Resistor<\/td>\n<td width=\"147\">0.25 W, \u00b10.1 %, \u00b110 ppm\/\u00b0C TCR<\/td>\n<td width=\"173\">Precision analogue, bridge networks<\/td>\n<td width=\"171\">Higher cost, lower power rating<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">1210 MLCC (X7R)<\/td>\n<td width=\"147\">1 \u00b5F \u2013 47 \u00b5F, 10\u2013100 V<\/td>\n<td width=\"173\">Bulk decoupling, snubber, filtering<\/td>\n<td width=\"171\">Capacitance loss under DC bias<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">1210 MLCC (C0G\/NP0)<\/td>\n<td width=\"147\">1 pF \u2013 100 nF, up to 200 V<\/td>\n<td width=\"173\">Resonant circuits, timing, RF filtering<\/td>\n<td width=\"171\">Lower max capacitance vs. X7R<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">1210 Chip LED<\/td>\n<td width=\"147\">20\u201330 mA, Vf 1.8\u20133.5 V, up to 300 mcd<\/td>\n<td width=\"173\">Front panel indicator, backlight arrays<\/td>\n<td width=\"171\">Lower intensity vs. PLCC-2<\/td>\n<\/tr>\n<tr>\n<td width=\"133\">1210 \/ PLCC-2 LED (3528)<\/td>\n<td width=\"147\">20\u201330 mA, J-lead, reflector cavity<\/td>\n<td width=\"173\">Automotive clusters, high-brightness front panel indicator<\/td>\n<td width=\"171\">Larger footprint; easier to hand-solder<\/td>\n<\/tr>\n<\/tbody>\n<\/table>\n<p>For general-purpose passive applications, the 1210 X7R MLCC and thick-film resistor offer the best cost-performance balance. Where accuracy is paramount, specify thin-film resistors and C0G capacitors instead. For front panel indicator applications requiring automotive qualification, select the PLCC-2 \/ 3528 with AEC-Q102 rating.<\/p>\n<h2>Frequently Asked Questions<\/h2>\n<h3>How do I calculate the series resistor for a 1210 LED on a 3.3 V supply?<\/h3>\n<p>Use Ohm\u2019s law: R = (Vsupply \u2212 Vf) \/ If. For a red 1210 LED with Vf = 2.0 V at If = 20 mA, R = (3.3 \u2212 2.0) \/ 0.020 = 65 \u03a9. Therefore, select the nearest E24 standard value of 68 \u03a9. Power dissipation is P = If\u00b2 \u00d7 R = 27 mW, so the 1210 0.5 W resistor provides ample margin. For white or blue LEDs where Vf \u2248 3.2 V from a 3.3 V rail, headroom is only 100 mV. Consequently, limit forward current to 5\u201310 mA and verify the minimum If in the datasheet first.<\/p>\n<h3>What standards govern the SMD 1210 footprint and land pattern dimensions?<\/h3>\n<p>The package code \u201c1210\u201d originates from the EIA imperial chip-package naming system. Metric equivalent dimensions (3225) follow IEC 60115-8 for resistors. Furthermore, recommended PCB land patterns are defined in IPC-7351B. Automotive-grade reliability testing references AEC-Q200 for passives and AEC-Q102 for LEDs. Board-level assembly workmanship is assessed to IPC-A-610 Class 2 or Class 3, depending on the application.<\/p>\n<h3>What is the expected operational lifetime of a 1210 front panel indicator LED?<\/h3>\n<p>High-quality 1210 LED components are rated for 50,000 hours of continuous operation at 25 \u00b0C ambient. That equals approximately 5.7 years of 24\/7 use. However, at an 85 \u00b0C junction temperature, lifetime may reduce to 20,000\u201330,000 hours. Arrhenius degradation modelling explains this reduction. Moreover, operating at 10\u201315 mA instead of the 20 mA maximum extends useful life significantly. It also reduces thermal stress on the phosphor layer in white front panel indicator LEDs.<\/p>\n<h3>When should I choose a 1210 MLCC over a 1206 for decoupling?<\/h3>\n<p>Select the 1210 when the 1206 cannot meet voltage derating requirements. X7R ceramics lose 30\u201340 % of rated capacitance at full DC voltage. For example, a 10 \u00b5F \/ 50 V X7R in 1210 delivers approximately 6\u20137 \u00b5F at a 48 V bus. That still meets many decoupling targets where a 1206 10 \u00b5F \/ 25 V part would fall short. Additionally, the 1210 is preferred in high-voltage snubber positions rated at 200 V to 630 V. Those ratings are not available in 1206 at equivalent capacitance values.<\/p>\n<h3>How do I source LED 1210 and SMD 1210 components from LCSC and what are typical MOQs?<\/h3>\n<p>LCSC lists 1210 resistors, MLCC capacitors, and LED diodes from multiple verified manufacturers. Real-time stock visibility makes it straightforward to confirm availability before ordering. Cut-tape samples start from as little as one piece, suiting both prototype and production workflows. Full-reel pricing at 2,500 pieces provides the lowest unit cost. Furthermore, LCSC provides RoHS compliance certificates, material declarations, and production lot traceability. Delivery within mainland China is typically 1\u20133 business days; international timelines depend on the logistics tier.<\/p>\n<h2>Conclusion: Choosing the Right LED 1210 and SMD 1210 Component<\/h2>\n<p>The 1210 SMD package offers a versatile, reliable foundation for resistors, MLCCs, and <a href=\"https:\/\/blogs.lcsc.com\/blog\/tvs-diodes-explained-the-definitive-guide-to-transient-voltage-protection\">LED diodes<\/a>. For power-stage bias, choose the thick-film resistor variant. For precision analogue circuits, specify thin-film instead. And for high-voltage decoupling, the X7R MLCC in 1210 outperforms smaller package alternatives. Finally, for front panel indicator and automotive backlighting, the PLCC-2 \/ 3528 with AEC-Q102 rating is the engineering-grade choice.<\/p>\n<h2>Find What You Need on <a href=\"http:\/\/lcsc.com\">LCSC<\/a><\/h2>\n<p>LCSC stocks a comprehensive range of 1210 resistors, MLCC capacitors, and LED diodes from verified manufacturers including Murata, TDK, Yageo, Cree, and Everlight. Cut-tape sampling starts from just one piece, and full-reel orders ship within 1\u20133 business days. Browse the 1210 component category on LCSC to compare specs, check real-time stock, and place your order today.<\/p>\n","protected":false},"excerpt":{"rendered":"<p>LED 1210 and SMD 1210 components use a standardized package measuring 3.2 mm \u00d7 2.5 mm. The EIA imperial code represents the body size in hundredths of an inch: 0.12&#8243; \u00d7 0.10&#8243;, while the metric designation is 3225. IEC 60115-8, JEDEC, and IPC-7351 standards define the footprint specifications. In addition, the 1210 package supports various [&hellip;]<\/p>\n","protected":false},"author":3,"featured_media":0,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"_monsterinsights_skip_tracking":false,"footnotes":""},"categories":[27],"tags":[289,339,338],"class_list":["post-4107","post","type-post","status-publish","format-standard","hentry","category-electronic-components","tag-electronic-components","tag-led-1210","tag-smd-1210"],"blocksy_meta":[],"yoast_head":"<!-- This site is optimized with the Yoast SEO plugin v27.8 - https:\/\/yoast.com\/product\/yoast-seo-wordpress\/ -->\n<title>LED 1210 and SMD 1210 Components - LCSC<\/title>\n<meta name=\"description\" content=\"Learn about LED 1210 and SMD 1210 components, including package size, specs, applications, and sourcing tips for PCB designs.\" \/>\n<meta name=\"robots\" content=\"index, follow, max-snippet:-1, max-image-preview:large, max-video-preview:-1\" \/>\n<link rel=\"canonical\" href=\"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/\" \/>\n<meta property=\"og:locale\" content=\"en_US\" \/>\n<meta property=\"og:type\" content=\"article\" \/>\n<meta property=\"og:title\" content=\"LED 1210 and SMD 1210 Components - LCSC\" \/>\n<meta property=\"og:description\" content=\"Learn about LED 1210 and SMD 1210 components, including package size, specs, applications, and sourcing tips for PCB designs.\" \/>\n<meta property=\"og:url\" content=\"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/\" \/>\n<meta property=\"og:site_name\" content=\"Blog | LCSC Electronics\" \/>\n<meta property=\"article:published_time\" content=\"2026-06-09T03:14:20+00:00\" \/>\n<meta property=\"article:modified_time\" content=\"2026-06-17T10:26:48+00:00\" \/>\n<meta name=\"author\" content=\"LCSC Editor\" \/>\n<meta name=\"twitter:card\" content=\"summary_large_image\" \/>\n<meta name=\"twitter:label1\" content=\"Written by\" \/>\n\t<meta name=\"twitter:data1\" content=\"LCSC Editor\" \/>\n\t<meta name=\"twitter:label2\" content=\"Est. reading time\" \/>\n\t<meta name=\"twitter:data2\" content=\"11 minutes\" \/>\n<script type=\"application\/ld+json\" class=\"yoast-schema-graph\">{\"@context\":\"https:\\\/\\\/schema.org\",\"@graph\":[{\"@type\":\"Article\",\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/led-1210-and-smd-1210\\\/#article\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/led-1210-and-smd-1210\\\/\"},\"author\":{\"name\":\"LCSC Editor\",\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/#\\\/schema\\\/person\\\/11d3b92d0208775e62d7f79a0da4e781\"},\"headline\":\"LED 1210 and SMD 1210 Components Guide\",\"datePublished\":\"2026-06-09T03:14:20+00:00\",\"dateModified\":\"2026-06-17T10:26:48+00:00\",\"mainEntityOfPage\":{\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/led-1210-and-smd-1210\\\/\"},\"wordCount\":2128,\"commentCount\":0,\"publisher\":{\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/#organization\"},\"keywords\":[\"Electronic Components\",\"LED 1210\",\"SMD 1210\"],\"articleSection\":[\"Electronic Components\"],\"inLanguage\":\"en-US\",\"potentialAction\":[{\"@type\":\"CommentAction\",\"name\":\"Comment\",\"target\":[\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/led-1210-and-smd-1210\\\/#respond\"]}]},{\"@type\":\"WebPage\",\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/led-1210-and-smd-1210\\\/\",\"url\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/led-1210-and-smd-1210\\\/\",\"name\":\"LED 1210 and SMD 1210 Components - LCSC\",\"isPartOf\":{\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/#website\"},\"datePublished\":\"2026-06-09T03:14:20+00:00\",\"dateModified\":\"2026-06-17T10:26:48+00:00\",\"description\":\"Learn about LED 1210 and SMD 1210 components, including package size, specs, applications, and sourcing tips for PCB designs.\",\"breadcrumb\":{\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/led-1210-and-smd-1210\\\/#breadcrumb\"},\"inLanguage\":\"en-US\",\"potentialAction\":[{\"@type\":\"ReadAction\",\"target\":[\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/led-1210-and-smd-1210\\\/\"]}]},{\"@type\":\"BreadcrumbList\",\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/led-1210-and-smd-1210\\\/#breadcrumb\",\"itemListElement\":[{\"@type\":\"ListItem\",\"position\":1,\"name\":\"Home\",\"item\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/\"},{\"@type\":\"ListItem\",\"position\":2,\"name\":\"LED 1210 and SMD 1210 Components Guide\"}]},{\"@type\":\"WebSite\",\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/#website\",\"url\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/\",\"name\":\"Blog | LCSC Electronics\",\"description\":\"LCSC Electronics Blogs and News\",\"publisher\":{\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/#organization\"},\"potentialAction\":[{\"@type\":\"SearchAction\",\"target\":{\"@type\":\"EntryPoint\",\"urlTemplate\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/?s={search_term_string}\"},\"query-input\":{\"@type\":\"PropertyValueSpecification\",\"valueRequired\":true,\"valueName\":\"search_term_string\"}}],\"inLanguage\":\"en-US\"},{\"@type\":\"Organization\",\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/#organization\",\"name\":\"Blog | LCSC Electronics\",\"url\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/\",\"logo\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-US\",\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/#\\\/schema\\\/logo\\\/image\\\/\",\"url\":\"https:\\\/\\\/blogs.lcsc.com\\\/wp-content\\\/uploads\\\/2023\\\/10\\\/logo.png\",\"contentUrl\":\"https:\\\/\\\/blogs.lcsc.com\\\/wp-content\\\/uploads\\\/2023\\\/10\\\/logo.png\",\"width\":939,\"height\":180,\"caption\":\"Blog | LCSC Electronics\"},\"image\":{\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/#\\\/schema\\\/logo\\\/image\\\/\"}},{\"@type\":\"Person\",\"@id\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/#\\\/schema\\\/person\\\/11d3b92d0208775e62d7f79a0da4e781\",\"name\":\"LCSC Editor\",\"image\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-US\",\"@id\":\"https:\\\/\\\/secure.gravatar.com\\\/avatar\\\/0c5d2ddc240c300192ecdc04c2d2f7914d4b02bd00ea81b32e98b698c49e357f?s=96&d=mm&r=g\",\"url\":\"https:\\\/\\\/secure.gravatar.com\\\/avatar\\\/0c5d2ddc240c300192ecdc04c2d2f7914d4b02bd00ea81b32e98b698c49e357f?s=96&d=mm&r=g\",\"contentUrl\":\"https:\\\/\\\/secure.gravatar.com\\\/avatar\\\/0c5d2ddc240c300192ecdc04c2d2f7914d4b02bd00ea81b32e98b698c49e357f?s=96&d=mm&r=g\",\"caption\":\"LCSC Editor\"},\"url\":\"https:\\\/\\\/blogs.lcsc.com\\\/blog\\\/author\\\/lcsc-editor\\\/\"}]}<\/script>\n<!-- \/ Yoast SEO plugin. -->","yoast_head_json":{"title":"LED 1210 and SMD 1210 Components - LCSC","description":"Learn about LED 1210 and SMD 1210 components, including package size, specs, applications, and sourcing tips for PCB designs.","robots":{"index":"index","follow":"follow","max-snippet":"max-snippet:-1","max-image-preview":"max-image-preview:large","max-video-preview":"max-video-preview:-1"},"canonical":"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/","og_locale":"en_US","og_type":"article","og_title":"LED 1210 and SMD 1210 Components - LCSC","og_description":"Learn about LED 1210 and SMD 1210 components, including package size, specs, applications, and sourcing tips for PCB designs.","og_url":"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/","og_site_name":"Blog | LCSC Electronics","article_published_time":"2026-06-09T03:14:20+00:00","article_modified_time":"2026-06-17T10:26:48+00:00","author":"LCSC Editor","twitter_card":"summary_large_image","twitter_misc":{"Written by":"LCSC Editor","Est. reading time":"11 minutes"},"schema":{"@context":"https:\/\/schema.org","@graph":[{"@type":"Article","@id":"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/#article","isPartOf":{"@id":"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/"},"author":{"name":"LCSC Editor","@id":"https:\/\/blogs.lcsc.com\/blog\/#\/schema\/person\/11d3b92d0208775e62d7f79a0da4e781"},"headline":"LED 1210 and SMD 1210 Components Guide","datePublished":"2026-06-09T03:14:20+00:00","dateModified":"2026-06-17T10:26:48+00:00","mainEntityOfPage":{"@id":"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/"},"wordCount":2128,"commentCount":0,"publisher":{"@id":"https:\/\/blogs.lcsc.com\/blog\/#organization"},"keywords":["Electronic Components","LED 1210","SMD 1210"],"articleSection":["Electronic Components"],"inLanguage":"en-US","potentialAction":[{"@type":"CommentAction","name":"Comment","target":["https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/#respond"]}]},{"@type":"WebPage","@id":"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/","url":"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/","name":"LED 1210 and SMD 1210 Components - LCSC","isPartOf":{"@id":"https:\/\/blogs.lcsc.com\/blog\/#website"},"datePublished":"2026-06-09T03:14:20+00:00","dateModified":"2026-06-17T10:26:48+00:00","description":"Learn about LED 1210 and SMD 1210 components, including package size, specs, applications, and sourcing tips for PCB designs.","breadcrumb":{"@id":"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/#breadcrumb"},"inLanguage":"en-US","potentialAction":[{"@type":"ReadAction","target":["https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/"]}]},{"@type":"BreadcrumbList","@id":"https:\/\/blogs.lcsc.com\/blog\/led-1210-and-smd-1210\/#breadcrumb","itemListElement":[{"@type":"ListItem","position":1,"name":"Home","item":"https:\/\/blogs.lcsc.com\/blog\/"},{"@type":"ListItem","position":2,"name":"LED 1210 and SMD 1210 Components Guide"}]},{"@type":"WebSite","@id":"https:\/\/blogs.lcsc.com\/blog\/#website","url":"https:\/\/blogs.lcsc.com\/blog\/","name":"Blog | LCSC Electronics","description":"LCSC Electronics Blogs and News","publisher":{"@id":"https:\/\/blogs.lcsc.com\/blog\/#organization"},"potentialAction":[{"@type":"SearchAction","target":{"@type":"EntryPoint","urlTemplate":"https:\/\/blogs.lcsc.com\/blog\/?s={search_term_string}"},"query-input":{"@type":"PropertyValueSpecification","valueRequired":true,"valueName":"search_term_string"}}],"inLanguage":"en-US"},{"@type":"Organization","@id":"https:\/\/blogs.lcsc.com\/blog\/#organization","name":"Blog | LCSC Electronics","url":"https:\/\/blogs.lcsc.com\/blog\/","logo":{"@type":"ImageObject","inLanguage":"en-US","@id":"https:\/\/blogs.lcsc.com\/blog\/#\/schema\/logo\/image\/","url":"https:\/\/blogs.lcsc.com\/wp-content\/uploads\/2023\/10\/logo.png","contentUrl":"https:\/\/blogs.lcsc.com\/wp-content\/uploads\/2023\/10\/logo.png","width":939,"height":180,"caption":"Blog | LCSC Electronics"},"image":{"@id":"https:\/\/blogs.lcsc.com\/blog\/#\/schema\/logo\/image\/"}},{"@type":"Person","@id":"https:\/\/blogs.lcsc.com\/blog\/#\/schema\/person\/11d3b92d0208775e62d7f79a0da4e781","name":"LCSC Editor","image":{"@type":"ImageObject","inLanguage":"en-US","@id":"https:\/\/secure.gravatar.com\/avatar\/0c5d2ddc240c300192ecdc04c2d2f7914d4b02bd00ea81b32e98b698c49e357f?s=96&d=mm&r=g","url":"https:\/\/secure.gravatar.com\/avatar\/0c5d2ddc240c300192ecdc04c2d2f7914d4b02bd00ea81b32e98b698c49e357f?s=96&d=mm&r=g","contentUrl":"https:\/\/secure.gravatar.com\/avatar\/0c5d2ddc240c300192ecdc04c2d2f7914d4b02bd00ea81b32e98b698c49e357f?s=96&d=mm&r=g","caption":"LCSC Editor"},"url":"https:\/\/blogs.lcsc.com\/blog\/author\/lcsc-editor\/"}]}},"_links":{"self":[{"href":"https:\/\/blogs.lcsc.com\/blog\/wp-json\/wp\/v2\/posts\/4107","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.lcsc.com\/blog\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.lcsc.com\/blog\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.lcsc.com\/blog\/wp-json\/wp\/v2\/users\/3"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.lcsc.com\/blog\/wp-json\/wp\/v2\/comments?post=4107"}],"version-history":[{"count":3,"href":"https:\/\/blogs.lcsc.com\/blog\/wp-json\/wp\/v2\/posts\/4107\/revisions"}],"predecessor-version":[{"id":4216,"href":"https:\/\/blogs.lcsc.com\/blog\/wp-json\/wp\/v2\/posts\/4107\/revisions\/4216"}],"wp:attachment":[{"href":"https:\/\/blogs.lcsc.com\/blog\/wp-json\/wp\/v2\/media?parent=4107"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.lcsc.com\/blog\/wp-json\/wp\/v2\/categories?post=4107"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.lcsc.com\/blog\/wp-json\/wp\/v2\/tags?post=4107"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}