Key Takeaways
-
Core Sensor Types:
-
Thermocouples: Best for extreme temperatures (well above 1000 °C); fast response and low cost, but require cold junction compensation.
-
Pt100 RTDs: Offer the highest accuracy and stability across mid-to-high temperature ranges.
-
NTC Thermistors: Cost-effective solution suited for moderate temperature ranges.
-
Digital Sensors (ICs): Simplify system design by integrating signal processing and digital communication.
-
-
Selection Factors: Choose the right sensor based on temperature range, accuracy requirements, cost constraints, and circuit interface ease.
What Is a Temperature Sensor and How Does It Work?
A temperature sensor converts a thermal quantity into an electrical signal that a circuit can read. That signal can be a voltage (thermocouple), a resistance (RTD and thermistor), or digital data (sensor IC).
There are four main families:
- Thermocouples: two dissimilar metals joined together that generate a millivolt-level voltage (the Seebeck effect).
- RTDs (Resistance Temperature Detectors): a platinum wire or thin film whose resistance rises almost linearly with temperature.
- NTC thermistors: ceramic semiconductors whose resistance drops as they heat up, with very high sensitivity.
- Sensor ICs: chips that integrate the sensing element, converter, and interface (I²C, SPI, or 1-Wire).
Types of Thermocouples: K, J, T, N and S
The types of thermocouples are identified by a standardized letter. Their voltage-to-temperature reference tables are defined by IEC 60584-1 and the NIST ITS-90 tables.
| Type | Alloys | Typical range | Common use |
| K | Nickel-chromium / nickel-aluminum | -200 °C to +1250 °C | General purpose, industrial |
| J | I | -40 °C to +750 °C | Legacy machinery, plastics |
| T | Copper/constantan | -200 °C to +350 °C | Refrigeration, laboratory |
| N | Nicrosil / Nisil | -200 °C to +1300 °C | Stable high-temperature use |
| S | Platinum-10 % rhodium / platinum | 0 °C to +1600 °C | Furnaces, metallurgy |
K-Type Thermocouple
The K-type thermocouple is the most popular because of its wide range, low price and availability in probes, wire, and connectors. It produces about 41 µV per degree Celsius, so the signal is tiny and calls for a low-noise amplifier or a dedicated converter.
Its limitations are moderate accuracy (typically ±1.5 °C or ±0.4 % depending on the tolerance class) and slight drift after prolonged exposure to high temperatures.
Cold Junction Compensation
A thermocouple does not measure absolute temperature. It measures the difference between the hot tip and the point where the wires reach your circuit. That is why you need cold junction compensation: measure the temperature at that connection point and add it to the reading.
You can do this with an auxiliary sensor (for example, an NTC or a sensor IC placed next to the connector) or use a chip that already includes it, as covered below. Without compensation, the error can reach tens of degrees.
Thermocouple Alternatives: RTDs, Thermistors and Digital Sensors
A thermocouple is not always the best choice. Below roughly 150 °C, there are options that are more accurate or easier to integrate.
Pt100 and Pt1000 RTDs
A Pt100 RTD has 100 Ω at 0 °C and a temperature coefficient of 0.00385 Ω/Ω/°C under IEC 60751. It covers -200 °C to +850 °C with excellent stability and repeatability. The Pt1000 (1000 Ω at 0 °C) is less affected by lead-wire resistance.
You need a stable excitation source and a 3-wire or 4-wire connection to cancel wiring resistance. Keep the current below 1 mA to avoid self-heating.
NTC Thermistors
A typical NTC thermistor rated 10 kΩ at 25 °C is cheap, small, and very sensitive. It works well from -40 °C to +125 °C, although its response is nonlinear and is modeled with the Steinhart-Hart equation or the Beta parameter.
It is the usual choice for batteries, power supplies, chargers, and fan control. All you need is a resistor divider and an ADC.
Digital Temperature Sensors
Digital temperature sensors integrate all the signal conditioning. A few examples:
- DS18B20 (Analog Devices/Maxim): 1-Wire bus, 9- to 12-bit resolution, -55 °C to +125 °C range.
- TMP117 (Texas Instruments): I²C, 16-bit, ±0.1 °C accuracy from -20 °C to +50 °C.
- LM75 and derivatives: I²C with an alarm output, ideal for board-level thermal protection.
They save design time and avoid calibration errors, but their range is limited by the chip package, normally up to 125 °C or 150 °C.
Temperature Sensor Comparison Table
| Feature | K-type thermocouple | Pt100 RTD | NTC thermistor | Digital sensor IC |
| Typical range | -200 to +1250 °C | -200 to +850 °C | -40 to +125 °C | -55 to +150 °C |
| Accuracy | ±1.5 to ±2.5 °C | ±0.15 to ±0.3 °C | ±0.5 to ±1 °C | ±0.1 to ±2 °C |
| Linearity | Medium | High | Low | Handled internally |
| Response time | Very fast | Medium | Fast | Slow (package) |
| Cost | Low | Medium-high | Very low | Low-medium |
| Required circuitry | Converter + cold junction | Excitation + ADC | Divider + ADC | None |
| Best for | High temperatures | Industrial precision | Consumer electronics | Boards and embedded systems |
As a rule of thumb: above 200 °C, use a thermocouple; if you need precision between -50 °C and 500 °C, choose an RTD; if you are monitoring a board or battery, an NTC or a sensor IC is enough.
How to Connect a Thermocouple to a Microcontroller
The simplest way to read a thermocouple is a dedicated converter that amplifies the signal, digitizes it, and applies cold junction compensation in one chip.
MAX31855 and MAX31856
According to its datasheet, the MAX31855 from Analog Devices (formerly Maxim) converts the signal from K, J, N, T, S, R, or E thermocouples into a 14-bit digital word with 0.25 °C resolution. It includes cold junction compensation, communicates over a read-only SPI interface and detects an open thermocouple or a short to GND or VCC. It runs from 3.0 V to 3.6 V and comes in an SO-8 package.
At LCSC you can find, for example, the T-type variant MAX31855TASA+T (C476183, SO-8). For other types, look for the matching letter in the part number (KASA, JASA, NASA, SASA). If you need higher resolution or support for more thermocouple types in a single part number, evaluate the MAX31856.
For RTDs, the MAX31865 plays the same role with Pt100 and Pt1000 probes [verify availability and LCSC part number].
PCB Best Practices for Temperature Measurement
An accurate reading depends on layout as much as on the chip. Follow these steps:
- Place a 0.1 µF capacitor between VCC and GND, as close as possible to the converter.
- Keep the converter and the connector isothermal. Both must be at the same temperature for the cold junction to be correct.
- Keep the chip away from heat sources such as linear regulators, power MOSFETs, and inductors.
- Use twisted or shielded wire for the thermocouple line, and avoid long analog traces near switching lines.
- Use connectors and extension wire made of the same material as the thermocouple. A copper splice adds an extra junction and a reading error.
- Add a simple RC filter on the inputs if you work in noisy environments such as motors or drives.
Frequently Asked Questions
Q: What is the difference between a thermocouple and an RTD?
A thermocouple generates a voltage from the temperature difference between two junctions and covers very high ranges. An RTD changes its resistance and offers better accuracy and stability, but over a smaller range and at a higher cost.
Q: Why is my thermocouple giving a wrong reading?
The most common causes are missing cold junction compensation, splices made of dissimilar metals, electrical noise on the line, or a tip with poor thermal contact. Check connectors and wiring first.
Q: Can I use an NTC thermistor instead of a digital sensor?
Yes, if you accept linearizing the signal in software and calibrating the sensor. It is cheaper, but it requires a good ADC and a stable resistor divider.
Q: Which thermocouple is best for an electronics project?
The K type is the most practical choice for its range, price, and availability. Pair it with a converter such as the MAX31855 to simplify the design.
Conclusion
No single sensor fits every case. Thermocouples dominate at high temperatures, RTDs in precision, NTCs in cost and sensor ICs in ease of integration. Define the range, accuracy, and interface you need first, then pick the component.
Explore the LCSC catalog: find thermocouple converters, digital temperature sensors, NTC thermistors and probe connectors, with worldwide shipping and wide stock availability. If you design your PCB with LCSCPCB, you can add these components to your assembly order.