Nozzle is a device designed to control the direction, velocity, and pressure of fluids—such as liquids or gases—as they flow through an opening. Typically, they consist of a pipe or tube with varying cross-sectional areas, allowing for precise manipulation of fluid dynamics. By adjusting these parameters, nozzles can increase fluid velocity at the expense of pressure energy, effectively converting pressure into kinetic energy.
Spray Patterns and Typical Applications
Engineers design spray nozzles to disperse liquids into specific spray patterns, optimizing coverage and efficiency for various applications. The choice of spray pattern is pivotal, as it directly influences the effectiveness of processes such as coating, cooling, cleaning, and humidification. Below is an overview of common spray patterns and their typical applications:
- Flat Fan Spray Pattern
Description: Produces a thin, flat sheet of spray with a tapered distribution, meaning the liquid is more concentrated at the center and decreases towards the edges.
Applications: Ideal for processes requiring uniform coverage over a linear area, such as conveyor belt washing, coating, or wetting applications.
- Full Cone Spray Pattern
Description: Delivers a solid cone-shaped spray with a circular impact area, providing full coverage within the defined perimeter.
Applications: Suitable for cleaning, cooling, and chemical applications where complete area coverage is essential.
- Hollow Cone Spray Pattern
Description: Creates a ring-like spray pattern with droplets concentrated around the outer edge, leaving the center relatively void of liquid.
Applications: Commonly used in gas cooling, gas scrubbing, and dust control due to the increased air-to-liquid interface provided by the smaller droplets.
- Solid Stream Spray Pattern
Description: Emits a concentrated, unbroken stream of liquid, achieving the highest impact per unit area among spray patterns.
Applications: Utilized in applications requiring focused impact, such as high-pressure cleaning and cutting operations.
- Mist/Fog Spray Pattern
Description: Generates extremely fine droplets, resulting in a mist or fog-like appearance.
Applications: Effective in humidification, cooling, and certain coating processes where fine droplet distribution is crucial.

Factors such as nozzle design, liquid properties, and operating conditions determine the characteristics of a spray pattern. Choosing the right nozzle involves considering the desired spray pattern, application requirements, and operating conditions.
Applications of Nozzle in PCB Manufacturing
Nozzles play a crucial role in various stages of Printed Circuit Board (PCB) manufacturing, ensuring precision and efficiency in each process.
- Cleaning and Surface Preparation:
Before any components are mounted, PCBs must be meticulously cleaned to remove contaminants that could affect performance. Hollow cone nozzles are employed to produce a fine spray mist, effectively moistening wafers post-sawing. This mist prevents impurities from drying onto the wafer, thereby ensuring an efficient production process.
- Component Placement:
The assembly process involves placing numerous electronic components onto the PCB with high precision. Pick-and-place machines utilize vacuum nozzles to handle this task. These nozzles pick up components from feeders and accurately position them onto the board. The design and material of these precision nozzles are crucial, as they must handle components of varying sizes and shapes without causing damage.
- Soldering:
Attaching components securely to the PCB requires precise soldering techniques, where nozzles are integral.
Selective Wave Soldering: This process uses specialized nozzles to apply solder only to specific areas, minimizing thermal stress and reducing the risk of solder bridging. Choosing the appropriate nozzle design is essential for achieving optimal solder flow and joint quality.
Ultrasonic Nozzles: In certain applications, ultrasonic nozzles are used to spray flux uniformly onto the PCB before soldering. This ensures proper adhesion and electrical connectivity of components.

- Surface Treatment
To enhance the adhesion of coatings or to modify surface properties, plasma surface treatment is employed. Rotary nozzle plasma systems treat the PCB surface uniformly, improving the bonding of subsequent layers or components.
In Short
Nozzle is an integral to various stages of PCB preparation, from cleaning and component placement to soldering and surface treatment. Their precise design and application ensure the reliability and performance of the final electronic assemblies.
Some images are sourced online. Please contact us for removal if any copyright concerns arise.
Custom Cables: Save 50%+ Avg Cost By JST, Molex, TE Alternatives | Processing Fee Down to $1 Per Piece | No Minimum Order Quantity (MOQ) Required
PCB & PCBA: New Customer Get Coupons Up to $125 | 1 – 32 Layers From $2 /5pcs | PCB Assembly From $8 /5pcs
Front Panels: High-quality Front Panel Acrylic/PET | Front Panel Order Up to 30% Off | Membrane Switch Available Soon