Selective Soldering: Key to Modern PCB Manufacturing And Assembly (Part Two)

Have you ever faced issues with unstable equipment performance or inefficient production due to soldering process challenges when developing electronic products? – Selective soldering is the key.

It’s a core technology in modern PCBA (Printed Circuit Board Assembly) manufacturing, not only allowing precise control over soldering quality but also significantly improving production efficiency and product reliability.

Selective Soldering Process in PCB Production
Selective Soldering Process in PCB Production (Image source: online)

What is the principle behind selective soldering? How does it help solve soldering challenges in practical applications? This article will unveil the mystery of selective soldering through a detailed analysis of the flux system, preheating module, and soldering module, while exploring its practical application in embedded systems like Raspberry Pi development boards.

Working Principle and Equipment of Selective Soldering

Selective soldering involves three modules: the flux system, the preheating module, and the soldering module.

Flux System

Flux is an auxiliary material in the soldering process, but excessive use can increase solder joint residue and even affect circuit performance. Incomplete cleaning of flux residues can hence cause a series of negative consequences:

  • Incomplete Reaction: After reflow soldering, the flux may not undergo a full chemical reaction, further leading to residue buildup.
  • Insufficient Cleaning: Even after cleaning processes, some flux residues may remain, potentially affecting the long-term reliability of the PCB.
  • Impact on Reliability: In harsh environments that require coatings or encapsulation, residues may reduce the adhesion of coatings or potting materials to the substrate.
Excessive flux on the single-row connector, which may affect the PCB if not subjected to a solder-washing process
Excessive flux on the single-row connector, which may affect the PCB if not subjected to a solder-washing process (Image source: online)
  • Dendritic Growth: Residues could cause the growth of conductive dendrites beneath the coating, leading to potential risk of short circuits or failures.
Flux residue beneath the coating leads to the growth of conductive dendrites, posing a potential risk of short circuits or component failure.
Flux residue beneath the coating leads to the growth of conductive dendrites, posing a potential risk of short circuits or component failure. (Image source: online)

The selective soldering system uses advanced inkjet technology in order to accurately apply flux to the solder joints, effectively reducing the risk of residue and optimizing soldering quality.

  • Precise Application: Flux is applied in small dots using an inkjet nozzle, preventing the risk of excessive flux usage that commonly used in traditional atomization methods.
  • Reduced Contamination: The non-soldering areas, such as copper foil contacts on the keyboard or COD bonding surfaces, remain unaffected, ensuring the cleanliness of the PCB surface.
  • Optimized Cleanliness: Precise control of the flux reduces residue formation, with this intention, ensuring long-term soldering quality even in demanding environments.

Preheating Module

The preheating process facilitates the successful soldering of complex multilayer PCBs. The selective soldering equipment optimizes preheating through the following methods:

  • Dual-sided Heating: Our equipment can heat the PCB from both sides simultaneously, ensuring even heat distribution across all solder joints and preventing soldering failures due to temperature imbalances.
  • Flexibility: The temperature profile can be adjusted to accommodate various circuit board specifications in mixed production lines.
  • SMD Protection: Prevent damage to surface-mounted devices (SMD) particularly caused by temperature fluctuations.
The diagram showing the full process of selective soldering, including the steps like flux application, preheating, and soldering
The diagram showing the full process of selective soldering, including the steps like flux application, preheating, and soldering (Image source: online)

Soldering Module

The key of selective soldering lies in its soldering module, which is typically divided into single-wave soldering and multi-wave soldering:

  • Single-wave Soldering: High flexibility and suitable for complex designs.
  • Multi-wave Soldering: Short production cycle and suitable for mass production.

The nozzle design is crucial to the soldering effect. For instance, in PCB Assembly, the Ersa VERSAFLOW system uses a round-tip nozzle design to provide balanced, omnidirectional solder flow, improving soldering reliability and avoiding solder bridges. Additionally, a nitrogen-protected environment around the nozzle further reduces solder oxidation, enhancing process consistency and quality.

A schematic diagram of a high-precision wave soldering structure, including a nitrogen-protected environment, solder wave height control, liquid level monitoring system, and solder pot temperature control.
A schematic diagram of a high-precision wave soldering structure, including a nitrogen-protected environment, solder wave height control, liquid level monitoring system, and solder pot temperature control. (Image source: online)

Selective Soldering in Raspberry Pi Development Boards

In embedded system development, the Raspberry Pi development board has become the platform of choice for hardware makers and engineers due to its flexibility and wide range of applications. LCSC offers one-stop PCBA services for such development boards as Raspberry Pi, with this in mind, ensuring that every solder joint meets high standards.

The GPIO (General Purpose Input/Output) interface of the Raspberry Pi is for the purpose of connecting peripherals and sensors, where soldering quality directly impacts the stability and reliability of the device. Traditional methods often result in short circuits or solder bridges between multiple pins, leading to device failures, whereas the selective soldering ensures uniform and precise soldering of each pin through accurate flux application, dual-sided heating, and efficient soldering modules.”

Raspberry Pi 5 8GB | Development Boards & Kits | LCSC Electronics
Raspberry Pi 5 8GB | Development Boards & Kits | LCSC

Some images are sourced online. Please contact us for removal if any copyright concerns arise.


Custom Cables: Save 50%+ Avg Cost By JST, Molex, TE Alternatives | Processing Fee Down to $1 Per Piece | No Minimum Order Quantity (MOQ) Required

PCB & PCBA: New Customer Get Coupons Up to $125 | 1 – 32 Layers From $2 /5pcs | PCB Assembly From $8 /5pcs

Front Panels: High-quality Front Panel Acrylic/PET | Front Panel Order Up to 30% Off | Membrane Switch Available Soon

Newsletter
Connect with us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30am to 12pm and 1:30pm to 10pm,
Monday through Friday, UTC/GMT +8.

SSL encrypted
payment
© 2024 LCSC.COM All Rights Reserved. 粤ICP备17041818号