Key Takeaways
Passive cooling (heat sinks, thermal vias, copper pours) uses no power and adds no moving parts. It’s ideal for loads under roughly 5–10 W. Active cooling (fans, liquid loops, thermoelectric coolers) forces air or fluid movement to handle higher power densities. However, it also adds noise, power draw, and failure points. As a result, most modern boards use a hybrid of both.
What Is PCB Thermal Management, and Why Does It Matter?
Every active component on a printed circuit board converts a portion of its electrical energy into heat. This includes MOSFETs, voltage regulators, MCUs, FPGAs, and power amplifiers. That heat must move to cooler regions of the surrounding environment. Otherwise, component temperatures will climb past their rated limits. Left unmanaged, excess heat degrades performance. It also accelerates component aging, and in the worst case, causes outright failure.
Thermal management is no longer an afterthought bolted on at the end of a design cycle. Instead, it’s now an integral part of the overall engineering workflow. Designers must balance mechanical, electrical, and cost constraints against the need for effective heat dissipation. Two broad strategies are available: passive cooling and active cooling. Choosing between them, or combining them, shapes everything from board layout to enclosure design. It also affects bill-of-materials cost.
Heat Sinks Guide: How Passive Cooling Keeps Boards Cool
Passive cooling relies entirely on conduction, natural convection, and radiation. No fans, pumps, or external power input are required. Common passive techniques include heat sinks, thicker copper planes, thermal vias, and high-conductivity substrate materials. Because passive systems have no moving parts, they’re inherently quiet. They’re also maintenance-free and highly reliable.
Passive heat sinks work by relying on natural convection and radiation to cool devices. No powered components are involved. As a result, they’re the default choice for low-power or noise-sensitive designs. For telecom equipment, LED systems, and embedded electronics, passive heat sinks are generally preferred. Their silent operation and high reliability make them a natural fit.
Reliability data backs this up at the system level, too. Field studies from the U.S. Air Force looked at electronics maintenance records. They found that fans and other mechanical parts account for up to 20–30% of field-replaceable failures in certain avionics subsystems. Removing moving parts, therefore, directly reduces failure rate. It also extends mean time between failures.
Types of Heat Sinks and When to Use Them
Heat sink geometry should match the airflow environment:
- Extruded aluminum fin heat sinks — the most common and cost-effective option for MOSFETs, voltage regulators, and small MCUs in enclosures with some airflow.
- Tall, sparsely finned heat sinks — best for pure natural convection, since rising air needs room to move between the fins.
- Pin-fin heat sinks — better for omnidirectional airflow, and common in dense, multi-orientation enclosures.
- Copper-base, aluminum-fin hybrids — used where thermal conductivity at the contact point matters more than weight or cost, such as in high-current power modules.
Any heat sink should be mounted using a thermal pad or thermal paste. Both materials have low thermal resistance. This helps move heat efficiently from the component into the heat sink, and then out into the surrounding air.
Thermal Vias, Copper Pours, and PCB-Level Passive Techniques
Before a heat sink even enters the picture, the PCB itself can act as a heat spreader. Via-in-pad designs sit directly under hot components. They transfer heat through the insulating FR-4 substrate to a larger copper area, such as an internal ground plane. There, the heat spreads out and dissipates. Similarly, thicker copper planes and additional thermal vias are among the lowest-cost, most effective passive techniques at the layout stage.
Active Cooling Solutions: Fans, Liquid Cooling, and TECs
When passive techniques can’t keep pace with power density, active cooling steps in. It adds energy to the system to force heat transfer. In practice, this means substituting weak natural convection with much stronger forced convection. It’s one of the most effective heat transfer mechanisms in electronic engineering. This category includes fans and blowers for forced-air convection. It also includes liquid cooling with cold plates or heat pipes, plus thermoelectric coolers (TECs, or Peltier devices) for the most demanding applications.
Fans are the simplest and cheapest active option, but they aren’t a cure-all. Active cooling typically starts with forced convection. However, simply adding a fan rarely solves a thermal problem on its own. Proper airflow control and ducting design matter just as much. Liquid cooling loops and TECs, meanwhile, step in for high-power-density boards. Think GPUs, RF power amplifiers, and industrial motor drives, where air alone can’t move enough heat fast enough.
The trade-off is reliability and complexity. Active heat sinks can be more compact than passive designs for the same cooling capacity. Their fans, however, generate noise and consume power. They also require maintenance as they wear or collect dust over time.
Cooling Solutions Calculator: Estimating Your Thermal Budget
Before choosing a cooling strategy, calculate whether passive cooling can handle your thermal load. The standard formula uses junction-to-ambient thermal resistance to find maximum safe power dissipation:
P_max = (T_j(max) − T_a) / R_th(JA)
For example, take a device with a maximum junction temperature of 150°C and a junction-to-ambient thermal resistance of 150°C/W. At an ambient temperature of 25°C, it can safely dissipate about 0.83 W.
To run your own quick check:
- Find your component’s θJA (junction-to-ambient thermal resistance) from its datasheet.
- Subtract your expected ambient temperature from the component’s maximum rated junction temperature.
- Divide that result by θJA to get your maximum safe power dissipation.
- Compare this to your actual power dissipation. If it’s exceeded, passive cooling alone likely isn’t enough, so budget for a heat sink. If the gap is large, plan for active cooling too.
Adding a heat sink extends the thermal path. It now includes three additional stages: junction-to-case resistance (θJC), the contact resistance through the thermal interface material (θCH), and heat sink-to-ambient resistance (θHA). Each stage adds to the total temperature rise. Recalculating with the heat sink’s θHA, therefore, shows exactly how much headroom the added surface area buys you.
Passive vs. Active Cooling: Head-to-Head Comparison
| Factor | Passive Cooling | Active Cooling |
| Power draw | None | Requires supply power for fans/pumps/TECs |
| Noise | Silent | Audible fan/pump noise |
| Moving parts | None | Fans, pumps, or compressors |
| Typical power handling | Low to moderate (≈ under 10 W per component, layout-dependent) | Moderate to very high |
| Reliability | High, minimal maintenance | Lower MTBF due to wear parts |
| Cost | Lower BOM cost | Higher BOM and assembly cost |
| Best for | Embedded systems, LED drivers, telecom, low-noise designs | GPUs, servers, industrial drives, RF power stages |
How to Choose the Right Thermal Strategy for Your Design
Most designs don’t have to pick one approach exclusively. In fact, you rarely need to choose between active and passive techniques at all. Both can work together for a more aggressive cooling strategy when a single approach falls short. In a well-designed hybrid system, passive cooling handles the baseline thermal load. As a result, active components like fans only need to run at higher speeds when necessary. This cuts average noise levels and power consumption compared to running a fan at full speed continuously.
A practical decision path:
- Calculate your power dissipation per component using the formula above.
- Start passive: add copper area, thermal vias, and a heat sink sized for your θJA budget.
- Re-measure or re-simulate junction temperature under worst-case ambient conditions.
- Add active cooling only if passive headroom is insufficient, starting with a low-speed fan before escalating to liquid cooling or TECs.
- Validate reliability. Check for risks like copper barrel fatigue, cracking, and delamination under thermal cycling, especially in passive copper-heavy designs.
Sourcing Thermal Management Components at LCSC
Whether you land on a passive-only heat sink or a full active cooling loop, component selection matters as much as the strategy itself. LCSC stocks a wide inventory of thermal management parts. This includes aluminum and copper heat sinks in multiple fin geometries, thermal pads and gap fillers, thermally conductive adhesives, DC fans, and TEC modules. It also carries the MOSFETs, regulators, and power ICs that generate the heat in the first place. Filtering by package size and thermal resistance rating makes it easy to match a heat sink to a component’s θJC and θCH values. Plus, JLCPCB integration means your thermal-via and copper-pour layout choices move straight from design to fabrication.
FAQ
Q: Can I use passive cooling for a high-power component like a GPU?
A: Generally, no, not on its own. High-TDP components like GPUs and server CPUs typically exceed what natural convection and a reasonably sized heat sink can dissipate. As a result, active cooling—fans, heat pipes, or liquid loops—is standard for these parts. That said, passive techniques still play a supporting role. Copper pours and thermal vias spread heat before it reaches the active cooling stage, which reduces the load the fan or pump has to handle.
Q: Do I need a heat sink if my board already has thermal vias and copper pours?
A: It depends on your calculated power dissipation. Thermal vias and copper pours extend the effective heat-spreading area of the PCB itself. For low-power components, that’s often enough on its own. However, for components dissipating more than a few watts, a discrete heat sink is usually still needed. It adds the extra surface area convection requires. Run the P_max calculation from this article to check where your specific components land.
Q: What’s the main downside of active cooling?
A: Moving parts. Fans and pumps introduce noise, consume power, and wear out over time. That’s why reliability-critical or noise-sensitive designs—avionics, telecom, medical—favor passive cooling wherever the thermal budget allows. Active cooling also adds bill-of-materials cost and assembly complexity. Fans and pumps need mounting hardware, wiring, and sometimes dedicated airflow ducting to work as intended.
Q: How do I know if my design needs a hybrid cooling approach?
A: Start with the thermal budget calculation. If the gap between passive heat sink capacity and actual power dissipation is small, a low-speed fan paired with a passive heat sink is often the better answer. It’s typically more efficient and quieter than sizing a heat sink alone to handle the full load. Hybrid designs also build in a safety margin: the passive stage keeps baseline temperatures in check, while the active stage only kicks in under peak load.
Q: Are thermoelectric coolers (TECs) considered active or passive?
A: Active. TECs require external power to move heat against a temperature gradient. A heat sink, by contrast, only ever moves heat toward a cooler surrounding environment. TECs are typically reserved for applications needing precise temperature control below ambient. Laser diodes and sensitive optical sensors are common examples, since even small temperature swings affect their performance.
Conclusion
Passive and active cooling solve the same problem: keeping component temperatures within their safe operating range. They just get there through fundamentally different means. Passive techniques—heat sinks, thermal vias, copper pours—cost less, run silently, and need no maintenance. However, they cap out at moderate power densities. Active techniques—fans, liquid cooling, TECs—scale to much higher thermal loads, but at the cost of noise, power draw, and wear parts. Run the thermal budget calculation early. Start with passive techniques wherever your numbers allow, and layer in active cooling only where the gap demands it.
Ready to spec your next thermal design? LCSC Electronics – Electronic Components Distributor to find parts matched to your exact power and package requirements.