Overcoming BGA Soldering Challenges: Best Practices for SMT Assembly

From smartphones to the electronic control units in modern vehicles and even to aerospace systems, Ball Grid Array (BGA) packaging plays a crucial role in high-performance electronics. Known for its compact size and pin density, BGA has become a preferred packaging solution for modern electronic products. Even though BGA soldering presents challenges in SMT assembly, we still manage to overcome.

BGA (Ball Grid Array) Chip: Top and Bottom View Showing Solder Balls - High-Density Interconnect for Modern Electronics
BGA (Ball Grid Array) Chip: Top and Bottom View Showing Solder Balls – High-Density Interconnect for Modern Electronics – TMS320C6713BZDP300

What Makes BGA Packaging Unique?

Ball Grid Array (BGA), is an advanced surface-mount packaging technology where solder balls replace traditional pins, connecting the chip to the Printed Circuit Board (PCB). The design allows for higher pin density in a compact size, enabling more complex circuits in a smaller footprint.

BGA (Ball Grid Array) Footprint on PCB: Solder Pad Layout for High-Density Chip Interconnection
BGA (Ball Grid Array) Footprint on PCB: Solder Pad Layout for High-Density Chip Interconnection (Image source: online)

However, the compact nature of BGA also introduces soldering challenges. The finepitch solder balls demand extreme precision during assembly. Any deviation can lead to connection failures, impacting overall circuit performance. Furthermore, traditional PCB via techniques often struggle to meet the routing demands of high-density BGA layouts.

Solder Paste Printing: The Foundation of Reliable Joints

Think of BGA soldering as constructing a skyscraper—the foundation must be solid and firm. In SMT assembly, that foundation is solder paste printing.

Solder paste is made of tiny solder powder mixed with flux. The printing process is similar to stencil art on coffee—PCB stencils (metal masks) are placed over the board, and a squeegee spreads solder paste across the aperture, ensuring precise deposition onto the solder pads.

Coffee Stencil
Coffee Stencil (Image source: online)
Solder Paste Printing: Stencil Application and Automated SMT Process
Solder Paste Printing: Stencil Application and Automated SMT Process (Image source: online)

Different application scenarios require the selection of the appropriate type of solder paste. Lead-free soldering has become the mainstream trend in the electronics industry. In addition, there are special types of low-temperature solder paste suitable for specific needs.

However, solder paste printing is not an easy task. If the squeegee parameters are not set correctly, or if there are problems with the solder paste itself, it may lead to various printing defects, such as insufficient solder paste, too much solder paste, bridging and so on.

PCB after Solder Paste Printing: Inspection for Defects like Insufficient Paste, Bridging, or Excess
PCB after Solder Paste Printing: Inspection for Defects like Insufficient Paste, Bridging, or Excess (Image source: online)

Reflow Soldering: Mastering Temperature Profiles

Once solder paste is applied, reflow soldering bonds the BGA to the PCB. This process is more than just heating—it’s about precise temperature control to prevent defects.

A typical reflow temperature profile consists of four key phases:

  1. Preheat – Gradually raises temperature to prevent thermal shock.
  2. Activation – Flux activates, removing oxides from the surface of the solder pad and solder balls.
  3. Reflow – Temperature reaches the peak, melting the solder and forming joints.
  4. Cooling – The solder solidifies to ensure strong mechanical and electrical bonds.
Reflow Soldering Temperature Profile: Preheat, Activation, Reflow, and Cooling Stages for Optimal SMT Solder Joints
Reflow Soldering Temperature Profile: Preheat, Activation, Reflow, and Cooling Stages for Optimal SMT Solder Joints (Image source: online)

Different PCB materials, component characteristics, and solder paste require tailored temperature profiles.

BGA Welding, Design Optimization and Quality Control: X-Ray Inspection, Via-inPad and Defect Analysis

Traditional visual inspection methods are ineffective since BGA solder joints are located beneath the chip. X-ray inspection offers a non-destructive solution, allowing manufacturers to visualize the inside structure of the solder joint and detect potential issues.

Common BGA Soldering Defects:

  • Bridging – Unintended connections between adjacent solder balls.
  • Cold Solder Joint – Incomplete melting leads to weak connections.
  • Voids – Air pockets or trapped inside solder joints reduce reliability.
  • Weak Solder Joint – Missing or poorly formed connections.
X-ray of BGA Solder Joint Defects: Bridging, Cold Solder, Voids, and Opens - PCBA Quality Control
X-ray of BGA Solder Joint Defects: Bridging, Cold Solder, Voids, and Opens – PCBA Quality Control (Image source: online)

Case Study and Solution

In the scenario shown below, pin U1_B7 presents challenges due to high-density constraints.

PCB Routing Issue and Solution of BGA
PCB Routing Issue and Solution of BGA (Image source: online)

To resolve this, we could redesign the entire routing scheme.

Constrained PCB Routing Example: Difficulty Routing Trace to BGA Pin U1_B7 - High-Density Design Challenge
Constrained PCB Routing Example: Difficulty Routing Trace to BGA Pin U1_B7 – High-Density Design Challenge (Image source: online)

Or we adopt a more direct approach—drilling a via in the pad and routing the trace from another layer. While this method simplifies routing and creates a cleaner layout, it has drawbacks. Drilling vias in pads may affect SMT soldering quality and weaken the pad’s mechanical strength, raising reliability concerns. This is why many PCB designers show hesitation in using this technique.

Via-in-Pad Solution for BGA Routing Challenges: PCB Layout with Drilled Pad for Alternative Trace Routing
Via-in-Pad Solution for BGA Routing Challenges: PCB Layout with Drilled Pad for Alternative Trace Routing (Image source: online)

To tackle this issue, we introduce Via-in-Pad technology, which not only optimizes routing density but also enhances electrical performance and soldering reliability.

Via-in-Pad technology uses a resin-filled and plated-over (resin plug + copper cap) approach. The approach allows vias to be placed directly in BGA pads without additional fan-out traces.

Via-in-Pad Technology for BGA: Cross-Section Showing Resin-Filled and Copper
Via-in-Pad Technology for BGA: Cross-Section Showing Resin-Filled and Copper (Image source: online)
Via-in-Pad vs. Conventional Via: Comparison of PCB Pad Appearance
Via-in-Pad vs. Conventional Via: Comparison of PCB Pad Appearance (Image source: online)

Advantages of Via-in-Pad Technology

  • Higher Routing DensityRelease more routing space, especially in high-density BGA designs.
  • Improved Electrical Performance – Reduces trace length, minimizing inductance and signal delay.
  • Eliminates Traditional Via IssuesEliminates the risk of via pad discoloration caused by solder mask covering. Moreover, it prevents solder ball blowout during BGA soldering due to plugged vias.
  • Increased Design Efficiency – A routing task that previously took 7 days may now take just 2 days.

Lead-Free Soldering

To protect the environment and human health, the electronics industry is gradually phasing out lead-based solder and adopting lead-free soldering. The RoHS directive enforces stringent environmental regulations on lead-free processes. However, lead-free solder has a higher melting point and lower wettability compared to traditional lead-tin solder, requiring stricter process control.

RoHS Compliant Lead-Free Solder Paste for Environmentally Friendly SMT Assembly
RoHS Compliant Lead-Free Solder Paste for Environmentally Friendly SMT Assembly (Image source: online)

Some images are sourced online. Please contact us for removal if any copyright concerns arise.

More Discount Information
Connect With Us
Customer Service: 0086-755-83210457
Logistics Dept.: 0086-755-83233027
9:30 am - 12 am, 1:30 pm - 10 pm
Monday - Friday, UTC/GMT +8
View Our Social Channels
Encrypted
Payment
© 2025 LCSC.COM All Rights Reserved.
粤ICP备17041818号 ISO/IEC