Key Takeaways
A multimeter measures voltage in parallel, current in series, and resistance on an unpowered circuit. First, set the dial and probe jacks to match the quantity you’re measuring. Then start on the highest range for unknown values. Above all, never measure current across a voltage source — it’s the single most common cause of a blown fuse.
Whether you’re troubleshooting a dead battery, verifying a resistor before soldering it to a PCB, or checking continuity on a cable assembly, the multimeter is the first tool most engineers reach for. However, it’s also one of the easiest to misuse. For instance, connecting the probes to the wrong jack, or measuring the wrong quantity in the wrong configuration, can blow an internal fuse or short a power source. So this guide covers how to measure voltage, current, and resistance correctly, what the dial and ports mean, and the mistakes that trip up even experienced technicians.
What Is a Multimeter and How Does It Work?
A multimeter (also called a volt-ohm-milliammeter, or VOM) is a handheld test instrument that combines a voltmeter, ammeter, and ohmmeter into a single device. Modern digital multimeters (DMMs) display readings numerically on an LCD. In doing so, they replace the analog needle-and-scale meters common before the 1970s. Inside, a DMM uses an analog-to-digital converter to sample the input signal. Meanwhile, internal resistors, shunts, and a small test current handle the actual measurement across each function.
Most DMMs today are autoranging, automatically selecting the correct measurement range. Still, many bench and field meters offer manual ranging for finer control. In addition, higher-end meters add True RMS (Root Mean Square) measurement, which reports accurate readings on non-sinusoidal AC waveforms. This matters for variable-frequency drives, switching supplies, or dimmer circuits, where a standard averaging meter can read incorrectly.
Multimeter Basics Guide: Understanding the Dial, Display, and Ports
Before taking a measurement, it helps to know what each part of the meter does. Most multimeters share a common layout:
- Display: Shows the numeric reading, the unit (V, A, Ω), and mode indicators like AC/DC or autorange.
- Rotary dial: Selects the measurement function — DC voltage (V⎓), AC voltage (V~), DC/AC current (A), resistance (Ω), continuity (🔊), diode test, and sometimes capacitance or frequency.
- Input jacks: Typically three or four ports, each dedicated to specific measurements.
Ports, Probes, and Symbols Explained
| Jack Label | Used For | Notes |
| COM | Common/negative return for every measurement | Black probe always goes here |
| VΩmA (or V/Ω) | Voltage, resistance, continuity, and low current (typically under 200–400 mA) | Red probe for most everyday measurements |
| 10A / 20A | High-current DC/AC measurement | Red probe moves here for currents above the mA jack’s rating |
The black lead stays in COM for every measurement. The red lead is the one that moves. For voltage, resistance, and continuity, it goes into the VΩmA jack; for amps above the milliamp range, it goes into the dedicated high-current jack. Leaving the red lead in the current jack during a voltage measurement is a classic mistake. As a result, it briefly turns the multimeter into a short circuit — more on that below.
For safety, check the meter’s CAT rating (CAT I–IV, defined under IEC 61010) before working on any circuit connected to mains power. This rating indicates how large a transient voltage spike the meter can survive at a given point in the system. Specifically, CAT II covers plug-in loads and appliances, CAT III covers a building’s fixed wiring and distribution panels, and CAT IV covers the service entrance and utility connection. Therefore, using a meter rated below the environment it’s used in is a genuine safety hazard, not just a technicality.
How to Measure Voltage with a Multimeter
Voltage is measured in parallel — across the two points you want to measure, without breaking the circuit.
- Insert the black probe into COM and the red probe into the VΩmA jack.
- Set the dial to DC voltage (V⎓) for batteries and DC supplies, or AC voltage (V~) for mains equipment.
- Touch the probes across the points of interest — red to the more positive point, black to the more negative (polarity doesn’t matter for AC).
- Read the value. On a manual-range meter, start with the highest range and step down as needed.
AC vs DC Voltage Measurement
DC voltage has a fixed polarity. So, reversing the probes on a DC measurement simply flips the sign of the reading rather than causing damage. AC voltage — like a 120V or 230V wall outlet — has no fixed polarity, since current reverses direction 50 or 60 times per second depending on region. Most basic DMMs measure AC using average-responding rectification calibrated for clean sine waves. However, a True RMS meter is needed for accurate readings on distorted or non-sinusoidal AC waveforms, such as those from motor drives or PWM-controlled circuits.
How to Measure Current with a Multimeter
Current is measured in series — meaning the circuit must be broken open and the meter inserted directly into the current path, not placed across a component.
- Power down the circuit before making any connections.
- Move the red probe to the appropriate current jack: mA for currents under roughly 200–400 mA (check the meter’s rating), or 10A/20A for higher currents.
- Set the dial to DCA or ACA as appropriate.
- Break the circuit and connect the meter in-line — red probe toward the positive supply side, black toward the load, for DC.
- Restore power, read the value, then power down before disconnecting.
Never place a multimeter set to current mode across a voltage source. Likewise, never leave the red probe in the current jack when switching back to a voltage measurement. In current mode, the meter presents an intentionally very low resistance to sense current flow. Consequently, touching that low-resistance path across a battery or supply creates a near dead short. This is the leading real-world cause of a blown internal fuse, and on unfused or high-energy sources, it can damage the meter or injure the user.
Multimeter Basics Calculator: Using Ohm’s Law to Verify Current Readings
A quick way to sanity-check a current reading — or to pick the right jack and range before connecting a meter — is Ohm’s Law: I = V ÷ R. Simply knowing the supply voltage and circuit resistance lets you calculate expected current before ever connecting a probe. For example, a 5V supply driving a 220Ω resistor should draw about 22.7 mA, which is comfortably inside a standard mA jack’s rating. That quick calculation also gives you a reference value, so you can confirm the meter is reading correctly rather than displaying a fault.
How to Measure Resistance and Continuity
Resistance and continuity checks must be done on a de-energized circuit with any capacitors discharged. This is because the meter injects its own small test current, and an external voltage will produce an invalid — or damaging — reading.
- Set the dial to Ω for a resistance value, or to the continuity setting (speaker/diode symbol) for a pass/fail beep test.
- Keep the red probe in the VΩmA jack.
- Touch the probes across the component. On an isolated resistor, this is straightforward. However, on a resistor still soldered in-circuit, parallel paths through other components can produce a lower reading than the true value.
- For continuity, a steady beep indicates a low-resistance path (often under a few hundred ohms), confirming a solid connection, trace, or fuse.
Reading Resistor Color Codes with a Multimeter
Resistor color-band codes give you a component’s rated value. In contrast, a multimeter confirms the actual measured value — useful for verifying tolerance, checking for damage, or identifying an unmarked part pulled from stock. If the measured resistance falls well outside the color-coded tolerance band (commonly ±1% or ±5%), the component may be damaged or miscategorized.
Common Multimeter Mistakes and Safety Tips
- Leaving the red lead in the current jack: the fastest way to blow a fuse on your next voltage measurement.
- Measuring resistance on a live circuit: produces inaccurate readings and can damage the meter.
- Using the wrong CAT-rated meter or leads on mains circuits: a serious shock and arc-flash risk.
- Ignoring “OL” (over-limit) on the display: means the value exceeds the selected range — step up the range or check your leads.
- Skipping continuity checks on fuses and leads: a worn lead or blown internal fuse is a common source of “no reading” confusion.
Always disconnect probes before changing the dial setting or moving a lead between jacks. Also, start with the highest range on an unknown value.
Frequently Asked Questions
Q: What’s the difference between an analog and digital multimeter?
An analog multimeter uses a moving needle over a printed scale, while a digital multimeter (DMM) uses an ADC and LCD to display a numeric reading. As a result, DMMs dominate today, since they’re easier to read precisely and include features like autoranging, continuity beepers, and True RMS AC measurement.
Q: Why did my multimeter fuse blow?
The most common cause is measuring current with the red probe still connected across a voltage source, or leaving the leads in the current jack while attempting a voltage reading. In both cases, the meter’s low-resistance current path is effectively shorted across a supply, so the internal fuse sacrifices itself to protect the meter and user.
Q: Can I measure current by putting the probes directly into a wall outlet?
No. Never insert probes into a live outlet to measure current, since this places the meter directly across mains voltage in current mode and creates a dangerous short circuit. Instead, use a clamp meter to measure current on live AC circuits without breaking the circuit.
Q: What does “OL” mean on a multimeter display?
OL stands for “over-limit.” It means the value being measured exceeds the currently selected range — for example, measuring a 2 MΩ resistor on a 200 kΩ range. In that case, select a higher range or switch to autorange and try again.
Q: Do I need a True RMS multimeter?
For clean sine-wave AC voltage — like a standard wall outlet — a standard averaging meter is accurate enough. However, for motor drives, dimmers, UPS output, or other non-sinusoidal AC waveforms, a True RMS meter gives a materially more accurate reading.
Choosing the Right Multimeter and Components for the Job
A reliable multimeter is only half the equation — accurate measurements also depend on quality test leads, the right replacement fuse, and correctly specified resistors and connectors on the board you’re testing.
LCSC stocks precision resistors, test connectors, fuses, and passive components for engineers who need accurate, repeatable measurements. In addition, LCSC offers global shipping and JLCPCB integration for teams moving from bench testing straight into board fabrication. Browse LCSC’s resistor and passive component catalog to source the parts behind your next measurement.