Effective thermal management is critical in electronic systems where power dissipation, component density, and enclosure constraints can cause local temperatures to rise. Heat sinks and thermal interface materials (TIMs) are widely used to control the thermal path from heat-generating components to the surrounding environment.
Their applications vary significantly between power supplies, LED lighting, industrial controls, motor drives, embedded systems, and PCB assemblies. Understanding the thermal path and interface requirements helps determine where each technology is most effective.
Heat Sinks and Thermal Interface Materials

A typical thermal path can be represented as:
Heat Source → Thermal Interface → Heat Spreading Structure → Cooling Medium → Environment
A heat sink spreads heat from a localized source over a larger surface area, allowing heat to be transferred to air or another cooling medium through convection and radiation.
A thermal interface material (TIM) reduces thermal resistance between two mating surfaces. Even apparently flat surfaces contain microscopic irregularities that can trap air and increase thermal resistance. A TIM fills these gaps and improves heat transfer.
Thermal pads are one type of TIM. They are particularly useful where a controlled thickness, gap filling, mechanical compliance, or electrical insulation is required. Other TIM technologies include thermal grease, thermal paste, phase-change materials (PCM), thermal gel, thermal adhesive, and thermal tape. These materials are not interchangeable in every application.
For high-heat-flux interfaces, grease or PCM may provide lower interface resistance than a relatively thick thermal pad. Thermal pads become particularly useful when the interface includes larger tolerances or multiple components that must contact the same heat-spreading structure.

Thermal Management in Power Supplies
Power supplies continuously convert electrical energy, and power losses in MOSFETs, rectifiers, switching devices, and other power components become heat.
A typical thermal path is:
Power Semiconductor → TIM → Heat Sink → Ambient Air
In compact power supplies, the main challenge is often removing heat from localized components while maintaining acceptable enclosure temperatures. A thermal pad can provide a compliant interface between the device and heat sink, especially when the mounting surfaces are not perfectly coplanar.
For enclosed power supplies, the heat sink must also work with the available airflow. Natural convection may be sufficient for lower-power designs, while forced airflow may be required as power density increases.
Thermal Management in LED Lighting
LED performance is strongly related to junction temperature. Excessive junction temperature can affect light output, efficiency, and long-term reliability.
A typical thermal path is:
LED Junction → Package / MCPCB → TIM → Heat Sink → Ambient
In high-power LED lighting, the heat sink provides the main heat-spreading and heat-dissipation structure, while the TIM reduces thermal resistance between the LED assembly and the heat sink.
Mechanical flatness, interface thickness, mounting pressure, and thermal conductivity can therefore influence the overall thermal path. The objective is not simply to select a heat sink with a large surface area, but to maintain a low-resistance path from the LED junction to the environment.
Thermal Management in Industrial Control Equipment
Industrial control equipment such as PLC systems, motor controllers, power controllers, and automation equipment often operates continuously inside electrical cabinets or enclosed housings.
Heat management can involve several mechanisms simultaneously:
- Component-level heat sinks
- Thermal pads or other TIMs
- PCB copper planes
- Thermal vias
- Metal enclosures or chassis
- Natural or forced airflow
The challenge is often cumulative heat rather than a single high-power component. Several moderately hot components can raise the internal enclosure temperature and reduce the thermal margin of the entire system.
For this reason, thermal management should consider both local component temperatures and system-level airflow and heat spreading.
Thermal Management in Motor Drives and Power Electronics
Motor drives and power converters can generate substantial heat through switching and conduction losses. MOSFETs, IGBTs, rectifiers, and power modules may require dedicated thermal paths.
A simplified thermal chain is:
Junction → Package → TIM → Heat Sink / Cold Plate → Cooling Medium
For higher-power systems, the thermal design may combine heat sinks with forced air, liquid cooling, cold plates, or chassis-based heat spreading.
Mechanical mounting is also important. The TIM must maintain adequate contact across the interface, while excessive mechanical pressure can introduce stress into the semiconductor package, PCB, or mounting structure.
Thermal Management in Embedded Computing Systems
Embedded computing systems combine high-power processors with limited physical space. Thermal design therefore depends strongly on heat flux, package construction, available airflow, and mechanical constraints.
High-heat-flux processors commonly use thermal grease or phase-change materials where very low interface resistance is required. Thermal pads are also widely used around processors for components such as VRM MOSFETs, voltage regulators, memory devices, and other power-management components.
In compact systems, a common approach is to transfer heat from several components to a shared heat spreader, chassis, or heat sink. Thermal pads are useful when component heights vary and the interface must accommodate mechanical tolerances.
Thermal Management in Communication Equipment
Communication equipment often contains a high density of processors, power-management devices, transceivers, and other heat-generating components within a limited enclosure.
Thermal pads can connect multiple components with different heights to a common heat-spreading structure, while low-profile heat sinks can provide localized cooling where space is restricted.
At the system level, the design must prevent heat generated by one component from unnecessarily increasing the temperature of neighboring heat-sensitive components. Airflow direction, component placement, heat spreading, and enclosure design therefore become part of the thermal solution.
PCB-Level Thermal Management

Thermal management does not always begin with a heat sink. For many surface-mount power devices, the PCB itself forms an important part of the thermal path.
A typical path can be:
Junction → Package → Exposed Pad → PCB Copper → Thermal Vias → Copper Plane → Heat Spreader / Heat Sink
An exposed thermal pad on the package can transfer heat directly into the PCB copper. Thermal vias then provide a path to internal or bottom copper layers, increasing the effective heat-spreading area.
This is particularly important for power MOSFETs, voltage regulators, LED drivers, and other surface-mount devices where the available package area is small.
Thermal Resistance, BLT, and Compression

Several interface parameters directly affect thermal performance.
Thermal Resistance describes how strongly a thermal path resists heat flow. For a simplified uniform interface:
R ≈ t / (k × A)
where:
- R= thermal resistance
- t= effective interface thickness
- k= thermal conductivity
- A= effective contact area
This relationship shows why increasing interface thickness can increase thermal resistance, while greater contact area and higher conductivity can reduce it.
However, thermal pad thickness cannot simply be minimized. A pad must be thick enough to fill the actual gap and accommodate component-height variation.
This is where BLT (Bond Line Thickness) becomes important. The effective BLT after assembly may differ from the material’s nominal free thickness because of compression and surface conditions.
Compression and contact pressure also affect interface performance. Insufficient compression can leave air gaps and increase contact resistance, while excessive compression may stress the component, PCB, or mechanical assembly.
Therefore, thermal conductivity alone is not enough to evaluate a TIM.
Choosing Thermal Management for Different Applications
| Application | Main Thermal Challenge | Typical Thermal Approach |
| Power Supplies | Continuous power loss | Heat sink + TIM + airflow |
| LED Lighting | Junction temperature | MCPCB + TIM + heat sink |
| Industrial Control | Continuous operation and enclosure heating | Heat spreading + airflow + TIM |
| Motor Drives | High power density | Heat sink/cold plate + TIM + forced cooling |
| Embedded Computing | High local heat flux and limited space | Grease/PCM or thermal pads depending on component |
| Communication Equipment | High component density | Low-profile heat sinks + thermal pads + chassis/airflow |
| PCB Power Devices | Localized package heating | Exposed pad + copper + thermal vias + heat spreading |
The correct thermal solution depends on the complete thermal path rather than on any single component specification.
FAQ
Are thermal pads the same as TIMs?
No. Thermal pads are one type of thermal interface material. Other TIMs include grease, PCM, gel, adhesive, and tape.
Is higher thermal conductivity always better?
Not necessarily. Interface thickness, contact resistance, compression, contact area, and actual mounting conditions also affect the resulting thermal performance.
Why is thermal pad thickness important?
A thicker pad can accommodate larger gaps and mechanical tolerances, but excessive interface thickness can increase thermal resistance.
Are thermal pads suitable for CPUs?
They can be used in some processor cooling designs, but high-heat-flux processors often use thermal grease or phase-change materials where lower interface resistance is required. Thermal pads are also common for nearby VRM, memory, and power-management components.
Why are thermal vias used under power devices?
Thermal vias transfer heat from the package or exposed pad into other PCB copper layers, increasing the available heat-spreading area and reducing the thermal resistance of the PCB path.
Find the Right Thermal Management Products at LCSC
LCSC offers heat sinks, thermal pads, and other thermal interface materials for power supplies, LED lighting, industrial controls, embedded systems, motor drives, communication equipment, and PCB-level thermal management.
When evaluating products, consider the complete thermal path, including thermal resistance, thermal conductivity, interface thickness, BLT, compression, electrical insulation, mounting method, operating temperature, and available cooling conditions.
Explore LCSC’s thermal management products to find solutions for different component-level and system-level cooling requirements.