Key Takeaways
A power budget is a spreadsheet that tracks input voltage, current draw, and output power for every load and regulator in a system. Calculate it by listing components, applying P = V × I, dividing by regulator efficiency, and summing active, idle, and peak states. Under-budgeting causes brownouts; over-budgeting wastes board space and cost.
Have you ever watched a prototype brown out the moment a motor spins up? Or found a voltage regulator running hot enough to leave a burn mark on the solder mask? The root cause is almost always the same. Nobody built a proper power budget before laying out the board. A power budget isn’t optional paperwork. It’s the document that tells you whether your power supply unit (PSU), battery, or DC-DC converter can deliver what the circuit needs. That includes every condition the product will see in the field.
What Is a Power Budget?
A power budget is an analysis of the entire power delivery network. It covers the input source, cables and connectors, every voltage conversion stage, and each electrical load. It accounts for the power each functional block consumes and the power dissipated along the way. Done correctly, it tells you three things before you ever touch a soldering iron:
- Whether your chosen power supply, battery, or wall adapter has enough headroom
- How much heat each regulator will need to dissipate
- What trace widths and copper pours your PCB layout actually requires
Skipping this step is how engineers end up discovering, after fabrication, that a 5 A peak load is running through a trace sized for 500 mA. The result shows up as voltage droop, microcontroller brown-outs, or a scorched PCB — not a clean bill of materials.
The Core Power Formula: Watt’s Law and Its Variations
Every power budget starts with the same relationship: P = V × I. Power (P) is in watts, voltage (V) is in volts, and current (I) is in amperes. When current isn’t directly measurable, two derived forms of Watt’s Law fill the gap:
| Known Values | Formula | Use Case |
| Voltage, current | P = V × I | Direct measurement from datasheet or bench supply |
| Voltage, resistance | P = V² / R | Resistive loads (heaters, resistor dividers) |
| Current, resistance | P = I² × R | Trace and connector loss calculations |
For AC systems, use RMS voltage and current rather than peak values. Apparent power (VA) and real power (W) diverge once phase angle and reactive components enter the picture. For DC rails on a typical embedded or IoT board, P = V × I is almost always the right formula.
Step-by-Step: Building Your Power Budget Spreadsheet
A power budget is best built as a spreadsheet, not a mental estimate. Each row is a component or power stage. The columns track input voltage, input current, output voltage, output current, power in, and power out.
Step 1: List Every Component and Its Current Draw
Start with a bill of materials. Pull the current consumption for each part directly from its datasheet. This includes the CPU, memory, RF transceiver, sensors, LEDs, motor drivers, and any auxiliary ICs. If a component appears multiple times on the board — say, six identical linear regulators — multiply its per-unit current by the quantity. Don’t estimate.
Step 2: Account for Regulator and Converter Efficiency
Power doesn’t pass through a linear regulator or DC-DC converter for free. A linear regulator dissipates the voltage drop as heat. If a 2.5 V rail drops to 2.0 V, that 0.5 V difference multiplied by current is wasted power, not delivered power. Switching converters are more efficient, but they rarely hit 100%. Texas Instruments’ switching regulator fundamentals documentation notes that buck converter efficiency is typically highest at the lowest input voltage. That efficiency often falls in the high-80s to low-90s percent range. A converter rated at, say, 85% efficiency has input power draw equal to output power divided by that figure. It’s not the same as output power. This is the step engineers most often skip. It’s usually where a “close enough” budget turns into a supply that can’t keep up.
Step 3: Sum Active, Idle, and Peak Power States
A single total-power number hides the details that actually break designs. Calculate the budget for at least three operating states:
- Idle/standby — sensors sleeping, radio off
- Active/typical — normal operation
- Peak/burst — motor start-up, RF transmit burst, simultaneous worst-case loads
Sizing a supply only for the “typical” state is a common cause of field failures. A motor inrush current or a radio transmit spike can briefly exceed what the regulator or battery can source.
Power Supply Calculators Guide: Tools That Speed Up the Process
Building a budget by hand is the most rigorous approach. But for quick sanity checks or early-stage estimates, a dedicated calculator tool saves time. This power supply calculators guide covers what to look for and when each tool type is appropriate.
- Battery life / runtime calculators — take total system current draw and battery capacity (mAh or Wh) to estimate operating time; useful for IoT and portable designs
- Trace width calculators (per IPC-2221) — convert your peak current figures into required copper trace width and thickness
- Regulator/converter selection tools — many manufacturers (Texas Instruments, Analog Devices, onsemi) publish efficiency and thermal calculators tied to specific part numbers
- Spreadsheet templates — the most flexible option, since they can be customized per project and reused across product revisions
Using a Power Supply Calculator
A power supply calculator is an online or spreadsheet-based tool built for this task. It typically asks for input voltage, load current per rail, and converter efficiency. In return, it outputs input power, power dissipation, and — for well-built tools — recommended trace width or heatsink sizing. Treat these outputs as a first-pass estimate, not a final sign-off figure. Always cross-check against the component-level datasheet numbers in your master spreadsheet. Generic calculators can’t account for board-specific thermal conditions or transient loads unique to your layout.
Thermal and PCB Design Implications of Your Power Budget
The power budget doesn’t stop at the bill of materials. It directly drives your PCB layout decisions. Peak current figures determine the copper trace width and weight needed to avoid excessive resistive heating. This follows IPC-2221, the Generic Standard on Printed Board Design. ([Related: Understanding PCB Trace Width and Current Capacity]) Total dissipated power, in turn, determines whether a regulator needs a heatsink, thermal vias, or a copper pour acting as a heat spreader. A board that dissipates several watts continuously needs that thermal path planned into the layout from the start. Don’t wait for a thermal-camera test to reveal a hot spot before adding it.
Common Power Budget Mistakes to Avoid
- Using typical current instead of maximum current from the datasheet, which leaves no margin for process variation or temperature effects
- Forgetting converter efficiency, treating input power as equal to output power
- Ignoring inrush and peak currents for motors, capacitive loads, and RF transmit bursts
- Measuring apparent power (VA) as if it were real power (W) on AC-input designs
- Skipping a margin allowance — a healthy power budget typically reserves 20–30% headroom above the calculated peak. This absorbs component tolerance, aging, and future firmware or feature additions. The Hardware and Systems Engineering Design – Power Budget walks through building and validating a margin-inclusive budget for an embedded device.
FAQ
Q: What formula is used to calculate power in a circuit?
The base formula is P = V × I. Power (P) in watts equals voltage (V) in volts multiplied by current (I) in amperes. When current isn’t directly measurable, two derived forms fill the gap. P = V²/R works for resistive loads like heating elements. P = I²R is commonly used to estimate resistive losses in PCB traces and connectors. For AC circuits, use RMS (root-mean-square) values of voltage and current instead of peak values. Real power (watts) and apparent power (volt-amps) diverge once phase angle and reactive components are involved.
Q: How much margin should I add to a power budget?
Most hardware teams reserve 20–30% headroom above the calculated peak power draw. This margin absorbs component tolerances, since datasheet current specs are often typical rather than worst-case. It also covers performance drift as components age, plus temperature-related efficiency losses in regulators. And it covers the near-certainty that firmware updates or added features will increase current draw over a product’s life. Skipping this margin is a common reason a design passes bench testing but fails in the field. Ambient temperature, battery aging, or an added sensor can push the real load past what was originally budgeted.
Q: Do I need to account for regulator efficiency in a power budget?
Yes. Input power to a regulator or DC-DC converter equals the load’s output power divided by the regulator’s efficiency. That’s not the same value as the output power. A linear regulator dissipates the voltage drop across it as heat. A switching converter, even at 80–90% efficiency, still loses some power as heat in its switches, inductor, and control circuitry. Skipping this step consistently underestimates the current your source actually needs to deliver. That’s a common reason a power budget looks fine on paper. It fails once the board is populated and running real loads.
Q: Can I rely on an online power supply calculator instead of a manual spreadsheet?
Online calculators are useful for fast, early-stage sanity checks. They can estimate battery runtime, trace width, or converter efficiency without building a full spreadsheet from scratch. However, they typically can’t account for board-specific conditions like ambient temperature, enclosure airflow, or the exact mix of components on your particular design. A complete spreadsheet remains the more reliable method for final sign-off. List every component’s datasheet current across idle, active, and peak operating states before committing to a PCB layout or ordering a production run.
Conclusion
A rigorous power budget is what separates a prototype that survives its first field test from one that browns out under load. Start with the P = V × I fundamentals. Build a spreadsheet that tracks every component across idle, active, and peak states. Factor in real regulator efficiency, and add margin before you commit to a PCB layout.
Once your power budget is finalized, browse LCSC’s selection of voltage regulators, DC-DC converters, and passive components. You can source every part on your bill of materials in one place. Datasheets, package options, and global shipping help take your next board from budget to build.